Command/Query
:CALCulate:EQUalization:STATe {ON|OFF|1|0}
:CALCulate:EQUalization:STATe?
This command sets the equalization function state on/off.
|
Description |
Equalization function ON/OFF |
|
Data Type |
Boolean type (Boolean) |
|
Range |
ON|OFF|1|0 |
|
Preset Value |
OFF |
|
Unit |
- |
|
Resolution |
- |
{1|0}<newline><^END>
10 OUTPUT 717;":CALC:EQU:STAT ON"
20 OUTPUT 717;":CALC:EQU:STAT?"
30 ENTER 717;A$
:CALCulate:EQUalization:CTLE:DC
:CALCulate:EQUalization:CTLE:POLE1
:CALCulate:EQUalization:CTLE:POLE2
:CALCulate:EQUalization:CTLE:ZERO1
:CALCulate:EQUalization:FILename
Setup > Adv Waveform > Equalization > Enable
Eye/Mask > Advanced Waveform (Under Stimulus) > Equalization > Enable