Command/Query
:CALCulate:EQUalization:FILename <File>
:CALCulate:EQUalization:FILename?
This command sets the filename of the equalization equation user file. It is necessary to select the file by :CALCulate:EQUalization:TYPE and turn ON the :CALCulate:EQUalization:STATe. This file is saved with .csv extension.
Specify the file name with the extension. When you use directory names (folder names) and file name, separate them with "\ " (back slash), or "/" (slash).
|
Description |
Equalization equation file name (extension: .csv) |
|
Data Type |
Character string type (String) |
|
Range |
254 characters or less |
|
Preset Value |
"" |
{string}<newline><^END>
10 OUTPUT 717;":CALC:EQU:FIL ""D:\folder\User.csv"""
20 OUTPUT 717;":CALC:EQU:FIL?"
30 ENTER 717;A$
:CALCulate:EQUalization:CTLE:DC
:CALCulate:EQUalization:CTLE:POLE1
:CALCulate:EQUalization:CTLE:POLE2
:CALCulate:EQUalization:CTLE:ZERO1
Setup > Adv Waveform > Equalization > Load
Eye/Mask > Advanced Waveform (Under Stimulus) > Equalization > Load