Controls math operations on the currently selected measurement and memory.
These commands are Superseded by the CALCulate:MEASure:MATH commands.
|
CALCulate:MATH: |
Click on a keyword to view the command details.
See Also
Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more.
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-Write) Sets math operations on the currently selected measurement and the trace stored in memory. (There MUST be a trace stored in Memory. See CALC:MATH MEM) |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<char> |
The math operation to be applied. Choose from the following: |
|
|
NORMal |
Trace data only |
|
|
ADD |
Data + Memory |
|
|
SUBTract |
Data - Memory |
|
|
MULTiply |
Data * Memory |
|
|
DIVide |
Data / Memory |
|
Examples |
CALC:MATH:FUNC NORM |
|
Query Syntax |
CALCulate<cnum>:MATH:FUNCtion? |
|
Return Type |
Character |
|
NORMal |
|
Applicable Models: N522xB, N523xB, N524xB (Read-Write) Sets and reads the state of the memory data interpolation. Learn more. |
|
|
Parameters |
|
|
<ch> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <ch> is set to 1. |
|
<bool> |
Choose from: 0 - OFF - Turn memory data interpolation OFF. 1 - ON - Turn memory data interpolation ON. |
|
Examples |
CALC2:MATH:INT 1 |
|
Query Syntax |
CALCulate<ch>:MATH:INTerpolate? |
|
Return Type |
Boolean |
|
0 |
|
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Write-only) Puts the currently selected measurement trace into memory. (Data-> Memory). |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
Examples |
CALC:MATH:MEM |
|
Query Syntax |
Not applicable |
|
Not applicable |
|