Selects a measurement parameter.
|
CALCulate:MEASure
|
Click a keyword to view the command details.
See Also
|
Applicable Models: All (Read-Write) Set/get a measurement parameter for the specified (cnum/mnum) measurement. This command replaces the following commands:
Note: For Application Measurements see CALCulate:MEASure:DEFine |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurements to be listed. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<string> |
(String ) Measurement Parameter to create. Case sensitive. For S-parameters: Any S-parameter available in the VNA Single-digit port numbers CAN be separated by "_" (underscore). For example: "S21" or "S2_1" Double-digit port numbers MUST be separated by underscore. For example: "S10_1" For ratioed measurements: Any two VNA physical receivers separated by forward slash '/' followed by comma and source port. For example: "A/R1, 3" Learn more about ratioed measurements See a block diagram showing the receivers in YOUR VNA. For non-ratioed measurements: Any VNA physical receiver followed by comma and source port. For example: "A, 4" Learn more about unratioed measurements. See the block diagram showing the receivers in YOUR VNA. Ratioed and Unratioed measurements can also use logical receiver notation to refer to receivers. This notation makes it easy to refer to receivers with an external test set connected to the VNA. You do not need to know which physical receiver is used for each test port. Learn more. For ADC measurements: Any ADC receiver in the VNA followed by a comma, then the source port. For example: "AI1,2" indicates the Analog Input1 with source port of 2. Learn more about ADC receiver measurements. For Balanced Measurements: For 1 port balanced measurement, choose from: Sdd11, Scd11, Sdc11, Scc11
For Balanced - Single-ended measurement, choose from: Sdd11, Scd11, Sdc11, Scc11, Ssd21, Ssc21, Sds12, Scs12, Sss22, Imb, CMMR1, CMMR2
For Single-ended - Balanced measurement, choose from: Sss11, Sds21, Scs21, Ssd12, Ssc12, Sdd22, Scd22, Sdc22, Scc22, Imb, CMMR1, CMMR2
For Balanced - Balanced measurement, choose from: Sdd11, Sdd21, Sdd12, Sdd22, Scd11, Scd21, Scd12, Scd22, Sdc11, Sdc21, Sdc12, Sdc22, Scc11, Scc21, Scc12, Scc22, Imb1, Imb2, CMMR
For Single-ended - Single-ended - Balanced measurement, choose form: Sss11, Sss21, Sss12, Sss22, Sds31, Scs31, Sds32, Scs32, Ssd13, Ssd23, Ssc13, Ssc23, Sdd33, Scd33, Sdc33, Scc33, Imb1, Imb2, CMMR1, CMMR2
Note: The right definition for SSB imbalance is added as Imb3, 4. The definition for SSB Imb1, 2 seem a mistake, but keep it remained for backward compatibility. Note: For Application Measurements see CALCulate:MEASure:DEFine |
|
Examples |
CALC:MEAS:PAR "Sdd11" calculate2:measure2:parameter "Sdd11" |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:PARameter? |
|
Return Type |
String |
|
"S11" |
|