Creates and modifies application measurements.
These commands are Superseded by the CALCulate:MEASure:DEFine and CALCulate:MEASure:PARameter commands.
|
CALCulate:CUSTom: |
See Also
|
Applicable Models: All (Write-only) Creates a custom measurement depending on the configurations and options. The custom measurement is not automatically displayed. You must also do the following:
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Parameters |
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
<cnum> |
Any existing channel number. If unspecified, value is set to 1. |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
<Mname> |
Name of the measurement. Any non-empty, unique string, enclosed in quotes. |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
<type> |
(string) - Choose from the following (click or scroll down to view valid <params> for each type) |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
[param] |
(variant) Measurement names to create:
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Examples |
CALC:CUST:DEF 'My VC21', 'Vector Mixer/Converter','S22' calculate2:custom:define 'MyNF', 'NoiseFigure', 'NF' |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Query Syntax |
Not applicable |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
No |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Not applicable |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
Applicable Models: All (Write-only) Changes the selected custom measurement to a different parameter. This is dependent upon the configurations and options. See an example using this command for a VMC and SMC measurement |
|
|
Parameters |
|
|
<cnum> |
Channel of the custom measurement to be changed. First, select the measurement using CALC:PAR:SEL. |
|
<param> |
Parameter to change the custom measurement to. Select a parameter that is valid for the type of measurement. Choose from the same arguments as Calc:Cust:Def. |
|
Examples |
SYST:PRES CALC2:CUST:DEF 'My VC21', 'Vector Mixer/Converter' CALC:PAR:SEL 'My VC21' CALC2:CUST:MOD 'S22' |
|
Query Syntax |
Not applicable |
|
No |
|
|
Not applicable |
|