Other System Configuration Topics
|
Note: To prevent premature wear, the VNA does not allow attenuators or other mechanical switches to switch continuously. These mechanical devices are set for the entire channel. When more than one channel is used, and a mechanical device setting is NOT the same for all channels, only the ACTIVE channel is allowed to sweep. All other channels are Blocked - NOT allowed to sweep. Blocked channels will resume sweeping when they are made ACTIVE, or when the conflict is resolved. Press Trigger > Main > Restart to cause ALL channels to sweep once. Then the active channel will resume sweeping continuously. |
The Mechanical Devices dialog shows the settings of all of the switches and attenuators in the VNA. The settings for all active channels are shown side-by-side for easy comparison. This dialog allows you to determine the settings which would cause mechanical devices to switch between states on consecutive sweeps, potentially leading to device wear-out. It also allows you to determine if the conflict can be resolved to enable continuous sweeps on all channels.
The following are the mechanical devices that are potentially shown in the dialog. These components may not appear in your VNA model:
Port 1 through Port 4 Bypass Switches
Port 1 through Port 4 Source Attenuator settings
Receiver A through Receiver R Attenuator settings
Port 1 Noise Tuner Switch and Port 2 Noise Receiver Switch
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
|
Remote commands SCPI: SENSe<cnum>:SWEep:BLOCked? COM: IsBlocked Property |
|
|
See Mechanical Devices Overview (scroll up) The devices that appear in the table depend on the VNA model and options. > Yellow highlighted cell indicates the Active channel. Blue highlighted cells indicate the following:
To modify entries in the table, click a cell. When a selection is changed, the new setting is applied immediately. If Port Power is coupled, a dialog prompts if coupling should be turned OFF. Limitations
Copy Active Available ONLY when there is a conflict which causes at least one channel to be Blocked. When clicked, the mechanical device settings of the Active channel are copied to the Blocked channels. A warning message appears to remind you that power to one or more channels may be increased. Exception: When one or more Noise channels are present, then the settings of the two Noise switches are be determined by the lowest-numbered Noise channel if none are the active channel. Trigger Launches the Trigger dialog box. OK Closes the dialog box. Cancel Does not apply changes that were made, and closes the dialog box.
|