|
Important Note: Connecting your Mixer/Converter DUT to the VNA. RF and IF terminology is NOT used in this topic because the VNA does not know how your DUT is labeled or how it will be used. Instead, the general terms INPUT and OUTPUT are used to describe the following VNA behavior:
|
SettingsFrequency Format Select Start/Stop (Swept) or Fixed. For Linear sweep type, at least one of these must be fixed. For CW or Power, ALL must be Fixed. Frequencies Enter the frequency values for each of the Mixer/Converter ports.
Calc buttons Calculates frequency settings based on your other mixer settings. For example, enter the Input frequency range and LO1 frequency range, then press Calc Output. The VNA will calculate and display the Output frequencies. Input > LO or IF1>LO2 Removes ambiguity when using a Calc button to determine the INPUT frequency. These check boxes are used ONLY when all 3 of the following conditions are TRUE:
Rules for Configuring a MixerA Red message across the bottom of the dialog indicates that one or more of the following settings are invalid:
Apply Applies the settings for your mixer/converter test setup to the measurement. The mixer setup dialog box remains OPEN. OK Applies the settings for your mixer/converter test setup to the measurement. The mixer setup dialog box CLOSES. Cancel Closes the mixer setup dialog box and does NOT apply the settings. See AlsoHow to measure a DUT with an Embedded LO |
|
Converter Stages Select either 1 or 2-stage converters. Hardware ConfigurationAdd Source Click to start the External Device Configuration dialog. Path Configuration This is not available on M9485A. DUT Portsselect VNA ports to connect to the DUT input and output. Note: In M9485A, Only ports 1 to 4 can be set even if your unit has more than 4-port configuration. Fractional Multipliers
The range for the numerator and denominator of a fractional multiplier is from +1 to +10. Negative values are NOT allowed. See Fractional Multiplier examples. LO1 and LO2Select Not controlled to allow an external source to provide a Fixed LO Frequency at all times. Otherwise, select an internal VNA source or External source to be used as the LO. Learn how to Configure an External Device (Source).
|
|
Configures LO Power settings. Power ON (All channels) Check to immediately turn ON or OFF ALL VNA internal RF Sources for all channels. LO1 Power Sets the power level for LO1. LO2 Power Sets the power level for LO2. Swept Power Settings Set the power sweep setting. Path Configuration
|
Use the LO fractional multiplier to replicate the action of the third-harmonic mixer so the VNA can accurately calculate the receiver frequency. The input and LO frequencies are known.

Enter these settings in the Mixer Setup dialog box:
Input Start Freq: 30 GHz
Input Stop Freq: 40 GHz
LO Fixed Freq: 16 GHz
Mixer-Product Selector: - (difference)
LOs: 1
LO fractional multiplier: 3/1
INPUT fractional multiplier: 1/1
Click Calculate Output
Results:
Output Start Freq: 18 GHz
Output Stop Freq: 8 GHz
Use the fractional multipliers to tune the VNA receiver frequency to the second harmonic of the mixer's 14 GHz fundamental output. The input, LO, and output frequencies are known.

Enter these settings in the Mixer Setup dialog box:
Input Start Freq: 4 GHz
Input Stop Freq: 4 GHz
LO Fixed Freq: 10 GHz
Mixer-Product Selector: + (Sum) of the input and LO signals
LOs: 1
INPUT fractional multiplier = 2/1
LO fractional multiplier = 2/1
Click Calculate Output
Results:
Output Start Freq: 28 GHz
Output Stop Freq: 28 GHz
Use the LO fractional multiplier to replicate the action of the divide-by-two mechanism inside the mixer package. Having done this, the VNA can accurately calculate the receiver frequency. The input and LO frequencies are known.

Enter these settings in the Mixer Setup dialog box:
Input Start Freq: 45 MHz
Input Stop Freq: 50 MHz
LO Fixed Freq: 670 MHz
Mixer-Product Selector: + (Sum) of the input and LO signals
LOs: 1
INPUT fractional multiplier = 1/1
LO fractional multiplier = 1/2
Click Calculate Output
Results:
Output Start Freq: 380 MHz
Output Stop Freq: 385 MHz
Last Modified:
|
18-May-2016 |
First Release |