VNA Preferences


VNA preferences are settings that survive a Preset or VNA Shutdown. VNA Preferences are listed on this page with links to locations that provide more information.

How to set VNA Preferences

Using Hardkey/SoftTab/Softkey

  1. Press System > System Settings > Preferences....

 

Preferences Dialog Box Help  

VNA Preferences survive a Preset and a system reboot.

A checked box makes the following statements true unless stated otherwise.

Avg: On PRESET set two-point Group Delay Aperture - Group delay aperture set to 2 points. Learn more.

Avg: On PRESET set two-point Group Delay Aperture (default) - Group delay aperture is set to 11 points.

Cal: Always use Internal Trigger during cal - Only use Internal Trigger source

Cal: Always use Internal Trigger during cal (default) -use the other Trigger source

This setting only affects calibrations performed using SCPI. Cals performed from the User Interface ALWAYS offer a choice to save to a named Cal Set.

Cal: (SCPI only) Auto-save to User Cal Set - Always automatically save completed calibrations to an auto-named User Cal Set. Caution: This can cause a lot of save User Cal Sets. Learn more.

Cal: (SCPI only) Auto-save to User Cal Set (default) - Save completed calibrations to Cal Registers to default, instead of User Cal Sets.

The following message appears when both the Cal Set choices above and below are selected:

"Cal: Auto-save preferences conflict "

Cal: (SCPI) Auto-save to User Cal Set (above)- or - Cal: (SCPI) Auto-save to current Cal Set (below)

Uncheck one of these.

This setting only affects calibrations performed using SCPI. Cals performed from the User Interface ALWAYS offer a choice to save to a named Cal Set.

Cal: (SCPI) Auto-save to current Cal Set - Always automatically save a completed Cal to the Cal Set that is currently selected on the specified channel, which could be the channel Cal Register. If the channel does not yet have a selected Cal Set, the Cal will be saved to a new User Cal Set with an automatically-generated name.

Cal: (SCPI) Auto-save to current Cal Set (default)- Do NOT automatically save a completed Cal to the Cal Set that is currently selected on the specified channel.

Cal: For Frequency Offset, use Primary frequencies - Use when making mm Wave measurements without a test set.

Cal: For Frequency Offset, use Primary frequencies (default) - Do NOT use when making mm Wave measurements without a test set.

Display: Selected trace changes width briefly - The selected trace changes width briefly in order to improve visibility.

Display: Selected trace changes width briefly (default) - The selected trace does NOT change width briefly.

Display: Selected Trace is wider - The active (selected) trace is always wider.

Display: Selected Trace is wider - The selected trace is the narrow, default size.

Ext Device: De-activate on Preset and Recall (default) - External devices are de-activated when the VNA is Preset or when a Instrument State is recalled.

Ext Device: De-activate on Preset and Recall - External devices remain active when the VNA is Preset or when a Instrument State is recalled.

Learn more about External Devices.

Limit: Draw failed trace segments in red - Failed segments are drawn in red.

Limit: Draw failed trace segments in red (default)- Failed data points (dots) are drawn in red.

Limit: Draw limit lines in red (default) - The limit line is red colors.

Limit: Draw limit lines in red - The limit line color is same as the trace color.

Limit: Test the nearest measurement point - When the stimulus of measurement point is not the same as the limit test point, the nearest limit test point is used for pass/fail judgement.

Limit: Test the nearest measurement point (default) - The pass/fail is judged at only the stimulus of limit test point.

Marker: Coupling controls on|off state of markers - If Coupled Channels is On and a marker is turned on for one trace, the marker with the same marker number will be turned on for all traces coupled to the original trace.

Marker: Coupling controls on|off state of markers - If Coupled Channels is On and a marker is turned on for one trace, no other marker on other traces is affected.

Marker: On Preset, Coupling Method is Channel - Coupling Method is set to "Channel" when preset is selected.

Marker: On Preset, Coupling Method is Channel - Coupling Method is set to "All" when preset is selected.

Marker: On Preset, Coupled Markers is On - Coupled Markers is set to ON when preset is selected.

Marker: On Preset, Coupled Markers is On - Coupled Markers is set to OFF when preset is selected.

Marker: Programming treats Mkr 10 as Reference - A marker programming command that includes 10 as its marker number argument will operate on the Reference Marker (NOT the general-purpose Marker 10).

Marker: Programming treats Mkr 10 as Reference (Default) - A marker programming command that includes 10 as its marker number argument will operate on a general-purpose Marker 10 (NOT the Reference marker).

Marker: Use single marker for marker search (default) - Use one marker for marker search. Sub Marker are displayed and used for Bandwidth, Notch searches. This mode is compatible with the E5071C.

Marker: Use single marker for marker search - Use multi marker for marker search.

Memory: Data Math 8510 Mode - Simulate the Keysight 8510 data processing chain as it pertains to Trace Math and Memory. Learn more.

Memory: Data Math 8510 Mode (default) - Standard VNA data processing chain.

Power: On Preset turn power on (default) - Instrument Preset always turns source power ON.

Power: On Preset turn power on - When the current source power setting is OFF, source power remains OFF after Preset. When the current power setting is ON, source power is turned ON after Preset.

Preset: Confirm preset - When Preset button at hardkey is pressed, VNA firmware immediately preset (Hardkey is required only).

Preset: Confirm preset (defaul) - When Preset > Preset is pressed, VNA firmware immediately preset (Hardkey and Softkey are required).

Recall: Softkey order is most recently used - Recall softkey order which is most recently used.

Recall: Softkey order is most recently used (default) - Do NOT recall softkey order which is most recently used.

Scale: On Preset Couple scale to Window - Scale coupling is set to Window when Preset.

Scale: On Preset Couple scale to Window (default) - Scale coupling is set to Off by default when Preset.

System: Enable sound (default) - Instrument speaker turns ON.

System: Enable sound - Instrument speaker turns OFF.

System: On VNA Start-up Run Self Tests (default) -  Module self tests and connection checks are executed at start up

System: On VNA Start-up Run Self Tests  -  Module self tests and connection checks are NOT executed at start up

System: Use keyboard to navigate softkeys - Enable the keyboard to browse the softkeys.

System: Use keyboard to navigate softkeys (default) - Disable the keyboard to browse the softkeys.

 

The More buttons launch dialogs that contain predefined preferences:

Data Saves...

Define Data Saves - While not explicitly called Preferences, all of these settings survive a shutdown. Learn more.

Power Limit...

Offsets and Limits - Sets Power Limits and Offsets. Learn more.

Transparency...

Dialog Transparency - Some VNA dialogs can be viewed in various levels of transparency. Learn more.

User Preset...

User Preset - Specify the Instrument State file that the VNA will use when Preset. Learn more.

Page Setup...

Page Setup - Standard printer settings (Paper, Orientation, Window, Channel Settings Table and Trace Attributes Table) do NOT survive a VNA shutdown.

All other settings DO survive a VNA shutdown. Learn more.

Disp Colors...

Display Colors - Sets VNA display items to custom colors. Learn more.

Print Colors...

Print Colors - Sets VNA print items to custom colors. Learn more.

 

Although they are called preferences, the following settings do NOT survive a VNA shutdown.

Calibration

UI Setting

Perform orientation of the ECal module during calibration?

ECal Wizard

Specify ECal port mapping when orientation is OFF

ECal Wizard

Show or hide custom Cal Windows during Cal

Cal Window (remote commands only)


Last Modified:

18-May-2016

First Release