Controls the Aperture setting used to make Group Delay measurements.
|
CALCulate:MEASure:GDELay |
Click on a Red keyword to view the command details.
See Also
Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more.
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets group delay aperture using a fixed frequency range. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<value> |
Frequency range (in Hz) to use for the aperture setting. Choose between the equivalent of two data points and the channel frequency span. |
|
Examples |
CALC:GDEL:FREQ 1E6 |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:GDELay:FREQuency? |
|
Return Type |
Numeric |
|
Frequency range that equates to 11 points. This can be changed to two points with a preference setting. |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets group delay aperture using a percent of the channel frequency span. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<value> |
Percent of frequency span to use for the aperture setting. Choose between the equivalent of two data points and 100 percent of the channel frequency span. |
|
Examples |
'set to 25 percent of the channel frequency span CALC:GDEL:PERC 25 |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:GDELay:PERCent? |
|
Return Type |
Numeric |
|
Percent of frequency span that equates to 11 points. This can be changed to two points with a preference setting. |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets group delay aperture using a fixed number of data points. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<value> |
Number of data points to use for the aperture setting. Choose between two points and the number of points in the channel. |
|
Examples |
'set to 25 data points CALC:MEAS:GDEL:POIN 25 |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:GDELay:POINts? |
|
Return Type |
Numeric |
|
11 points. This can be changed to two points with a preference setting. |
|
Last modified:
|
18-May-2016 |
First Release |