Controls the limit segments used for Pass/Fail testing.
|
CALCulate:MEASure:LIMit: | DELete DISPlay | [STATe] SEGMent | AMPLitude | STARt | STOP | STIMulus | STARt | STOP | TYPE SOUNd | [STATe] REPort | ALL? | [DATA]? | POINts? CALCulate:MEASure:BLIMit: DISPlay | MARKer | STATe | BWIDth REPort | DATA CALCulate:MEASure:RLIMit: DISPlay | LINE | STATe | RIPPle | SELect | TYPE | STATe |
Click on a Red keyword to view the command details.
See Also
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets data for limit segments. |
|||||||||||
|
Parameters |
|
||||||||||
|
<cnum> |
Channel number of the measurement for which limit lines are to be set. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
||||||||||
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
||||||||||
|
<block> |
Data for all limit segments in REAL,64 format. The following is the data format for 1 segment:
|
||||||||||
|
Examples |
The following writes three max limit segments for a bandpass filter. CALC:MEAS:LIM:DATA 1,3e5,4e9,-60,0,1,4e9,7.5e9,0,0,1,7.5e9,9e9,0,-30 |
||||||||||
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:DATA? |
||||||||||
|
Return Type |
Depends on FORM:DATA - All 100 predefined limit segments are returned. |
||||||||||
|
100 limit segments - all values set to 0 |
|||||||||||
Applicable Models: E5080A, M9485A
|
(Write-only) Deletes all limit line data for the selected measurement on the specified channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
Examples |
CALC:MEAS:LIM:DATA:DEL |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns ON or OFF the display of limit segments (if the data trace is turned ON). |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<bool> |
Select limit segments from the following: ON or 1 - Turns the display of limit segments ON. |
|
Examples |
CALC:MEAS:LIM:DISP:STAT ON |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:DISPlay[:STATe]? |
|
Return Type |
Boolean |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-only) Reads the Pass/Fail status of the limit line test. Returns 1 (Fail) if any data point fails for any limit segment. Limit display (CALC:MEAS:LIM:DISP) does NOT have to be ON. Notes: When the limit test is set to OFF, False or OFF is always read out. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
Examples |
CALC:MEAS:LIM:FAIL? |
|
Return Type |
Boolean
|
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the start (beginning) of the Y-axis amplitude (response) value. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<snum> |
Segment number; if unspecified, value is set to 1. |
|
<num> |
Choose any number between: -500 and 500. Display value is limited to the Maximum and Minimum displayed Y-axis values. |
|
Examples |
CALC:MEAS:LIM:SEGM1:AMPL:STAR 10 |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>AMPLitude:STARt? |
|
Return Type |
Numeric |
|
0 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the stop (end) of the Y-axis amplitude (response) value. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<snum> |
Segment number; if unspecified, value is set to 1. |
|
<num> |
Choose any number between: -500 and 500. Display value is limited to the Maximum and Minimum displayed Y-axis values. |
|
Examples |
CALC:MEAS:LIM:SEGM1:AMPL:STOP 10 |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>AMPLitude:STOP? |
|
Return Type |
Numeric |
|
0 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the start (beginning) of the X-axis stimulus value. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<snum> |
Segment number; if unspecified, value is set to 1. |
|
<num> |
Choose any number within the X-axis span of the analyzer. |
|
Examples |
CALC:MEAS:LIM:SEGM1:STIM:STAR 10 |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:SEGMent<snum>STIMulus:STARt? |
|
Return Type |
Numeric |
|
0 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the stop (end) of the X-axis stimulus value. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<snum> |
Segment number; if unspecified, value is set to 1. |
|
<num> |
Choose any number within the X-axis span of the analyzer. |
|
Examples |
CALC:MEAS:LIM:SEGM1:AMPL:STOP 10 |
|
Query Syntax |
CALCulate<cnum>:LIMit:SEGMent<snum>STIMulus:STOP? |
|
Return Type |
Numeric |
|
0 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets the type of limit segment. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<snum> |
Segment number. Choose any number between: 1 and 100 |
|
<char> |
Choose from: LMIN - a MIN limit segment. Any response data below the MIN value will fail. OFF - the limit segment (display and testing) is turned OFF. |
|
Examples |
CALC:MEAS:LIM:SEGM:TYPE LMIN |
|
Query Syntax |
CALCulate<cnum>:measure2:LIMit:SEGMent<snum>:TYPE | TYPe ? |
|
Return Type |
Character |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns limit testing fail sound ON or OFF. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<bool> |
ON or 1 - Turns limit testing ON. |
|
Examples |
CALC:MEAS:LIM:SOUN ON |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:SOUNd[:STATe]? |
|
Return Type |
Boolean |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-only) Reads the bandwidth test results (stimulus value, limit test result, upper limit value and lower limit value of all measurement points), for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<block> |
Depends on FORM:DATA If the number of the measurement points is N, <Block> = <first stimulus>,<test result>,<upper limit>,<lower limit>, …, <Nth stimulus>,<test result>,<upper limit>,<lower limit> Where <test result>= -1: No limit, 0:Fail, 1:Pass |
|
Examples |
CALC:MEAS:LIM:REP:ALL? |
|
Return Type |
Variant |
|
Depend on the preset status |
|
Applicable Models: E5080A, M9485A
|
(Read-only) Reads the stimulus values (frequency, power level or time) at all the measurement points that failed the limit test, for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<block> |
Depends on FORM:DATA If the number of the measurement points that failed the limit test is N, <block>=<First failed stimulus>, ..., <Nth failed stimulus>. |
|
Examples |
CALC:MEAS:LIM:REP:DATA? |
|
Return Type |
Numeric |
|
9.91E37 |
|
Applicable Models: E5080A, M9485A
|
(Read-only) Reads the number of the measurement points that failed the limit test, for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
Examples |
CALC:MEAS:LIM:REP:POIN? |
|
Query Syntax |
Numeric |
|
0 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns limit segment testing ON or OFF.
|
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<mnum> |
Measurement number for each measurement. There must be a selected measurement on the trace. If unspecified, <mnum> is set to 1. |
|
<bool> |
ON or 1 - Turns limit testing ON. |
|
Examples |
CALC:MEAS:LIM:STAT ON |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:LIMit:STATe? |
|
Return Type |
Boolean |
|
OFF or 0 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns ON/OFF the bandwidth value display of the bandwidth test, for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<bool> |
ON or 1 - Turns limit testing ON. |
|
Examples |
CALC:BLIM:DISP:MARK:STAT ON |
|
Query Syntax |
CALCulate<cnum>:BLIMit:DISPLay:BWIDth:STATe? |
|
Return Type |
Boolean |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets bandwidth threshold value (attenuation from the peak) of the bandwidth test. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<value> |
Bandwidth N dB points |
|
Examples |
CALC:BLIM:DISP:BWID:THR 5 |
|
Query Syntax |
CALCulate<cnum>:BLIMit:DISPLay:BWIDth:THReshold? |
|
Return Type |
Numeric |
|
3 |
|
Applicable Models: E5080A, M9485A
|
(Read-only) Get the bandwidth limit test results, for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<bool> |
Boolean
|
|
Examples |
CALC:BLIM:FAIL? |
|
Query Syntax |
CALCulate<cnum>:BLIMit:FAIL? |
|
Return Type |
Boolean |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets/gets the upper limit value of the bandwidth test, for the selected channel). |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<max> |
Maximum bandwidth |
|
Examples |
CALC:BLIM:MAX 1E6 |
|
Query Syntax |
CALCulate<cnum>:BLIMit:MAXimum? |
|
Return Type |
Numeric |
|
|
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets or returns the lower limit value of the bandwidth test, for the selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<Minl> |
Minimum bandwidth |
|
Examples |
CALC:BLIM:MIN 1E6 |
|
Query Syntax |
CALCulate<cnum>:BLIMit:MINimum? |
|
Return Type |
Numeric |
|
|
|
Applicable Models: E5080A, M9485A
|
(Read-only) Read the bandwidth value of the bandwidth test, for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<data>> |
|
|
Examples |
CALC:BLIM:REP:DATA? |
|
Query Syntax |
CALCulate<cnum>:BLIMit:REPort:DATA? |
|
Return Type |
Variant |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns ON/OFF the bandwidth test function, for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<bool> |
ON or 1 - Turns limit testing ON. |
|
Examples |
CALC:MEAS:LIM:STAT ON |
|
Query Syntax |
CALCulate<cnum>:BLIMit:DIPLay:MARKer:STATe? |
|
Return Type |
Boolean |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets or returns the ripple limit table for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<data> |
Indicates the array data (for ripple line) of 1 + Num (number of limit lines)* 4. Where n is an integer between 1 and Num.
Specify an integer 0 to 1 as follows. 0: OFF 1: ON
The index of the array starts from 0. |
|
Examples |
CALC:RLIM:DATA |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:RLIMit:DATA? |
|
Return Type |
Variant type Array |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns ON/OFF the ripple limit line display, for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<bool> |
ON or 1 - Turns limit testing ON. |
|
Examples |
CALC:RLIM:DISP:LINE:STAT ON |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:RLIMit:DISPLay:LINE:STATe? |
|
Return Type |
Boolean |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets or gets the ripple limit band for ripple value display for selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<band> |
1 to 12 |
|
Examples |
CALC:RLIM:DISP:RIPP:SEL calculate2:rlimit:display:ripple:select |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:RLIMit:DISPlay:SELect? |
|
Return Type |
Numeric |
|
1 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets/gets the display type of ripple value for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<typ> |
Select from the following:
|
|
Examples |
CALC:RLIM:DISP:TYPE |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:RLIMit:DISPLay:TYPE? |
|
Return Type |
Boolean |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns ON/OFF the ripple test function for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<bool> |
ON or 1 - Turns limit testing ON. |
|
Examples |
CALC:RLIM:DISP:RIPP:STAT ON |
|
Query Syntax |
CALCulate<cnum>:RIMit:DISPlay:STATe? |
|
Return Type |
Boolean |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-only) Read the ripple test result for the active trace. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<bool> |
Boolean
|
|
Examples |
CALC:RLIM:FAIL? |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:RLIMit:FAIL? |
|
Return Type |
Boolean |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-only) Reads the ripple value of the ripple test for the active trace. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<data> |
{numeric 1} ... {numeric NOP×3+1}<newline><^END> NOP is the number of measurement points.
|
|
Examples |
CALC:RLIM:REP:DATA? calculate2:rlimit:report:data? |
|
Query Syntax |
CALCulate<cnum>:MEASure<mnum>:RLIMit:REPort:DATA? |
|
Return Type |
Variant |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Turns ON/OFF the ripple test function for the active trace of selected channel. |
|
|
Parameters |
|
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
|
<bool> |
ON (or 1) - turns limit testing ON. |
|
Examples |
CALC:RLIM:STAT ON |
|
Query Syntax |
CALCulate<cnum>:RLIMit:STATe? |
|
Return Type |
Boolean |
|
OFF |
|
Last modified:
|
18-May-2016 |
First Release |