Configures and makes settings for an external Power Meter as Receiver.
|
SYSTem:CONFigure:EDEVice:PMAR | FLIMit | FMAXimum | FMINimum | READing: | COUNt | SENSor | TABLe: | CFAC: | DATA | LOSS: | DATA | STATe | RFACtor | ZERO |
Click on a blue keyword to view the command details.
Learn about: Configure a Power Meter As Receiver
See root SYST:CONF:EDEV commands
Learn about Configure and External Device
SYST:PREF:ITEM:EDEV:DPOL - Determines whether External Devices remain activated or are de-activated when the VNA is Preset or when a Instrument State is recalled.
Applicable Models: E5080A, M9485A
|
(Write-only) Performs a calibration of the power sensor. Calibration usually involves connecting the power sensor to the meter's 1 mW reference.
This command is always synchronous, so *OPC? is the only way to determine that the operation is complete. Set an I/O timeout of at least 20 seconds. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
Examples |
SYST:CONF:EDEV:PMAR:CAL "myDevice" system:configure:edevice:pmar:calibrate "myDevice" |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Enable or disable the power meter min and max frequencies. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
<value> |
Boolean. State of min and max frequency. Choose from: OFF or 0 - Min and max frequencies disabled. ON or 1 - Min and max frequencies enabled. |
|
Examples |
SYST:CONF:EDEV:PMAR:FLIM "myDevice", 0 system:configure:edevice:pmar:flimit "myDevice", ON See example program |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:PMAR:FLIMit? <name> |
|
Return Type |
Boolean |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Set and return the maximum frequency of the power meter. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
<value> |
Numeric - Max frequency in Hz. |
|
Examples |
SYST:CONF:EDEV:PMAR:FMAX "myDevice", 1e10 system:configure:edevice:pmar:fmaximum "myDevice", 3e9 See example program |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:PMAR:FMAXimum? <name> |
|
Return Type |
Numeric |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Set and return the minimum frequency of the power meter. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
<value> |
Numeric - Min frequency in Hz. |
|
Examples |
SYST:CONF:EDEV:PMAR:FMIN "myDevice", 1e10 system:configure:edevice:pmar:fminumum "myDevice", 3e9 See example program |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:PMAR:FMAXimum? <name> |
|
Return Type |
Numeric |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) This command, along with SYST:CONF:EDEV:PMAR:READ:NTOL, allows for settling of the power sensor READINGS. Set and return the maximum number of power readings that are taken at each stimulus point to allow for measurement settling. Each reading is averaged with the previous readings at that stimulus point. When this average meets the Average:NTOLerance value or this number of readings has been made, the average is returned as the valid reading. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
<value> |
Number of readings. Choose a value between 1 and 25 |
|
Examples |
SYST:CONF:EDEV:PMAR:READ:COUN "myDevice", 20 system:configure:edevice:pmar:reading:count "myDevice", 10 See example program |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:PMAR:READing:COUNt? <name> |
|
Return Type |
Numeric |
|
3 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) This command, along with SYST:CONF:EDEV:PMAR:READ:COUN, allows for settling of the power sensor READINGS. Each power reading is averaged with the previous readings at each stimulus point. When the average meets this nominal tolerance value, or the max number of readings has been made, the average is returned as the valid reading. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
<value> |
Power measurement settling tolerance value in dB. Choose any number between 0 and 5. |
|
Examples |
SYST:CONF:EDEV:PMAR:READ:NTOL "myDevice", .5 system:configure:edevice:pmar:reading:ntolerance "myDevice",.01 See example program |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:PMAR:READing:NTOLerance? <name> |
|
Return Type |
Numeric |
|
.05 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and returns the power sensor channel (1 or 2) to be used. This performs the same function as the Use this sensor only checkbox. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
<value> |
Power Meter channel. 1 - Channel A 2 - Channel B |
|
Examples |
SYST:CONF:EDEV:PMAR:SENS "myDevice",2 system:configure:edevice:pmar:sensor "myDevice",1 See example program |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:PMAR:SENSor? <name> |
|
Return Type |
Numeric |
|
1 |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and returns the cal factor data for the power sensor. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
<value>[,value] |
Cal factor data in percent. For each frequency used with SYST:CONF:EDEV:PMAR:TABL:CFAC:FREQ, enter a cal factor number between 1 and 100. |
|
Examples |
SYST:CONF:EDEV:PMAR:TABL:CFAC:DATA "myDevice", 98,99,99 system:configure:edevice:pmar:table:cfac:data "myDevice", 97,97,97 See example program |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:PMAR:TABLe:CFAC:DATA? <name> |
|
Return Type |
Numeric - one number per table segment. |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and returns the cal factor frequencies for the power sensor. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
<value>[,value] |
Cal factor frequencies in Hz. |
|
Examples |
SYST:CONF:EDEV:PMAR:TABL:CFAC:FREQ "myDevice", 1e7,1e8,1e9 system:configure:edevice:pmar:table:cfac:frequency "myDevice", 5e7,5e8,5e9 See example program |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:PMAR:TABLe:CFAC:FREQuency?<name> |
|
Return Type |
Numeric - one number per table segment. |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and returns the power loss data for the power sensor. Each table can contain up to 9999 segments. Values can also be loaded using the Characterize Adapter macro. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
<value>[,value] |
Loss data in dB. POSITIVE values in dB are interpreted as LOSS. To compensate for gain, use negative values. For each frequency used with SYST:CONF:EDEV:PMAR:TABL:LOSS:FREQ, enter a cal factor number between 1 and 100. |
|
Examples |
SYST:CONF:EDEV:PMAR:TABL:LOSS:DATA "myDevice",.01,.02,.03 system:configure:edevice:pmar:table:loss:data "myDevice", .04,.05,.06 See example program |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:PMAR:TABLe:CFAC:DATA? <name> |
|
Return Type |
Numeric - one number per table segment. |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and returns frequencies for the power loss data. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
<value>[,value] |
Power Loss frequencies in Hz. |
|
Examples |
SYST:CONF:EDEV:PMAR:TABL:LOSS:FREQ "myDevice",1e7,1e8,1e9 system:configure:edevice:pmar:table:loss:frequency "myDevice",5e7,5e8,5e9 See example program |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:PMAR:TABLe:LOSS:FREQuency? <name> |
|
Return Type |
Numeric - one number per table segment. |
|
Not Applicable |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and returns whether to use the power loss table. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
<value> |
Boolean. State of the power loss table. Choose from: OFF or 0 - Power loss table not used. ON or 1 - Power loss table used. |
|
Examples |
SYST:CONF:EDEV:PMAR:TABL:LOSS:STAT "myDevice",1 system:configure:edevice:pmar:table:loss:state "myDevice",1 See example program |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:PMAR:TABLe:LOSS:STATe? <name> |
|
Return Type |
Boolean |
|
OFF |
|
Applicable Models: E5080A, M9485A
|
(Read-Write) Sets and returns the reference cal factor for the power sensor. Note: If the sensor connected to the power meter contains cal factors in EPROM (such as the Keysight E-series power sensors), those will be the cal factors used. The reference cal factor value associated with this command, and any cal factors entered into the VNA for that sensor channel, will not be used. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
<value> |
Reference cal factor in percent. Choose any number between 1 and 150. |
|
Examples |
SYST:CONF:EDEV:PMAR:TABL:RFAC "myDevice", 1 system:configure:edevice:pmar:table:rfactor "myDevice", 1 See example program |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:PMAR:TABLe:RFACtor? <name> |
|
Return Type |
Numeric |
|
100 |
|
Applicable Models: E5080A, M9485A
|
(Write-only) Performs a zeroing of the PMAR device. This command is always synchronous, so *OPC? is the only way to determine that the operation is complete. Set an I/O timeout of at least 20 seconds. Keysight P-Series sensors do ONLY Internal zeroing. These, and Keysight USB power sensors when Internal is selected, do NOT require disconnecting from the measurement path before zeroing. All other Keysight sensors do ONLY External zeroing. |
|
|
Parameters |
|
|
<name> |
String - Name of the power meter. |
|
[,SYNC,<value>] |
Optional argument for use with power sensors that support both internal and external types of zeroing such as Keysight USB power sensors. Choose from: SYNC,INTernal - Internal zeroing. Power is automatically removed from the sensor input before zeroing occurs (Default setting). SYNC,EXTernal - External zeroing. First remove the sensor input, then send this command. External zeroing is recommended for powers below -30 dBm with the U2000-Series sensors (-20 dBm for the H models). |
|
Examples |
SYST:CONF:EDEV:PMAR:ZERO "myDevice" system:configure:edevice:pmar:zero "myDevice",sync,internal |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
Last Modified:
|
16-Mar-2015 |
First Release |