Configures and makes settings for an external Keysight 81110A Pulse Generator.
|
SYST:CONF:EDEVice:PULSe | CHAN | HAMP | LAMP | LIMP | MMODe | SIMP |
Click on a blue keyword to view the command details.
Root SYST:CONF:EDEV commands
Learn about: Configure an External Pulse Generator
Learn about Configure and External Device
SYST:PREF:ITEM:EDEV:DPOL - Determines whether External Devices remain activated or are de-activated when the VNA is Preset or when a Instrument State is recalled.
Applicable Models: M9485A
|
(Read-Write) Sets and returns the output channel of the pulse generator. |
|
|
Parameters |
|
|
<name> |
String - Name of the external pulse generator. |
|
<value> |
Pulse Generator output port. Choose from 1 or 2. |
|
Examples |
SYST:CONF:EDEV:PULS:CHAN "81110",1 system:configure:edevice:pulse:chan "myPG",2 |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:DC:PULSe:CHAN? <name> |
|
Return Type |
Numeric |
|
1 |
|
Applicable Models: M9485A
|
(Read-Write) Sets and returns the High amplitude (voltage) of the pulse generator. |
|
|
Parameters |
|
|
<name> |
String - Name of the external pulse generator. |
|
<value> |
Pulse Generator high amplitude voltage. |
|
Examples |
SYST:CONF:EDEV:PULS:HAMP "81110",3 system:configure:edevice:pulse:HAMP "myPG",4 |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:DC:PULSe:HAMP? <name> |
|
Return Type |
Numeric |
|
5 |
|
Applicable Models: M9485A
|
(Write-only) Adds an external device to the list of configured devices. This is the same as pressing New on the Select an external device dialog. Upon creation, all settings on the new device are set to the defaults. The device is not active until set using SYST:CONF:EDEV:STAT |
|
|
Parameters |
|
|
<name> |
String - Model and type of the external device. To see a list of configured external devices, use SYST:CONF:EDEV:CAT? |
|
Examples |
SYST:CONF:EDEV:ADD "myDevice" system:configure:edevice:add "myDevice" |
|
Query Syntax |
Not Applicable |
|
Not Applicable |
|
|
(Read-Write) Pulse Generator low amplitude voltage. |
|
|
Parameters |
|
|
<name> |
String - Name of the external pulse generator. |
|
<value> |
Pulse Generator low amplitude voltage. |
|
Examples |
SYST:CONF:EDEV:PULS:LAMP "81110",.2 system:configure:edevice:pulse:lamp "myPG",1 |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:DC:PULSe:LAMP? <name> |
|
Return Type |
Numeric |
|
0 |
|
Applicable Models: M9485A
|
(Read-Write) Sets and returns the load impedance of the pulse generator. |
|
|
Parameters |
|
|
<name> |
String - Name of the external pulse generator. |
|
<value> |
Pulse generator load impedance. |
|
Examples |
SYST:CONF:EDEV:PULS:LIMP "81110",52 system:configure:edevice:pulse:limp "myPG",49 |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:DC:PULSe:LIMP? <name> |
|
Return Type |
Numeric |
|
50 |
|
Applicable Models: M9485A
|
(Read-Write) Sets and returns the Master (On/Off) setting of the external pulse generator. The ON setting allows the external pulse generator to set the master clock frequency for the other pulse generators. |
|
|
Parameters |
|
|
<name> |
String - Name of the external pulse generator. |
|
<bool> |
Master setting. Choose from: ON or 1 - Use the external pulse generator becomes the master clock frequency. OFF or 0 - Use the internal pulse generator as the master clock frequency. |
|
Examples |
SYST:CONF:EDEV:PULS:MMOD "81110",OFF system:configure:edevice:pulse:mmode "myPG",1 |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:DC:PULSe:MMODe? <name> |
|
Return Type |
Boolean |
|
OFF or 0 |
|
Applicable Models: M9485A
|
(Read-Write) Sets and returns the source impedance of the pulse generator. |
|
|
Parameters |
|
|
<name> |
String - Name of the external pulse generator. |
|
<value> |
Pulse generator source impedance. |
|
Examples |
SYST:CONF:EDEV:PULS:SIMP "81110",52 system:configure:edevice:pulse:simp "myPG",49 |
|
Query Syntax |
SYSTem:CONFigure:EDEVice:DC:PULSe:SIMP? <name> |
|
Return Type |
Numeric |
|
50 |
|
Last modified:
|
18-May-2016 |
First Release |