Once configured, one or more 81110A External Pulse Generators can be accessed from the VNA Integrated Pulse Application.
Only the 81110A Keysight Pulse Generator is supported.
In this topic:
How to Configure an External Pulse Generator
|
|
|
Using front-panel |
Using a mouse with VNA Menus |
|
|
|
|
|
|
Tip: In the External Device Configuration dialog, you can configure the same 81110A twice; once for each output module. For example:
|
|
System SettingsTime out - Set the amount of time allowed to communicate with the external pulse generator. If communication has not been established before this amount of time has elapsed, a Timeout message will appear. Check connection settings on the External Device dialog. Master Mode - When checked, the 81110A trigger mode is set to Internal. This also causes the 81110A to appear as a selection on Integrated Pulse App, Master Pulse Trigger setting. When selected here and on that dialog, the timing of configured 'slave' pulse generators is controlled by the 81110A pulse generator. Although more than one configured pulse generator can have the Master Mode setting checked, only one pulse generator can be connected to the rear-panel Pulse connections. Learn more about making physical connections. When this setting is cleared, the 81110A trigger mode is set to External and can be configured as a 'slave' pulse generator to the VNA internal pulse generators or another external pulse generator. Output SettingsThe following are 81110A settings made by the VNA. Some settings may not be possible depending on the modules that are installed on the 81110A. Please refer to the 81110A Quick Start Guide for more information. Output - Select an output on the 81110A. High/Low - Set the pulse voltage levels at the 81110A output. Src Imp (Source Impedance) - Source impedance of the pulse generator output. Load Imp (Load Impedance) - The load impedance value expected at the pulse generator output.
|
Once configured, an external pulse generator can be used with the Integrated Pulse App as though it were an internal pulse generator.
N1966A Pulse I/O Adapter. See an enlarged view of the IF Block diagram

An External Pulse Generators can be used for ONE OR MORE of the following pulsed functions within the Integrated Pulse Application.
Trigger the ADC to make receiver measurements
When using an external source modulator (Z5623AH81):
Connect: the 8110A to the Z5623AH81 as shown in the Narrowband Pulse topic.
Setting: On the Pulse Generator Setup dialog, disable (clear) the Internal Pulse Modulators .
When using internal source modulators, the external pulse generator can drive the internal modulators in two ways:
81110A directly to the internal pulse modulators.
Connect: 81110A to RF Pulse Mod In on the N1966A OR rear-panel Pulse I/O connector.
Setting: On the Pulse Generator Setup dialog, set Modulator Drive to "External".
81110A drives internal pulse generators, which drives the internal modulator.
Connect: 81110A to Pulse Sync IN, on the N1966A OR rear-panel Pulse I/O connector.
Settings:
On the Pulse Generator Configuration dialog (above) check Master mode.
On the Pulse Setup dialog, set Master Pulse Trigger to <ext pulse gen name> .
Pulse0 is hardwired to trigger the ADC. However, the following shows how P0 be driven by the external pulse generator timing.
Connect: 81110A to Pulse Sync IN, on the N1966A OR rear-panel Pulse I/O connector.
Settings:
On the Pulse Generator Configuration dialog (above) check Master mode.
On the Pulse Setup dialog, set Master Pulse Trigger to <ext pulse gen name>.
On the Pulse Setup dialog, under Measurement Timing, for the receivers to be triggered, set Pulse Gen to Pulse0. Set unique pulse Width and Delay for the Receiver.
Last modified:
|
16-Sep-2011 |
New topic (A.09.50) |