The Pulse Setup dialogs shown in this topic are now integrated in the VNA firmware and are available with Opt 025.
External pulse generators can be used along with the VNA internal pulse generators. Learn more.
In this topic
App Note: Active-Device Characterization in Pulsed Operation Using the VNA (1408-21)
Connect the cable (p/n M9485-61604) between M9310A Trig 1 connector and one of the four pulse output pins (connectors). See Handler I/O Connector (M9485A) for pulse output pins.
How to start the Pulse Setup dialogTo provide quicker access, use the Setup softkey. Learn how. |
|
Hardkey/SoftTab/Softkey |
|
|
The Basic (upper box) controls allow simple pulse measurements using the default (Autoselect) settings in the Advanced section (lower box) of the dialog. Pulsed measurements are performed in a Standard channel. See Measurement Class. However, several VNA measurement settings are controlled by the Pulse setup, such as sweep type, number of points, and so forth. Pulse MeasurementOff - Source and Receivers are NOT pulsed Standard Pulse - With pulsed RF, the VNA can be configured to sweep in frequency, power sweep, and CW time. Pulse Profile - Pulse profile measurements provides a time domain (CW frequency) view of the pulse envelope. Profiling is performed using a measurement technique that "walks" a narrow receiver "snapshot" across the width of the pulse. This is analogous to using a camera to take many small snapshots of a wide image, then piecing them together to form a single, panoramic view.
Pulse Profile measurement using default settings and R1 receiver.
Pulse TimingPulse Width - Sets the width of the source pulse. See measurement timing to learn how to control the receiver width and delay. Pulse Period The time to make one complete pulse. Pulse Frequency (PRF) The reciprocal of Period (1/ Period). See Internal Pulse Generators to learn more. By default, these settings configure Pulse Gen 1 to drive Source Modulators 1. This can be changed from the Advanced Settings Pulse Generator Setup dialog. -------- Advanced Settings ----------The following settings allow maximum control of a Pulse measurement. PropertiesAutoselect pulse detection method - check to automatically switch between Narrowband and Wideband based on the Pulse Width. In Standard Pulse:
Autoselect IF Path Gain and Loss - For future use. Optimize Pulse Frequency - Automatically selects the Pulse Frequency and Pulse Period. (This is not available for M9485A) Autoselect Profile Sweep Time - In Pulse Profile mode, adjusts the default X-axis start time to zero and the stop time double the Pulse Width. This allows you to see one complete pulse. If unchecked, the Sweep Time will not be changed. . IFBW - Select the IFBW for the measurement.
Measurement TimingSource1 - Used as RF Source Modulation Drive.
Master Pulse Trigger Choose from:
Autoselect Width and Delay - When checked, for Wideband mode and Pulse0, the default setting for the receiver is adjusted to approximately 75% of the source pulse width, with 20% delay. This leaves approximately 5% of the source pulse ON after acquisition is complete. This pulse width is further adjusted after an IFBW is selected. Autoselect Pulse Generators - When checked:
Pulse Generators Click to launch the Pulse Generators Setup dialog. |
|
This dialog is available with Option 025. To see this dialog, press Pulse Gen Setup on the Pulse Setup dialog. Pulse GeneratorsConfigure the Pulse Generators to be used for your measurement. When configured, external pulse generators appear in this list. Learn more. Pulse0 triggers the VNA receivers when Enabled. The Width can NOT be configured. Delay defines the delay between the pulse clock and when the receiver begins to make a measurement. Learn more.
Important: If D + W is greater than P, then undefined VNA behavior results. There is NO error message or warning. P-(D+W) >120 ns should be satisfied. Invert Check to cause the pulse ON time to be active low and OFF be active high. Enable Check to enable individual pulse generators. Trigger Choose from: (When ONE of these is changed, they ALL change. The internal Pulse Generators can NOT be triggered individually).
Frequency - Set the pulse frequency of each generator.
Learn more about the Pulse Generators. Pulsed SourceCheck to enable one or both internal source modulators. Important: When internally modulating the sources, source leveling is automatically set to Open-loop. Modulator Drive Choose the pulse generator to modulate the specified source. Choose from CW (NO pulse), Pulse 1, 2, 3, 4, External. Pulsed Receivers Synchronize ADCs using pulse trigger - Check to enable triggering used to gate the ADC for wideband receiver measurements. This is the same as Pulse0 Enable. The Width can NOT be configured. ADC trigger delay - Set the amount of time to wait before triggering the ADC to begin acquisition. This is the same as Pulse0 Delay. Use Pulse4 output connector to indicate ADC activity - Check to use an oscilloscope connected to Pulse4 pin to display when the ADC is making measurements. Pulse Trigger.. Click to start the Pulse Trigger dialog. |
|
To see this dialog, press Pulse Trigger on the Pulse Generator Setup dialog or select Stimulus, then Trigger from the VNA Menu. Pulse Sync Trigger - SourceSelect Internal or External to provide sync capability for the internal pulse generators.
The PULSE SYNC IN pin provides a configurable trigger signal into the Pulse Generators. Only one set of pulses is emitted when edge triggering is used. The length of time that it takes to emit one set of pulses is the end time of the last enabled pulse (largest of width + delay of all the pulses P0-P4). Level/EdgeSets the edge or level of the trigger signal to which the internal pulse generators will respond when being externally triggered at the PULSE SYNC IN pin. Positive = rising edge; Negative = falling edge. Receiver SynchronizationSynchronize ADCs using pulse trigger - Check to enable triggering used to gate the ADC for wideband receiver measurements. The Width can NOT be configured. ADC trigger delay - Set the amount of time to wait before triggering the ADC to begin acquisition.
|
Setup the External Pulse Generator as an External Device.
To perform a calibration in pulse mode, first configure and apply the pulse parameters (PRF, Pulse Width, Delays, IF gating, and so forth) before calibrating the system. This will ensure the VNA is configured properly during the calibration and measurement.
Turn off the pulse mode when the power calibration is performed with a power sensor.
Last Modified:
|
19-Dec-2013 |
Added Pulse-to-Pulse |
|
11-Apr-2010 |
MX New topic (A.09.20) |