|
|
The following section describes procedures for Windows XP. Refer to the Windows 7 Help and Support to perform equivalent operating system tasks under Windows 7. |
The Microsoft Windows XP operating system provides tools for error checking and defragmenting a hard disk drive (HDD).
If you believe your PXB is having problems:
If the PXB boots successfully, run the error checking and disk defragmenter utilities described below.
If the PXB will not boot successfully, see Recovering from Hard Drive Problems.
However, the error checking and disk defragmenter utilities should be
run routinely, about once a month. These utilities should be run more
frequently if the PXB is unexpectedly shut down.
|
|
When the PXB is shut down unexpectedly or power is removed without first shutting down, large amounts of HDD space are rendered unusable. If shut down in this manner enough times, the PXB could become unstable and no longer work. |
Microsoft's error-checking utility scans the HDD for bad sectors, scans for file system errors to see whether certain files or folders are misplaced, and corrects errors. This error-checking utility is also known as "Check Disk." Use this utility to find and correct HDD errors.
Close all open files.
Click Start, and then click My Computer.
In the My Computer window, right-click the drive you want to run the error-checking utility on, and then click Properties.
In the
Properties
dialog box, click the Tools tab.
Click the Check Now... button under Error-checking.
In the Check Disk
dialog box, select the Scan for and attempt
recovery of bad sectors check box, and then click Start.
The
Checking
Disk
dialog box is displayed.
When the error-checking utility is complete, the following prompt appears: Disk check complete. Click OK to close the dialog box.
If bad sectors are found, choose to fix them.
The error-checking (CHKDSK) utility is also provided as an option on the Agilent Technologies Recovery Options Menu. You can use either the Microsoft Windows or Agilent Technologies error-checking utility on your PXB.
Click Start, Shutdown, Restart.
After the Agilent logo, when Please
select the operating system to start: displays, quickly press the
down arrow on the PXB's front panel or keyboard to select the
Agilent Recovery System.
Press Enter.
To start the error-checking utility, select Option 1
(Run CHKDSK to resolve Disk Issues...) from the
Recovery Options Menu, then
press Enter and follow the prompts.
After running either Error-Checking utility, run the Disk Defragmenter utility to recover HDD space.
Close all open files.
Click Start, and then click My Computer.
In the My Computer window, right-click the drive you want to run the Disk Defragmenter utility on, and then click Properties.
In the
Properties
dialog box, click the Tools tab.
Click the Defragment Now... button under Defragmentation.
The
Disk Defragmenter
window appears. Click the Defragment
button at the bottom of the window to begin the
When the
Operating
System Recovery
Preventing Hard Disk Drive Problems
Recovering from Hard Disk Drive Problems