The hard drive is divided into three partitions:
The C: partition contains the Windows operating system (OS) and the PXB firmware installed by Agilent Technologies. It is an open system wherein the installation of additional software is permitted.
|
|
The installation and use of other software is not warranted, and may interfere with the operation of the PXB firmware. If a PXB repair is ever needed, the Agilent version (OS and PXB firmware) of the C: partition is the only part that is restored by the Agilent Recovery System Procedure. You will need to reload any other software that you have added in the PXB. |
The D: partition is reserved for data storage. The User Accounts that are configured by Agilent Technologies have their My Documents folder mapped to the D: partition. This allows you to back up user-created waveforms or user-defined configurations on an external device to restore the data if you ever need to replace the hard drive.
The E: partition is reserved for Agilent Technologies' use and contains the self test data and the log files of the last self test performed.
|
|
Do not change or overwrite the files on this drive. This could cause your instrument to not meet specification or, in the worst case, stop functioning correctly. Do not use this drive for data storage. |
If you are experiencing problems with your PXB's hard disk drive (HDD),
see Recovering
from Hard Disk Drive Problems. These problems are usually preventable,
and in many cases, recoverable. Following the tips below could save you
from costly HDD repairs.
|
|
The
|
Remove AC power from the PXB only
when the Power LED is yellow (in
Shutdown mode). Removing power while the LED is green may permanently
damage the instrument. The LED will remain yellow for several seconds
after the power cord has been removed. Learn
more about powering the PXB On and Off.
The PXB has been sent from the factory with its HDD set to shut down after three minutes of inactivity. To minimize HDD failures, do not change the HDD Power Option's setting.
These programs recover HDD space that is lost from unexpected power shutdowns. See Error Checking and Disk Defragmenter Utilities.
The PXB does not have antivirus protection installed when shipped. Use
of an antivirus program is strongly recommended if you intend to connect
the instrument to the Internet. The use of a
The PXB is shipped with the latest service packs and critical updates
that were available at the time that the instrument was manufactured.
We recommend that you maintain the latest available protection for your
PXB by automatically accepting and installing the latest critical security
patches from the
Related topics