The hard disk drive (HDD) clicks continuously or is very loud (indications of a mechanical problem).
If you are experiencing problems with your PXB's hard disk drive (HDD), you can use another computer to access the PXB's online documentation and service information by:
Viewing the Documentation DVD that was received with your PXB
Accessing the Agilent website: www.agilent.com/find/PXB
HDD problems are usually preventable (see Preventing Hard Disk Drive Problems), and in many
cases, recoverable.
|
|
Make a note of the current firmware revision installed on your PXB. After a system recovery or after a HDD has been replaced, it is often necessary to update the PXB firmware. If the HDD is replaced, the following data will be lost:
|
Send the PXB into the Agilent Service Center for repair or replace the HDD assembly.
Order a new HDD. (Refer to the Guided Service and Support information for HDD part number.)
If possible, save copies of your programs and the files that you created on a USB memory device, CD ROM, or DVD.
Replace the HDD assembly. (Refer to the Guided Service and Support information for on replacing the hard disk drive.)
Restore the files from your memory device.
|
|
It is important to backup any waveforms or custom configuration data that you want to save on a separate HDD or memory device regularly. |
Preventing
HDD Problems
Operating System Recovery
Recovering from Firmware Problems