ESG/PSG Signal Generator
Output
RF turns the operating
state of the RF signal on or off.
Modulation
turns on or off all active modulation formats that are applied to the
RF output carrier signal of the signal generator.
Signal
Frequency changes
the frequency parameter limits as well as the output frequency of the
signal generator. The signal generator output frequency is:
Signal Generator Output Frequency = Frequency
– Frequency
Offset
Minimum Frequency = 100 kHz + Frequency Offset
Maximum Frequency = SigGen
Max + Frequency Offset
Frequency is also used during the generate correction routine to set
the spectrum analyzer center frequency. Use frequency offset, auto crest
factor, and mirror spectrum if there is a frequency translation between
the signal generator and the spectrum analyzer.
Frequency Offset alters
the visual display on the signal generator and the frequency range limits.
It allows the source frequency display to account for a system with frequency
translation in it. The frequency offset value is also used by the generate
correction function.
The actual output frequency and frequency range limits for the signal
generator are offset by the frequency offset value.
Signal Generator Output Frequency = Frequency
– Frequency
Offset
Minimum Frequency = 100 kHz + Frequency Offset
Maximum Frequency = Signal Generator Max
+ Frequency Offset
Amplitude sets
the signal generator output amplitude. The amplitude value is also used
during the generate correction routine to set the spectrum analyzer reference
level and attenuator.
The actual output amplitude and amplitude range limits are offset by
the amplitude offset:
Signal Generator Output Amplitude = Amplitude
– Amplitude
Offset
Minimum Amplitude = Signal Generator Minimum
+ Amplitude Offset
Maximum Amplitude = Signal Generator Maximum
+ Amplitude Offset
It is not possible to set the maximum amplitude level with the ALC Enable
On.
PSG Maximum = 30 dBm, Maximum with ALC Enable
= On, 25 dBm
ESG Maximum = 25 dBm, Maximum with ALC Enable
= On, 20 dBm
When Attenuator Hold is off, setting the amplitude also sets the ALC
level and the attenuator. The ALC level
and attenuator value are chosen to keep the ALC level at its optimum level.
When the Attenuator Hold is On, the attenuator value is held constant.
Changing the amplitude or ALC level causes the other parameter to change
an equal amount. In general, ignoring amplitude offset, the output amplitude
is:
Amplitude(dBm) = ALC Level(dBm)
– Attenuator Value(dB)
Amplitude Offset applies
an offset to the value and range limits of the signal generator amplitude.
Use this parameter if there is additional gain or loss between the signal
generator and the spectrum analyzer. If there is an amplifier with 10
dB of gain on the output of the signal generator, the amplitude offset
should be set to 10 dB. Now all entries to the amplitude value account
for this external gain. The amplitude offset value
is also used by the generate correction function. The actual output amplitude
of the signal generator is:
Signal Generator Output Amplitude = Amplitude
– Amplitude
Offset
Sample
Clock controls the ESG/PSG's Arb Sample Clock setting. This setting
is coupled with the Playback Sample Rate
setting in the Waveform Setup
and playback N5110B Playback Setup
tables.
I/Q
I/Q turns the
IQ modulation on or off.
Inputs displays
the source of the IQ inputs. This information is taken from the hardware
configuration and is a read-only feature.
Modulation Filter
enables you to select either a 40 MHz lowpass filter
in the I/Q signal path before the IQ modulator or a Through path. The
40 MHz filter helps reduce broadband noise and spurs for signals with
an 80 MHz or less RF bandwidth. This parameter should be set to Through
when using external IQ inputs and signals that have RF bandwidths greater
than 80 MHz. The filter has no affect on the PSG Option 015 wide band
signal path. The modulator filter value is used by the generate correction
function.
Modulation Attenuation Auto determines
the mode of modulation attenuation. When set to On, the instrument uses
a predefined Modulation Attenuation value for best performance. When set
to Off, the instrument uses the value set in the Modulation Attenuation
field.
Modulation Attenuation enables
you to adjust the attenuator to optimize signal performance at the RF
output. The modulator attenuator
is an electronic attenuator in the IQ path before the IQ modulator. When
ALC is on, the RF output amplitude will not change while the attenuator
value is changed until the ALC range is exceeded. The modulator attenuator
value is used by the generate correction function.
|

|
Changing the IQ modulator attenuator
after applying corrections can degrade the image correction. The degradation
occurs because the delay through the two attenuators (one for I and one
for Q) may not remain constant. If this degradation is observed, try changing
the modulator attenuator a few tenths of a decibel (dB) in 0.1 dB steps.
|
I/Q Scaling adjusts
the amplitude of both I and Q outputs while the waveform is playing. Use
this setting to attain better ACP and to optimize dynamic
range without overdriving the I and Q D/A converters.
|

|
I/Q Scaling is preset to 70%. In most
cases, this setting provides good dynamic range without overdriving the
I and Q DACs. Increasing the I/Q scaling value beyond
70% increases the risk of DAC over-range errors. If an error occurs at
the signal generator, reduce the I/Q Scaling value until errors no longer
occur. |
I/Q Adjustments turns
the IQ adjustments on or off.
I Offset
applies a DC offset to the I
signal before the IQ modulator. It can be used to help minimize carrier
leakage or to introduce calibrated impairments.
Q Offset
applies a DC offset to the Q
signal before the IQ modulator. It can be used to help minimize carrier
leakage or to introduce calibrated impairments.
Quadrature Skew
enables you to adjust the phase
angle between the I and Q vectors. When the quadrature
skew is zero, the phase angle is 90 degrees. Positive skew increase the
angle from 90 degrees while negative skew decreases the angle from 90
degrees.
ALC and Attenuation
The RF output power of the signal generator is constantly monitored
and controlled by the automatic leveling control (ALC) circuit. Its purpose
is to hold output power at its desired level in spite of drift due to
temperature and time.
There are some modulation conditions the ALC circuit cannot handle properly
that lead to output level errors. In these conditions, better power level
accuracy can be obtained by turning the ALC off and using power search.
ALC off is useful with pulse modulation when the pulse width is narrower
than two microseconds, and with certain external I/Q
modulation.
Pulse modulation is accomplished using a modulator which precedes the
ALC detector. The ALC must, therefore, measure a pulsed signal, and it
is able to do this if the pulse width exceeds two microseconds. For narrower
pulses, set the ALC to off.
With external I/Q modulation, the ALC loop acts to
hold the average output power of the signal generator constant, in spite
of variations in the I/Q input power (I2
+ Q2). Rapid
variations of (I2
+ Q2) propagate
to the output, while slow variations are removed by the ALC loop, with
a high-pass corner of 1 kHz. If you do not want this high-pass filtering,
set the ALC to off. With ALC off, the I/Q modulation
will be DC-coupled. Using power search, power level accuracy is preserved
if (I2
+ Q2)1/2 = 0.5 Vrms.
ALC
turns the automatic level control
on or off. It is not possible to set the maximum amplitude level with
ALC on.
PSG
Max = 30 dBm, Max with ALC on, 25 dBm
ESG Max = 25 dBm, Max with ALC on, 20 dBm
ALC BW
enables you to
select the ALC loop bandwidth
from the drop-down list . The Auto selection lets the signal generator
select the bandwidth automatically based on the current signal setup.
Attenuator Hold turns
the attenuation hold on or off. When this function is turned on, the attenuator
is locked at its current setting to prevent glitches that can occur when
the attenuator is changed. You can use this function any time you want
to guarantee that there will be no power discontinuity normally associated
with the attenuator switching during power adjustments. When this function
is turned off, the attenuator is in a dynamic state, and setting the amplitude
also sets the ALC level and the attenuator.
Attenuator Setting
sets the value of the output
attenuator. The attenuator value is used by the generate correction function.
The attenuator value can only be set when the Attenuator Hold is on. When
the Attenuator Hold is on, the attenuator value is held constant. Changing
the amplitude or ALC level causes the other parameter to change an equal
amount. The ALC level and attenuator value are
chosen to keep the ALC at its most effective level.
ALC Level
sets the output power level only using the ALC. When the ALC circuit is
on, the output power level is constantly monitored and controlled. When
the ALC circuit is off, the output power level is not controlled. The
ALC level value is used by the generate correction function.
Do Power Search
enables the power search routine. Power search is an internal calibration
routine that improves output power accuracy when the ALC is off. A power
search is recommended for pulse-modulated signals with pulse widths less
than two microseconds.
If you are using external I/Q modulation, the power
search routine assumes that the I/Q input level is
= 0.5 Vrms.
Actual output amplitude will scale directly with
.
Power Search Mode
enables you to select either
manual or auto as the power search mode. With the manual selection, power
search will not run until the Do Power Search button is pressed. When
the selection is auto, power search will run automatically with each change
to the RF frequency or power, and with each change to the AM, burst, pulse,
or I/Q modulation state.
Power Search Reference enables
you to select either fixed CW or a modulated signal
from the drop-down menu when doing a power search. The power search reference
function is not available when ALC is on.
RF During Power Search enables
you to select either normal or minimum to control the output power of
the signal generator during a power search routine. When the selection
is normal, nothing is done to the output power during the power search.
Glitch and power changes may be present during the search. With minimum
selected, the output is protected by putting the attenuator to its maximum
value during the power search.
Marker Routing
ALC Hold enables
you to select a marker for this function. When the specified marker signal
is low, ALC Hold is enabled. With ALC Hold enabled, the output power leveling
does not respond to changes to the signal amplitude. Selecting Off disconnects
all markers from ALC Hold.
ALT Power enables
you to select a marker for the alternate amplitude function. When the
marker signal is low, the alternate amplitude settings configured on the
ESG signal generator are active. Selecting Off disconnects all markers
from the alternate amplitude function.
Burst Pulse Mod
enables you to select a marker for this function. When the marker signal
is high and the marker polarity is positive, the waveform is blanked until
an enabled marker is encountered. When the marker polarity is negative,
the waveform is blanked when it encounters an enabled marker. Selecting
Off disconnects all markers from the Burst Pulse Mod function.
Related Topics
Basic
RF Playback Setup
Waveform Setup
N5110B
Playback Setup