When the sequencing mode is set to On in
Waveform
Setup,
the software displays the Sequence node in the tree view. Click the node
to access the Sequence pane where you can set up previously configured
waveforms to be played in an order specific to your requirements. You
can add and arrange up to 10 waveforms for playback. You can also play
each waveform up to 65,535 times before stepping to the next waveform
and control the four marker states for each waveform.
If you have 1xEV-DO Rev. 0 Forward FTM mode set to On in
Waveform Setup,
these parameters cannot be edited.
Inserts a waveform (WFM) into the sequence. The added waveform is inserted immediately above the selected waveform.
Appends a waveform (WFM) to the bottom of the sequence.
Deletes the selected waveform from the sequence.
Moves the selected waveform up one position in the sequence table.
Moves the selected waveform down one position in the sequence table.
Displays the waveform number. You cannot edit cells in this column.
Displays the waveform name. You cannot edit cells in this column.
Displays the number of sample points. This field is updated after the waveform is generated and cannot be edited. You cannot edit cells in this column.
Range: 1 to 65535
Default: 1
Sets the number of times you want the waveform to play before playing the next waveform. Click the number in this column to highlight the repetitions and enter the number of times you want the waveform to play.
Selections: On, Off
Default: On
Sets the marker state for each marker of each waveform in the sequence.
If you click in the cell, the
icon is displayed.
Click the icon and you may select from either On or Off to set the individual
marker state. The source of each marker is defined when the waveform is
defined in the WFM "N"
pane.