Real Time

WFM "N"

Waveform Name

Marker 3 Source

Comment

Marker 4 Source

Total Sample Points

CCDF

Map

Waveform

Marker 1 Source

 

Marker 2 Source

 

Carrier Configuration Summary Table

This table enables you to view the key parameters for each carrier in the waveform. You can also add or delete carriers using the buttons above the table (see descriptions below). Double-clicking a carrier row activates the setup tables for that carrier.

Opens a Closeddrop-down menu of predefined carrier configuration selections. Double-clicking a configuration replaces the current configuration in the Carrier Configuration Summary Table.  

Opens a Closeddrop-down menu which allows you to add a carrier to the current configuration.

The new carrier is added immediately above the currently highlighted carrier in the Carrier Configuration Summary Table.

Deletes the currently highlighted carrier in the Carrier Configuration Summary Table. You can highlight multiple carriers by holding down the CTRL key while selecting the carriers. You can also use the SHIFT key to select a succession (group) of carriers.

Copies the highlighted carrier and appends it at the bottom of the carrier list.

Waveform Attributes

1. Basic

Waveform Name

Displays the name of the waveform entered in the waveform setup window. It cannot be edited in this cell.

Comment

Allows you to enter an alpha-numeric comment up to 32 characters in length. The comment may be unique for each individual waveform.

Total Sample Points

Displays the number of sample points. This field is updated after the waveform is generated and cannot be edited.

I/Q Map

Selections: Normal, Invert

Default: Normal

Allows you to select a normal or inverted I/Q signal. The icon at the right edge of the entry box displays a drop-down list with all available selections. 

2. Marker

Marker 1 Source

Selections: None, Frame, RF ALC Control, RF Blanking Control, Timing Control, User Defined Bits

Default: Frame

Defines the source of the marker points for Marker 1. Click at the right edge of the cell to display the ClosedMarker Source Selection dialog box from which you can select the marker source.

Select one of the following sources for the marker.

None

Sets all maker points are set to zero (inactive).

Frame

Sets the first five marker bits of the frame to 1, which sets an active marker for the first five waveform samples (waveform points). The signal generator outputs the Marker 1 output from the rear-panel Event 1 output.

RF ALC Control

Activates the automatic leveling control (ALC) function. When enabled, the ALC constantly monitors and controls the RF output power of the signal generator.

The ALC circuit cannot properly handle some modulation conditions, leading to output power level errors. In these conditions, turning the ALC off and using the signal generator power search function can achieve better power level accuracy.

RF Blanking Control

Assigns a specific marker to activate RF blanking. The automatic leveling control (ALC) hold is automatically enabled during output blanking.

RF Blanking Control improves the signal quality when the MAC channel and/or traffic channel are de-activated in a timeslot. It does so by increasing the on/off ratio of the forward link RF bursts.

When RF Blanking Control is enabled, the marker polarity must be set to positive or the wanted RF signal will be blanked, resulting in no RF output from the signal generator.

Timing Control

Sets the marker so that it is generated by the waveform.

IS95/cdma2000 generates the first five waveform samples (waveform points) in the short code cycle. 1xEV-DO generates the half-slot timing.

User Defined Bits

Opens the user Closeddata entry area, which lets you customize the marker signal.

The data entry area contains buttons to import, export, or clear user marker data along with the ability to insert a PN9 sequence as the marker bits. Optionally you can manually insert or delete marker data. To manually insert marker data, simply place the cursor within the data entry area or highlight existing bits, and insert bits. There are three ways to insert marker data:

(The key board shortcuts Ctrl+C and Ctrl+V work for user data entry.)

To delete data, simply place the cursor at the desired location within the data or highlight bits, and delete data. The key board short cut Ctrl+Z also deletes highlighted data.

The maximum number of marker bits for the user data entry area is 2,097,152 which equals 32,768 (1short code data points) * 64 (oversampling ratio). This is also the maximum file size.

The four buttons in the expanded area are:

Import

Loads a user-defined pattern from a selected location. When you select this button, the Open user defined data dialog box appears for navigating to and selecting the desired file. An imported file automatically updates the user data entry area. The software accepts the following file types:

The maximum file size is 2,097,152 bits. If the imported file is larger than bits, the software truncates the bits to conform to the maximum file size. 

Export

Saves the current data pattern, showing in the user data entry area, to a file. When you select this button, a Save user defined data dialog box appears for navigating to the location where you can save the file. The software saves the user data as one of the following selected file types:

Clear

Clears all data showing in the user data entry area.

Insert PN9

Inserts a fixed pattern pseudo-random bit sequence containing 511 bits (29–1) into the user data entry area. The software generates this fixed pattern in accordance with the CCITT recommendation O.153. Repeated clicking of this button adds additional PN9 sequences until the software attains the maximum file size of 2,097,152 bits. The software truncates data in excess of the maximum file size.

To edit the data pattern, insert the cursor at the desired point in the file and click Insert PN9, or enter the information manually using the keyboard keys 1 and 0. The software inserts the data at the cursor position and truncates all data in excess of 2,097,152 bits.

The software lets you create a file larger than it uses for the waveform. When this occurs, the software truncates the excess marker bits. Conversely, if there are not enough marker bits, the software repeats the marker bit pattern until there are enough marker bits to match the Waveform Length cell value.

The signal generator outputs the marker 1 signal from the rear-panel EVENT 1 output. For more information, see the signal generator's User Guide.

Marker 2 Source

Selections: None, Frame, RF ALC Control, RF Blanking Control, Timing Control, User Defined Bits

Default: None

Defines the source of the marker points for Marker 2. Click at the right edge of the cell to display the ClosedMarker Source Selection dialog box from which you can select the marker source.

Select one of the following sources for the marker.

None

Sets all maker points are set to zero (inactive).

Frame

Sets the first five marker bits of the frame to 1, which sets an active marker for the first five waveform samples (waveform points). The signal generator outputs the Marker 1 output from the rear-panel Event 1 output.

RF ALC Control

Activates the automatic leveling control (ALC) function. When enabled, the ALC constantly monitors and controls the RF output power of the signal generator.

The ALC circuit cannot properly handle some modulation conditions, leading to output power level errors. In these conditions, turning the ALC off and using the signal generator power search function can achieve better power level accuracy.

RF Blanking Control

Assigns a specific marker to activate RF blanking. The automatic leveling control (ALC) hold is automatically enabled during output blanking.

RF Blanking Control improves the signal quality when the MAC channel and/or traffic channel are de-activated in a timeslot. It does so by increasing the on/off ratio of the forward link RF bursts.

When RF Blanking Control is enabled, the marker polarity must be set to positive or the wanted RF signal will be blanked, resulting in no RF output from the signal generator.

Timing Control

Sets the marker so that it is generated by the waveform.

IS95/cdma2000 generates the first five waveform samples (waveform points) in the short code cycle. 1xEV-DO generates the half-slot timing.

User Defined Bits

Opens the user Closeddata entry area, which lets you customize the marker signal.

The data entry area contains buttons to import, export, or clear user marker data along with the ability to insert a PN9 sequence as the marker bits. Optionally you can manually insert or delete marker data. To manually insert marker data, simply place the cursor within the data entry area or highlight existing bits, and insert bits. There are three ways to insert marker data:

(The key board shortcuts Ctrl+C and Ctrl+V work for user data entry.)

To delete data, simply place the cursor at the desired location within the data or highlight bits, and delete data. The key board short cut Ctrl+Z also deletes highlighted data.

The maximum number of marker bits for the user data entry area is 2,097,152 which equals 32,768 (1short code data points) * 64 (oversampling ratio). This is also the maximum file size.

The four buttons in the expanded area are:

Import

Loads a user-defined pattern from a selected location. When you select this button, the Open user defined data dialog box appears for navigating to and selecting the desired file. An imported file automatically updates the user data entry area. The software accepts the following file types:

The maximum file size is 2,097,152 bits. If the imported file is larger than bits, the software truncates the bits to conform to the maximum file size. 

Export

Saves the current data pattern, showing in the user data entry area, to a file. When you select this button, a Save user defined data dialog box appears for navigating to the location where you can save the file. The software saves the user data as one of the following selected file types:

Clear

Clears all data showing in the user data entry area.

Insert PN9

Inserts a fixed pattern pseudo-random bit sequence containing 511 bits (29–1) into the user data entry area. The software generates this fixed pattern in accordance with the CCITT recommendation O.153. Repeated clicking of this button adds additional PN9 sequences until the software attains the maximum file size of 2,097,152 bits. The software truncates data in excess of the maximum file size.

To edit the data pattern, insert the cursor at the desired point in the file and click Insert PN9, or enter the information manually using the keyboard keys 1 and 0. The software inserts the data at the cursor position and truncates all data in excess of 2,097,152 bits.

The software lets you create a file larger than it uses for the waveform. When this occurs, the software truncates the excess marker bits. Conversely, if there are not enough marker bits, the software repeats the marker bit pattern until there are enough marker bits to match the Waveform Length cell value.

The signal generator outputs the marker 2 signal from the rear-panel EVENT 2 output. For more information, see the signal generator's User Guide.

Marker 3 Source

Selections: None, Frame, RF ALC Control, RF Blanking Control, Timing Control, User Defined Bits

Default: None

Defines the source of the marker points for Marker 3. Click at the right edge of the cell to display the ClosedMarker Source Selection dialog box from which you can select the marker source.

The signal generator outputs the marker 3 signal from the rear-panel EVENT 3 output. For more information, see the signal generator's User Guide.

When Parameter Optimization in the Signal Generator node is set to Auto, Marker 3 and Marker 4 source selection in the Waveform Setup node and the marker routing selected in the Dual Arb Marker Utilities are overridden.

To manually set Marker 3 and Marker 4 source, the marker routing, or both, set the Parameter Optimization to Off.

Select one of the following sources for the marker.

None

Sets all maker points are set to zero (inactive).

Frame

Sets the first five marker bits of the frame to 1, which sets an active marker for the first five waveform samples (waveform points). The signal generator outputs the Marker 1 output from the rear-panel Event 1 output.

RF ALC Control

Activates the automatic leveling control (ALC) function. When enabled, the ALC constantly monitors and controls the RF output power of the signal generator.

The ALC circuit cannot properly handle some modulation conditions, leading to output power level errors. In these conditions, turning the ALC off and using the signal generator power search function can achieve better power level accuracy.

RF Blanking Control

Assigns a specific marker to activate RF blanking. The automatic leveling control (ALC) hold is automatically enabled during output blanking.

RF Blanking Control improves the signal quality when the MAC channel and/or traffic channel are de-activated in a timeslot. It does so by increasing the on/off ratio of the forward link RF bursts.

When RF Blanking Control is enabled, the marker polarity must be set to positive or the wanted RF signal will be blanked, resulting in no RF output from the signal generator.

Timing Control

Sets the marker so that it is generated by the waveform.

IS95/cdma2000 generates the first five waveform samples (waveform points) in the short code cycle. 1xEV-DO generates the half-slot timing.

User Defined Bits

Opens the user Closeddata entry area, which lets you customize the marker signal.

The data entry area contains buttons to import, export, or clear user marker data along with the ability to insert a PN9 sequence as the marker bits. Optionally you can manually insert or delete marker data. To manually insert marker data, simply place the cursor within the data entry area or highlight existing bits, and insert bits. There are three ways to insert marker data:

(The key board shortcuts Ctrl+C and Ctrl+V work for user data entry.)

To delete data, simply place the cursor at the desired location within the data or highlight bits, and delete data. The key board short cut Ctrl+Z also deletes highlighted data.

The maximum number of marker bits for the user data entry area is 2,097,152 which equals 32,768 (1short code data points) * 64 (oversampling ratio). This is also the maximum file size.

The four buttons in the expanded area are:

Import

Loads a user-defined pattern from a selected location. When you select this button, the Open user defined data dialog box appears for navigating to and selecting the desired file. An imported file automatically updates the user data entry area. The software accepts the following file types:

The maximum file size is 2,097,152 bits. If the imported file is larger than bits, the software truncates the bits to conform to the maximum file size. 

Export

Saves the current data pattern, showing in the user data entry area, to a file. When you select this button, a Save user defined data dialog box appears for navigating to the location where you can save the file. The software saves the user data as one of the following selected file types:

Clear

Clears all data showing in the user data entry area.

Insert PN9

Inserts a fixed pattern pseudo-random bit sequence containing 511 bits (29–1) into the user data entry area. The software generates this fixed pattern in accordance with the CCITT recommendation O.153. Repeated clicking of this button adds additional PN9 sequences until the software attains the maximum file size of 2,097,152 bits. The software truncates data in excess of the maximum file size.

To edit the data pattern, insert the cursor at the desired point in the file and click Insert PN9, or enter the information manually using the keyboard keys 1 and 0. The software inserts the data at the cursor position and truncates all data in excess of 2,097,152 bits.

The software lets you create a file larger than it uses for the waveform. When this occurs, the software truncates the excess marker bits. Conversely, if there are not enough marker bits, the software repeats the marker bit pattern until there are enough marker bits to match the Waveform Length cell value.

Marker 4 Source

Selections: None, Frame, RF ALC Control, RF Blanking Control, Timing Control, User Defined Bits

Default: None

Defines the source of the marker points for Marker 4. Click at the right edge of the cell to display the ClosedMarker Source Selection dialog box from which you can select the marker source.

The signal generator outputs the marker 4 signal from the rear-panel EVENT 4 output. For more information, see the signal generator's User Guide.

When Parameter Optimization in the Signal Generator node is set to Auto, Marker 3 and Marker 4 source selection in the Waveform Setup node and the marker routing selected in the Dual Arb Marker Utilities are overridden.

To manually set Marker 3 and Marker 4 source, the marker routing, or both, set the Parameter Optimization to Off.

Select one of the following sources for the marker.

None

Sets all maker points are set to zero (inactive).

Frame

Sets the first five marker bits of the frame to 1, which sets an active marker for the first five waveform samples (waveform points). The signal generator outputs the Marker 1 output from the rear-panel Event 1 output.

RF ALC Control

Activates the automatic leveling control (ALC) function. When enabled, the ALC constantly monitors and controls the RF output power of the signal generator.

The ALC circuit cannot properly handle some modulation conditions, leading to output power level errors. In these conditions, turning the ALC off and using the signal generator power search function can achieve better power level accuracy.

RF Blanking Control

Assigns a specific marker to activate RF blanking. The automatic leveling control (ALC) hold is automatically enabled during output blanking.

RF Blanking Control improves the signal quality when the MAC channel and/or traffic channel are de-activated in a timeslot. It does so by increasing the on/off ratio of the forward link RF bursts.

When RF Blanking Control is enabled, the marker polarity must be set to positive or the wanted RF signal will be blanked, resulting in no RF output from the signal generator.

Timing Control

Sets the marker so that it is generated by the waveform.

IS95/cdma2000 generates the first five waveform samples (waveform points) in the short code cycle. 1xEV-DO generates the half-slot timing.

User Defined Bits

Opens the user Closeddata entry area, which lets you customize the marker signal.

The data entry area contains buttons to import, export, or clear user marker data along with the ability to insert a PN9 sequence as the marker bits. Optionally you can manually insert or delete marker data. To manually insert marker data, simply place the cursor within the data entry area or highlight existing bits, and insert bits. There are three ways to insert marker data:

(The key board shortcuts Ctrl+C and Ctrl+V work for user data entry.)

To delete data, simply place the cursor at the desired location within the data or highlight bits, and delete data. The key board short cut Ctrl+Z also deletes highlighted data.

The maximum number of marker bits for the user data entry area is 2,097,152 which equals 32,768 (1short code data points) * 64 (oversampling ratio). This is also the maximum file size.

The four buttons in the expanded area are:

Import

Loads a user-defined pattern from a selected location. When you select this button, the Open user defined data dialog box appears for navigating to and selecting the desired file. An imported file automatically updates the user data entry area. The software accepts the following file types:

The maximum file size is 2,097,152 bits. If the imported file is larger than bits, the software truncates the bits to conform to the maximum file size. 

Export

Saves the current data pattern, showing in the user data entry area, to a file. When you select this button, a Save user defined data dialog box appears for navigating to the location where you can save the file. The software saves the user data as one of the following selected file types:

Clear

Clears all data showing in the user data entry area.

Insert PN9

Inserts a fixed pattern pseudo-random bit sequence containing 511 bits (29–1) into the user data entry area. The software generates this fixed pattern in accordance with the CCITT recommendation O.153. Repeated clicking of this button adds additional PN9 sequences until the software attains the maximum file size of 2,097,152 bits. The software truncates data in excess of the maximum file size.

To edit the data pattern, insert the cursor at the desired point in the file and click Insert PN9, or enter the information manually using the keyboard keys 1 and 0. The software inserts the data at the cursor position and truncates all data in excess of 2,097,152 bits.

The software lets you create a file larger than it uses for the waveform. When this occurs, the software truncates the excess marker bits. Conversely, if there are not enough marker bits, the software repeats the marker bit pattern until there are enough marker bits to match the Waveform Length cell value.

Graphs

CCDF

Displays the Complimentary Cumulative Distribution Function (CCDF) graph. This Closedgraph shows the plot and peak-to-average values for the current waveform. A waveform can only be plotted after it has been generated.

The CCDF graph displays the probability (in percentage) of the generated carrier's calculated peak-to-average power ratio (measured in dB) meeting or exceeding a certain level. The table to the left of the CCDF plot displays the calculated peak-to-average values for the carrier. For additional information, see Understanding CCDF Curves.

Click Generate or Generate and Download from the main tool bar to generate an I/Q waveform and plot the CCDF graph using the current channel configuration. Any changes to the channel configuration setup do not appear on the graph until you generate the waveform. The status bar at the bottom of the screen shows waveform generation progress.

Each time you adjust parameters and generate a waveform, a plot is added to the Closedgraph. The graph retains your three most recent plots (in shades of gray), allowing you to make comparisons of waveform characteristics.

Use the buttons shown below to plot the Gaussian data, reference data and generated waveform data to the CCDF graph. The graph's initial state shows only the Gaussian curve (blue) until you generate a waveform.

Gaussian

Toggles the view of the band-limited Gaussian noise curve (blue).

Reference

Toggles the view of the reference curve (red). The reference appears as a flat line until you generate a waveform and click the Acquire Ref. button.

Acquire Ref.

Sets the current waveform curve to yellow and the reference curve to red. Click the Reference button to view the reference curve.

Waveform

Power

Selects different waveform plots. Selections include Power, ClosedI+Q, ClosedI|Q, and ClosedSpectrum. Each click selects the next plot type in the list. You can also click the arrow to access a drop-down menu where you can make a direct selection.

I+Qplots the I and Q curves overlapped.

I|Qdisplays the I and Q curves separately.

 

Spectrum displays a frequency domain based plotting.

Waveform Setup

Carrier "N"