The Fast Rate Control Channel Full Rate (FACCH/F) is a coded channel that is available with Option QFP.To open the Data node, click Data in the tree view. Use the Data window to define the bits in the bursts. The cells displayed in the Data section are determined by the Channel Type for the selected timeslot as defined in the Timeslot window.
Figure: Coded FACCH/F Data Node
1. Data (Normal GMSK Burst) |
---|
2. Control Frame |
Click to display a drop-down menu in which you can copy a timeslot configuration
from one timeslot to another
Use the Data window to define the bits in the bursts. The cells displayed in the Data section are determined by the burst type (Timeslot Type) for the selected timeslot as defined in the Timeslots window. In the window shown above, Timeslot 0 is set up for a data cell with a coded Fast Rate Control Channel Full rate (FAACH/F) burst.
Tail bits are set by the software.
Choice: PN9 |PN15 | User Defined Bits
Default: PN9
Click the Details button
in this cell to open the
Data Source
Selection
window.
Select an encoded
, or . The selected data is coded continuously across the RLC data block per the 3GPP standards. An independent version of the selected data is coded across the MAC header.To perform a receiver test with a continuous PN sequence, select .
You can enter 1 (control channel burst) or 0 (data channel burst). The default is 0. When Coded FAACH/F is entered at the Timeslot node, the software automatically sets the Stealing Flag bit to 1 (The Stealing Bits are not editable when Coded FAACH/F is selected).
Default: TSCO
Click the Details button in this cell to open the
Data Source Selection
window.
Select
to or to use for the training sequence bits.The training sequences selections are defined as follows:
If you manually change a timeslot (channel type), the training sequence for that timeslot resets to
provided that the training sequence was not previously changed for the new channel type.
TSC0 |
0970897 |
TSC1 |
0B778B7 |
TSC2 |
10EE90E |
TSC3 |
11ED11E |
TSC4 |
06B906B |
TSC5 |
13AC13A |
TSC6 |
29F629F |
TSC7 |
3BC4BBC |
Select custom training sequence
bits.
Guard period bits are set by the software. This setting is not editable.
Table: Guard Period Lengths Between Different Timeslots
Burst Transition |
Burst Transition Guard Period Between Timeslots (In terms of normal symbol periods) |
|
---|---|---|
TS0 and TS1 or TS4 and TS5 |
Any other timeslot pair |
|
normal symbol period to normal symbol period |
9 |
8 |
Choice: PN9 |PN15 | User Defined Bits
Default: PN9
Set the data for the control frame within a multiframe
setup. Click the Details button in this cell to open the
Data Source Selection
window.
Select create
a data string.
If the Multiframe type parameter at the Carrier n node is set to , the parameter, while appearing as active, has no effect since there is no control frame.