Timeslot-based Waveform Setup 1 2 3 4 5 6
Press the New icon
or select
from the menu.
In the tree view, select .
Double-click the field in the section and enter a name for the waveform.
Double-click the field in the section and enter a comment to associate with the waveform.
Set to as shown below
Set to as shown below.
In the tree view, select .
Click
the predefined configuration button
,
located above the summary table.
From the Pre-defined Carrier Configuration list that appears, select .
Select .
The selected predefined carrier appears in the carrier configuration summary table.
Use default instrument settings and Carrier settings.
Click the Generate and Download icon as shown below.
Measure the signal using an Keysight E4406A vector signal analyzer. Refer to in Keysight Literature number 5988-2389EN for instructions.