Timeslot-based Waveform Setup 1 2 3 4 5 6
Install the N7602B software. See Installing Signal Studio Software.
Obtain and install the appropriate license on your instrument. See Getting a License.
Run the N7602B software and connect to the instrument using LAN or GPIB. See Equipment Setup and Connection.
Ensure that the software
is set to its initial state. Press the New icon
or select
from the menu.
Obtain an Keysight 4406A vector signal analyzer.
Obtain Keysight Literature number 5988-2389EN.
The waveforms needed for this tutorial can be created as described in
the following topics or by using the PSA_demo_GSM.scp
and PSA_demo_EDGE.scp files provided. To use the files,
click >
(or click the Open Settings File icon
) and navigate to
> . Select the desired
file and click . The GSM configuration
contains four different waveforms. After you generate and download these
waveforms, you can select them individually using the instrument front
panel or the Signal Studio software.
Press > > >
Use the arrow keys or the knob to select the desired waveform.
Click in the tree view to display the basic characteristics of each waveform. Delete all of the waveforms except the one you want to use, then download the waveform to the instrument.