The is an advanced feature and applies to the following:
The Waveform Generation Log is available with Option QFP. Use the Waveform Generation Log to create a summary of the generated waveform's information.
Including:
Carrier type
Encrypted data source (i.e. for the first frame)
Time to generate all carriers
Using one of the two
examples
--or create your own-- set up the N7602B software to generate a Control
Channels waveform.
In the Tool menu, click to open the window.
Click the
button
to create a waveform. The transport layer information appears
in the window, as shown.
If you open the Waveform Generation Log after generating a waveform, no information is displayed.