Click  
 
 or  
 
 from the main 
 tool bar to generate an I/Q waveform and plot four different waveform 
 graphs (Power, I+Q, I/Q, and Spectrum) in accordance with the current 
 channel configuration. Any changes to the channel configuration do not 
 appear on the graph until you generate the waveform. The status bar at the bottom of the screen shows waveform 
 generation progress.
plot shows the cumulative power of the carrier configuration.
            
 
 Click this button to select from the list of different waveform plots. 
 Selections include Power (shown above), 
I+Q, 
 
I|Q, 
 and 
Spectrum. 
 Click the arrow to access a drop-down menu where you can make a direct 
 selection. Clicking the button selects the next plot type in the list 
 without displaying the menu.
The Waveform and CCDF graphs are minimized in 
 the Waveform WFMn node's initial view. To view the graphs, click and drag 
 the 
border 
 above the CCDF and Waveform graphs.