This example shows how to create an uplink (TDD) waveform with one UL PUSC zone and 3 bursts using auto allocation. It assumes the you know the MAC PDUs that you want to configure, and uses auto allocation to fit those into the UL PUSC zone. You might use this configuration for some receiver test situations.
In parameter configuration windows, you can check
in the upper right, and then click the desired
parameter for a brief description.
From the Welcome dialog, select
Click in the tree view. This section contains the key system parameters. Many of the default settings are used for this exercise.
Enter a name for your waveform.
: Use the default setting of 1.
: Select Uplink Only (TDD).
: Use the default setting, 50.0000. This parameter determines what portion of the total frame time is available for the downlink subframe.
: Use the default 10 MHz.
Leave the default settings for the other parameters.
Click in tree view.
: Use the default of 802.16e-2005 for this example. However, flexibility is provided to select either 802.16-2004/Cor1/D2 or 802.16-2004/Cor1/D3 depending on which standard specifications you want to use for subchannel randomization and subcarrier allocation.
Click the frame tab in the lower portion of the window to display the
frame plot view.
A small yellow triangle
at the bottom of the graph indicates the division between the downlink
and uplink. The available subframe time determines how many symbols can
be put into the subframe (see
example.)
Note that the RF burst off time will include any unused frame time, shown
as gap (TTG), plus the downlink portion (grayed out) of the TDD frame
when the Output Mode is Uplink Only (TDD).
Click in tree view. The top half shows various uplink parameters that are automatically calculated by the software. These cannot be modified. The bottom portion of the screen allows you to add PUSC, OPUSC, AMC or Sounding zones (maximum 3) to the uplink. The software already has a PUSC zone by default. Use this zone with a default burst and MAC PDU.
Click under Uplink in the tree view. Set the following parameters:
: Use the default (On).
: This parameter starts at 3 and will be incremented by the software as more MAC PDUs are added. Note that this must be a multiple of 3 because the UL PUSC zone is divided into slots which are 1 subchannel x 3 symbols (section 8.4.3.1).
Note that the available is 35.
The lower
half of the screen allows you to add regular
bursts, HARQ
bursts or collaborative
bursts. click
and select to add two regular bursts. Fields that are white in the table
may be edited either here or from the burst editing window.
Click under in the tree view to display the burst editing window. (You can also double-click in first column for Burst#1 in the table.) Leave all default values. Note that a power offset can be added to the burst. In the lower portion, one MAC PDU has been added by default.
Enter a number for the CID (Connection Identifier) from 0 to 65535. This identifies a connection between the base station and a specific subscriber station.
Change to 500 bytes and note the increased size of the zone in the frame view and the burst allocation in the zone plot in the lower right. The zone is now extended from symbol 0 to symbol 8.
Click in the tree view to configure the next burst.
Choose to be 16QAM 1/2. Note that a MAC PDU was automatically added in the lower half.
Enter a value for CID different from the one you previously used to indicate this MAC PDU is for a different subscriber station.
Click and select PN9.
Change to 600 bytes. Note in the zone plot in the lower right that the zone now extends out to symbol 14. Also note Burst#2 is smaller than Burst#1 (even though there are more data bytes) due to the higher order modulation.
Click in the tree view.
Choose to be 64QAM 2/3.
Set to 2 dB.
Set the to any valid value.
Set to 1000. Note the zone now extends to symbol 17, but it is not full.
Click
to verify all parameters are okay. View the result in the
window at the bottom of the main window.
Click on in the tree view to view the CCDF, Waveform, or Power Envelope graphs at the bottom of the page if desired.
Click
to generate waveform.
Click
to download waveform to the instrument if you have configured the instrument
connection.