PXIe VNA Front Panel Tour


  

M9370A to M9375A

M9800A to M9808A

M9834A-205

M9834A-270 and M9837A-205/270

2 Port

 2 Port (-200)

4 Port (M980xA-400)

6 Port (M980xA--600)

2Port

2 Port

See Also


Status LED

The following LED colors indicate the PXIe VNA status:

Green (solid) – Firmware is running but the PXIe VNA is NOT sweeping.

Green (blinking) - Each blink indicates a measurement sweep. The PXIe VNA may be sweeping faster than the indicator can blink.

Amber – Power is ON but the firmware is not running.

Red – A hardware error has occurred.

Off – Power is OFF.

Test Ports

All M937xA models are available with 2 test ports.

M980xA models are available with 2/4/6 test ports.

M983xA models are available with 2 test ports.

See data sheet for more information about the connector type and Input damage levels.

 Ref In / OUT

 

 

Ref In   To use a external reference signal, either one below is required. It is not detected automatically.

Note:  The external reference on the PXI chassis can be used by using SENS:ROSC:SOUR command.

 

Ref Out  This connector outputs a 10 or 100 MHz frequency reference signal for use by other modules and test equipment.

 

See data sheet for more information about the connector type and Input/output levels.

100 MHz signal for Ref In and Ref Out is available from Reference menu or SCPI command.

 

Trigger Lines (M937xA)

Trig IN  When enabled, the module accepts signals on this connector which indicates that the external devices is ready to be triggered.

Trig OUT  When enabled, the module outputs signals on these connectors either before or after a measurement.

Trig Ready  When enabled, the module outputs a 'READY' signal on this connector to other devices. This indicates that the module is ready to be triggered.

Learn more about External Triggering

LO Out / LO In

For Daisy-chaining two or more modules. See the following information. See data sheet for more information about the connector type and Input damage levels. A 50 ohm terminations (p/n 1810-0118) is placed at the factory shipment.

Ctrl M/Ctrl S (M98xxA)

For Daisy-chaining two or more modules for multi-port or I/O adapter.

M983xA Other Ports (R1 In, R2 In, A In, B In, R1 Out, R2 Out, A Out, B Out, Src X In, Src 1 In , Src 2 In, RF 1 Out, RF 2 Out, RF In, BB In)

See the Path Configurator (RF and IF) for internal block diagram.

The following ports on the M9837A and M9834-270 are connected with RF semi-rigid cables at the factory shipment.  These three cables must be connected at the service center calibration (performance test/adjustment)

Connector Name

M9834A

M9837A

R1 Out, R2 Out, Src1 Out, Src2 Out, A Out, B Out, BB In, RF In , Src X In, LO In, LO Out

SMA Female

SMA Female

RF1 Out, RF2 Out, A In, B In, R1 In, R2 In, Src1 In, Src2 In, Port 1, Port 2

3.5 mm Female

2.4 mm Female

 

       

Notes:  

Maintain Semi-Rigid Cable Orientation 

  • Do not mix, interchange, swap, or reverse the semi-rigid cables between units.

  • Ideally, a cable would exhibit identical characteristics in both directions. In practice, however, small differences may exist. Because the test-port characterization is performed using a specific cable in a specific orientation, reversing the cable orientation is not recommended.

  • If a semi-rigid cable is inadvertently swapped or reinstalled in an orientation different from that used during adjustment, perform a full User Cal to compensate for much of the cable-related systematic error introduced at the test ports.

  • If any semi-rigid cable is damaged, missing, or requires replacement, send the M983xA to a Keysight service center for cable replacement and calibration.