Controls the Trace Hold settings.
These commands are Superseded by the CALCulate:MEASure:HOLD commands.
CALCulate:HOLD |
Click on a keyword to view the command details.
See Also
Critical Note: CALCulate commands act on the selected measurement. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more.
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-Write) Sets the type of trace hold to perform. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<char> |
Trace Hold type. Choose from: OFF - Disables the Trace Hold feature. MINimum - Sets Trace Hold to store the lowest measured data points. MAXimum - Sets Trace Hold to store the highest measured data points. |
Examples |
CALC:HOLD:TYPE MAX calculate2:hold:type minimum |
Query Syntax |
CALCulate<ch>:HOLD:TYPE? |
Return Type |
Character |
OFF |
|
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Write-only) Resets the currently-stored data points to the live data trace and restarts the currently-selected Trace Hold type. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
Examples |
CALC:HOLD:CLE calculate2:hold:clear |
Query Syntax |
Not Applicable |
Not Applicable |
|