Measure

These commands are for setting up measurements.

CALCulate:MEASure

BLIMit More commands

COMPutation

    | DEViation

CONVersion

    | FUNCtion

CORRection More commands

DATA More commands

DEFine

DELete

    | ALL

DISTortion More commands

EQUation

    | FAST[:STATe]

    | [:STATe]

    | TEXT

    | VALid?

FILTer More commands

FORMat

    | UNIT

FUNCtion More commands

GCData More commands

GCMeas More commands

GDELay More commands

HOLD

    | CLEar

    | [TYPE]

LIMit More commands

MARKer More commands

MATH

    | FUNCtion

    | INTerpolate[:STATe]

    | LOCKed[:STATe]?

    | MEMorize

    | NORMalize

    | NEW

MIXer

    | XAXis

OFFSet More commands

PARameter More commands

PN More commands

RDATa?

RLIMit More commands

SMOothing More commands

TRANsform More commands

X More commands

Y More commands

Click a keyword to view the command details.

See Also


CALCulate<cnum>:MEASure<mnum>:CONVersion:FUNCtion <char>

Applicable Models: All

(Read-Write) Sets or gets the parameter after conversion using the parameter conversion function, for the active trace of selected channel.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<char>

Select from the following parameters after conversion:

  • "OFF"

  • "ZREFlection" - Specifies the equivalent impedance in reflection measurement.

  • "ZTRansmit" - Specifies the equivalent impedance (series) in transmission measurement.

  • "ZTSHunt" - Specifies the equivalent impedance (shunt) in transmission measurement.

  • "YREFlection" - Specifies the equivalent admittance in reflection measurement.

  • "YTRansmit" - Specifies the equivalent admittance (series) in transmission measurement.

  • "YTSHunt" - Specifies the equivalent admittance (shunt) in transmission measurement.

  • "INVersion" - Specifies the inverse S-parameter (1/S).

  • "CONJugation" - Specifies the conjugate.

Examples

SCPI sequence to retrieve resistance from a polar chart:

CALC:MEAS:CONV:FUNC ZREFlection

CALC:MEAS:FORM:REAL

CALC:MEAS:DATA:FDATA?

 

SCPI sequence to retrieve reactance from a polar chart:

CALC:MEAS:CONV:FUNC ZREFlection

CALC:MEAS:FORM:IMAG

CALC:MEAS:DATA:FDATA?

 

Query Syntax

CALCulate<cnum>:MEASure<mnum>:CONVersion:FUNCtion?

Return Type

Character

Default

"OFF"


CALCulate<cnum>:MEASure<mnum>:COMPutation:DEViation <char>

Applicable Models: All

(Read-Write) Calculates the deviation from a least-squares best fit line.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<char>

Select from the following parameters:

  • "OFF"

  • "LINear" -Fit to 1st order curve minimizing RSS deviation.

  • "PARabolic" - Fit to 2nd order curve minimizing RSS deviation.

  • "CUBic" - Fit to 3rd order curve minimizing RSS deviation.

Examples

CALC:MEAS1:COMP:DEV LIN
calculate2:measure1:computation:deviation linear

Query Syntax

CALCulate<cnum>:MEASure<mnum>:COMPutation:DEViation?

Return Type

Character

Default

"OFF"


CALCulate<cnum>:MEASure<mnum>:DEFine <string>

Applicable Models: All

(Write-only) Creates a measurement but does NOT display it, on an existing or new channel. When a new channel is created, any licensed measurement class can be used. Up to 580 (2000 for M98xxA, P50xxA/B and E5080B, E5081A)  measurements can be created.

Note that each display window can only display a limited number of traces. See Traces, Channels, and Windows on the VNA.

This command replaces the following commands:

CALCulate:PARameter[:DEFine]

CALCulate:PARameter[:DEFine]:EXTended

CALCulate:CUSTom:DEFine

Parameters

 

<cnum>

Channel number of the new measurement. If unspecified, value is set to 1.

If the specified channel does not exist, then a channel of the specified type will be created. If no type of channel is specified, then a standard channel will be created.

If the specified channel exists, then the parameter will be added to the channel provided the existing channel supports the parameter (otherwise, an error will be generated).

<mnum>

Measurement number for the new measurement.

If the specified measurement number is already in use, an error will be generated.

<string>

 

(String ) Measurement Parameter and optional measurement class name separated by a ":" (colon). For example, "S21:Gain Compression" creates an S21 measurement and selects the Gain Compression measurement class for the channel.

Note: If a measurement class of a channel does not support the defined measurement parameter, an error is generated.

Case sensitive.

For S-parameters:

Any S-parameter available in the VNA

Single-digit port numbers CAN be separated by "_" (underscore). For example: "S21" or "S2_1"

Double-digit port numbers MUST be separated by underscore. For example: "S10_1"

For ratioed measurements:

Any two VNA physical receivers separated by forward slash '/' followed by comma and source port.

For example: "A/R1, 3"

Learn more about ratioed measurements

See a block diagram showing the receivers in YOUR VNA.

For non-ratioed measurements:

Any VNA physical receiver followed by comma and source port.

For example: "A, 4"

Learn more about unratioed measurements.

See the block diagram showing the receivers in YOUR VNA.

Ratioed and Unratioed measurements can also use logical receiver notation to refer to receivers. This notation makes it easy to refer to receivers with an external test set connected to the VNA. You do not need to know which physical receiver is used for each test port. Learn more.

For ADC measurements:

Any ADC receiver in the VNA followed by a comma, then the source port.

For example: "AI1,2" indicates the Analog Input1 with source port of 2.

Learn more about ADC receiver measurements.

 

(string) - The following are the existing valid measurement parameters for each measurement class. The Measurement Class must be installed and registered on the VNA.

(variant) Measurement names to create:

Meas Class

Measurement Name

Description

"Standard"

"S11", "S21", and so forth

"A_1","A_2", and so forth

S-parameter name

Unratioed parameter names with notation: "receiver_source port"

See balanced parameter names

Active Hot Parameters

Port 1 is the Source Port (DUT input). Port 3 or Port 2 can be chosen as the output of the DUT.

"HotS11"

"HotS31"

"HotS13"

"HotS33"

"IPwr"

"OPwr"

"Gamma"

"Pmax"

"Xs(3,3)"

"Xt(3,3)"

"Xf(3,1)"

"DeltaOPwr"

Learn about Active Hot parameters

"Scalar Mixer/Converter"

For input port X and output port Y:

"SCXY"

"SCYX"

"SXX"

"SYY"

"Ipwr"

"RevIPwr"

"Opwr"

"RevOPwr"

Learn about SMC parameters

Note: Input and output ports are set up using the Mixer Setup dialog. If the ports are not set up using the Mixer Setup dialog, then ports 1 and 2 are the default input and output ports and the only ports that can be used.

"Gain Compression"

Learn more

"Gain Compression Converters"

Learn more

GCA:

"CompIn21"

Input power at the compression point.

"CompOut21"

Output power at the compression point.

"CompGain21"

Gain at the compression point.

"CompS11"

 Input Match at the compression point

"RefS21"

Linear Gain

"DeltaGain21"

CompGain21 -Linear Gain

"S11", "S21", "S12", "S22"

Standard S-parameters; measured at port 1 and port 2

GCX - All Gain Compression parameters (except S21 and S12) plus the following:

"S11"

"SC21"

"SC12"

"S22"

"Ipwr"

"RevIPwr"

"Opwr"

"RevOPwr"

Mixer parameters

"Modulation Distortion"

Modulation Distortion Converters

Learn more

Modulation Distortion:

"PIn1"

Power In

"POut1"

Reflected Power In

"POut2"

Power Out

"PModFile"

Power of modulation file

"MSig2"

Modulation Signal Out

"MDist2"

Modulation Distortion Out

"MDistIR2"

Modulation Distortion Input-referred

"MGain21"

Modulation Gain

"MComp21"

Modulation Compression

"PGain21"

Power Gain

"LMatch2"

Load match of VNA port

"CarrIn1"

Input Band Power

"CarrOut2"

Output Band Power

"CarrGain21"

Band Power Gain

"NPRIn1"

NPR at Input

"NPROut2"

NPR at Output

"NPRDist21"

NPR Distortion, Added by DUT

"NPRPwrIn1"

NPR Input Power

"NPRPwrOut2"

NPR Output Power

"ACPIn1"

ACP at input

"ACPOut2"

ACP at output

"ACPDist21"

ACP distortion, Added by DUT

"ACPPwrIn1"

ACP Input Power

"ACPPwrOut2"

ACP Output Power

"EVMDistEq21"

EVM Equalized Distortion, Added by DUT

"EVMDistUn21"

EVM Unequalized Distortion, Added by DUT

"EVMPwrIn1"

EVM Input Power

"EVMPwrOut2"

EVM Output Power

"ModFilter"

Measurement Modulation Filter

"A", "b1"

Port 1 test port receiver

"B", "b2"

Port 2 test port receiver

"C", "b3"

Port 3 test port receiver

"D", "b4"

Port 4 test port receiver

"R1", "a1"

Port 1 reference receiver

"R2", "a2"

Port 2 reference receiver

"R3", "a3"

Port 3 reference receiver

"R4", "a4"

Port 4 reference receiver

Modulation Distortion ONLY - NOT Modulation Distortion Converters

"S11"

Linear Input Match

"S21"

Linear Gain

"LPIn1"

Linear Input Match

"LPOut1"

Linear Reflected Power In

"LPOut2"

Linear Power Out

"Noise Figure Cold Source"

Learn more

"Noise Figure Converters"

Learn more

Noise Figure AND NFX:

"NF"

Noise figure

"ENR"

Validate noise source measurements.

"T-Eff"

Effective noise temperature.

"DUTRNP"

"DUTRNPI"

DUT noise power ratio. (Noise power expressed in Kelvin divided by 290).

"SYSRNP"

"SYSRNPI"

System noise power ratio

"DUTNPD"

"DUTNPDI"

DUT noise power density. (Noise power expressed in dBm/Hz).

"SYSNPD"

"SYSNPDI"

System noise power density.  

"OvrRng"
(Opt 029 Only)

Indication that the noise receiver is being over powered.

"T-Rcvr"

(Opt 029 Only)

Temperature reading (in Kelvin) of the noise receiver board.

Noise Figure ONLY - NOT NFX:

"S11", "S21", "S12", "S22"

Standard S-parameters; measured with the port1 and port2 noise switches set for noise mode.

"A_1","A_2" ...and so forth.

Unratioed parameters; with notation:
"receiver, source port"

"GammaOpt"

Optimum Complex Reflection Coefficient

"Rn"

Noise Resistance

"NFMin"

Minimum noise figure that occurs at GammaOpt

NFX ONLY:

"S11"

"SC21"

"SC12"

"S22"

"Ipwr"

"RevIPwr"

"Opwr"

"RevOPwr"

Mixer parameters

"ALO1"," BLO1" ...and so forth.

Test port receiver at LO1 frequency

"R1_1", "B_2" ..and so forth.

Unratioed parameters with notation:

"receiver_source port"

"Swept IMD"

"Swept IMD Converters"

Learn more

There are over 150 possible Swept IMD parameters, too many to list here.

Build the parameters with the Swept IMD Parameter dialog, then copy the parameter name to the remote command.

The following are a few example parameters:

"PwrMainLo"

Absolute power of the Low tone at the DUT output.

"IM3"

Power of the third product relative to the average power of the f1 and f2 tones measured at the DUT output.

"OIP3"

Theoretical power level at which the third product will be the same power level as the average of the main tones at the output of the DUT.

"Differential I/Q"

Learn more

Create custom parameters using Sens:DIQ:Par:Def, then specify your custom parameter name here.

The following are default parameters:

"IPwrF1"

"OPwrF1"

"GainF1"

Input Power over F1 range

Output Power over F1 range

Gain over F1 range

"Spectrum Analyzer"

Learn more

"a<n>"

"b<n>"

where <n> is the port number to measure

"ImageReject<n>"

where <n> is the image reject trace

Reference receiver

Test port receiver

"Vector Signal Analyzer"

Learn more

"a<n>"

"b<n>"

where <n> is the port number to measure

Reference receiver

Test port receiver

TDR

Use SYSTem:TDR:PRESet instead of CALC:MEAS:DEFine

Examples

CALC1:MEAS2:DEF "S11" 'Defines an S11 measurement for channel 1, measurement number 2.

CALC4:MEAS3:DEF "S21:Gain Compression" 'Defines an S21 measurement for channel 4, measurement number 3, and creates a GCA channel.

CALC2:MEAS:DEF "R1,1:Standard" 'Defines an R1,1 measurement for channel 2, measurement number 1 (default), and creates a Standard channel.

SYST:FPRest
CALC1:MEAS1:DEF "NF:Noise Figure Cold Source" 'Defines a Noise Figure measurement for channel 2, measurement number 2, and creates a Noise Figure channel.
DISP:WIND1 ON
DISP:MEAS1:FEED 1
CALC2:MEAS2:DEF "CompIn21:Gain Compression" 'Defines an input power at Compression point but doesn't display on channel 2.
DISP:WIND2 ON
DISP:MEAS2:FEED 2 'CompIn21 measurement in window number 2.
CALC2:MEAS3:DEF "CompOut21:Gain Compression"  'Defines an output power at Compression point but doesn't display on channel 2
DISP:MEAS3:FEED 2 'CompOut21 measurement in window number 2

Query Syntax

Not Applicable

Default

Not Applicable


CALCulate<cnum>:MEASure<mnum>:DELete

Applicable Models: All 

(Write-only) Deletes the specified measurement.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number.

Examples

CALC:MEAS2:DEL
calculate2:measure2:delete

Query Syntax

Not Applicable

Default

Not Applicable


CALCulate:MEASure:DELete:ALL

Applicable Models: All

(Write-only) Deletes all measurements on the VNA.

Parameters

 

Examples

CALC:MEAS:DEL:ALL

Query Syntax

Not Applicable

Default

Not Applicable


CALCulate<cnum>:MEASure<mnum>:EQUation:FAST[:STATe] <bool>

Applicable Models: All

(Read-Write) Set and return equation editor trace update delay. This command delays updating the equation editor trace until all trace references have finished updating to ensure that all data is present.

Note: This command does not work in application channels. In addition, this command does not work with the standard channel when the channel is in HOLD and then SINGLE sweeps are sent.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<bool>

Choose from:

OFF (0)  Do not delay equation editor trace update.

ON (1)  Delay equation editor trace update.

Examples

CALC:MEAS:EQU:FAST 1
calculate2:measure1:equation:fast OFF

Query Syntax

CALCulate<cnum>:MEASure<mnum>:EQUation:FAST[:STATe]?

Return Type

Boolean

Default

OFF or 0


CALCulate<cnum>:MEASure<mnum>:EQUation[:STATe] <bool>

Applicable Models: All

(Read-Write)  Turns ON and OFF the equation on selected measurement for the specified channel. If the equation is not valid, then processing is not performed. Use CALC:EQUation:VALid? to ensure that the equation is valid.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<bool>

ON (or 1) - turns equation ON.

OFF (or 0) - turns equation OFF.

Examples

CALC:MEAS:EQU 1

calculate2:measure1:equation:state 0

Query Syntax

CALCulate<cnum>:MEASure<mnum>:EQUation[:STATe]?

Return Type

Boolean

Default

OFF (0)


CALCulate<cnum>:MEASure<mnum>:EQUation:TEXT <string>

Applicable Models: All

(Read-Write)  Specifies an equation or expression to be used on the selected measurement for the specified channel.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<string>

Any valid equation or expression. See Equation Editor.

Examples

'Equation (includes '=')

CALC:MEAS:EQU:TEXT "foo=S11/S21"

'Expression
calculate2:measure1:equation:text "S11/S21"

Query Syntax

CALCulate<cnum>:MEASure<mnum>:EQUation:TEXT?

Return Type

String

Default

Not Applicable


CALCulate<cnum>:MEASure<mnum>:EQUation:VALid?

Applicable Models: All

(Read-Only)  Returns a boolean value to indicate if the current equation on the selected measurement for the specified channel is valid. For equation processing to occur, the equation must be valid and ON (CALC:EQU:STAT 1).

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

Examples

CALC:MEAS:EQU:VAL?

calculate2:measure1:equation:valid?

Return Type

Boolean

1 - equation is valid

0 - equation is NOT valid

Default

Not Applicable


CALCulate<cnum>:MEASure<mnum>:FORMat <char>

Applicable Models: All

(Read-Write) Sets the display format for the measurement.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<char>

Choose from:

  • MLINear

  • MLOGarithmic

  • PHASe

  • UPHase 'Unwrapped phase

  • IMAGinary

  • REAL

  • POLar

  • SMITh

  • SADMittance 'Smith Admittance

  • SWR

  • GDELay 'Group Delay

  • KELVin

  • FAHRenheit

  • CELSius

  • PPHase 'Positive Phase

  • COMPlex

Examples

CALC:MEAS:FORM MLIN
calculate2:measure1:format polar

Query Syntax

CALCulate<cnum>:MEASure<mnum>:FORMat?

Return Type

Character

Default

MLOG


CALCulate<cnum>:MEASure<mnum>:FORMat:UNIT <dataFormat>, <units>

Applicable Models: All

(Read-Write) Sets and returns the units for the specified data format. Measurements with display formats other than those specified are not affected.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<dataFormat>

Choose from:

  • MLOG - Log magnitude

  • MLIN - Linear magnitude

<units>

For unratioed MLOG measurements, choose from:

  • dB  Units are displayed in decibels.

  • DBM  Units are displayed in dBm.  0 dBm = 0.001 watt

  • DBMV Units are displayed in dBmV.  0 dBmV = 0.001 volt
    DBmV value depends on the reference impedance: dBmV = dBm + 30 + 10*log10(Z0)

  • DBMA Units are displayed in dBmA. 0 dBmA = 0.001 Ampere

  • DBUV Units are displayed in dBuV. 0 dBuV = 1 uV
    DBuV value depends on the reference impedance: dBuV = dBm + 90 + 10*log10(Z0)

For unratioed MLIN measurements, choose from:

  • UNIT - No units. Linear magnitude without conversion
  • W - Units are displayed in  Watts
  • V - Units are displayed in Volts
  • A - Units are displayed in Amperes

Examples

CALC:MEAS:FORM:UNIT MLOG, DBM
calculate2:measure1:format:unit mlog,dbmv

Query Syntax

CALCulate<cnum>:MEASure<mnum>:FORMat:UNIT? <dataFormat>

Return Type

Character

Default

MLOG, DBM


CALCulate<ch>:MEASure<mnum>:HOLD:CLEar

Applicable Models: All

(Write-only) Resets the currently-stored data points to the live data trace and restarts the currently-selected Trace Hold type.

Parameters

 

<ch>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

Examples

CALC:MEAS:HOLD:CLE

calculate2:measure1:hold:clear

Query Syntax

Not Applicable

Default

Not Applicable


CALCulate<ch>:MEASure<mnum>:HOLD:TYPE <value>

Applicable Models: All

(Read-Write) Sets the type of trace hold to perform.

Parameters

 

<ch>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<value>

Trace Hold type. Choose from:

OFF - Disables the Trace Hold feature.

MINimum - Sets Trace Hold to store the lowest measured data points.

MAXimum - Sets Trace Hold to store the highest measured data points.

Examples

CALC:MEAS:HOLD:TYPE MAX

calculate2:measure1:hold:type minimum

Query Syntax

CALCulate<ch>:MEASure<mnum>:HOLD:TYPE?

Return Type

Character

Default

OFF


CALCulate<cnum>:MEASure<mnum>:MATH:FUNCtion <char>

Applicable Models: All

(Read-Write) Sets math operations on the currently selected measurement and the trace stored in memory. (There MUST be a trace stored in Memory. See CALC:MEAS:MATH MEM)

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<char>

The math operation to be applied. Choose from the following:

 

NORMal

Trace data only

 

ADD

Data + Memory

 

SUBTract

Data - Memory

 

MULTiply

Data * Memory

 

DIVide

Data / Memory

Examples

CALC:MEAS:MATH:FUNC NORM
calculate2:measure1:math:function subtract

Query Syntax

CALCulate<cnum>:MEASure<mnum>:MATH:FUNCtion?

Return Type

Character

Default

NORMal


CALCulate<cnum>:MEASure<mnum>:MATH:INTerpolate[:STATe]

Applicable Models: N522xB, N523xB, N524xB

(Read-Write) Sets and reads the state of the memory data interpolation. Learn more.

Parameters

 

<cnum>

Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <ch> is set to 1.

<mnum>

Measurement number for each measurement.

<bool>

Choose from:

0 - OFF - Turn memory data interpolation OFF.

1 - ON - Turn memory data interpolation ON.

Examples

CALC2:MEAS:MATH:INT 1

Query Syntax

CALCulate<cnum>:MEASure<mnum>:MATH:INTerpolate?

Return Type

Boolean

Default

0


CALCulate<cnum>:MEASure<mnum>:MATH:LOCKed[:STATe]?

Applicable Models: All

(Read-only) Returns whether the measurement number is the locked trace created by Data-> New Trace under Math. A locked trace indicates that the trace will not update from sweep to sweep. Learn more.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

Examples

CALC2:MEAS3:MATH:LOCK:STAT?

Query Syntax

CALCulate<cnum>:MEASure<mnum>:MATH:LOCKed:STATe?

Return Type

Boolean

0 - Measurement is not locked.

1 - Measurement is locked.

Default

0


CALCulate<cnum>:MEASure<mnum>:MATH:MEMorize

Applicable Models: All

(Write-only) Puts the currently selected measurement trace into memory. (Data-> Memory).

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

Examples

CALC:MEAS:MATH:MEM
calculate2:measure1:math:memorize

Query Syntax

Not applicable

Default

Not applicable


CALCulate<cnum>:MEASure<mnum>:MATH:NORMalize

Applicable Models: All

(Write-only) Execute the normalized for specified measurement

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

Examples

CALC:MEAS:MATH:NORM
calculate2:measure1:math:normalize

Query Syntax

Not applicable

Default

Not applicable


CALCulate<cnum>:MEASure<mnum>:MATH:NEW [<mnum2>][, <windType>]

Applicable Models: All

(Read-Write) Create a new data trace to be saved from the same trace data (Data-> New Trace under Math). The query command returns the measurement number of the memory trace created by the most recent execution of the CALC:MEAS:MATH:NEW command. The query form takes no parameters.

The CALC<cnum>:MEAS<mnum>:DATA returns the trace values. Learn more.

 

When the number of traces per window exceeds the limit, returns an error +113, "Exceeded the maximum number of traces per windowz".

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number. The query command ignores <mnum>. If the measurement number is provided, the new measurement is created with that identifying number. If the measurement number is not provided, the new measurement uses the next available measurement number.

<mnum2>

(Optional) The new measurement (trace number) is created with that identifying number..

<windType>

(Optional) Feed the new measurement depending on this parameter.

  • NONE: No feed (Default) When not fed, the measurement is not visible on the display until it is placed into a window with the DISP:WIND:TRAC:FEED  command.
  • ACTive: Feed to active window
  • NEW: Feed to new window

Examples

CALC:MEAS:MATH:NEW
calculate2:measure2:math:new 2, ACT

Query Syntax

CALCulate<cnum>:MEASure<mnum>:MATH:NEW?

This command is useful for determining the new measurement’s number in the case where the optional <mnum2> parameter was not provided in a CALC:MEAS:MATH:NEW command.

Default

Not applicable


CALCulate<ch>:MEASure<mnum>:MIXer:XAXis <char>

Applicable Models: All

(Read-Write) Sets or returns the swept parameter to display on the X-axis for the selected FCA ,GCX, IMDX and  NFX measurement.

Parameters

 

<ch>

Any existing channel number. If unspecified, value is set to 1.

<mnum>

Measurement number for each measurement.

<char>

Parameter to display on the X-axis. Choose from:

INPut  - Input frequency span

OUTPut  - Output frequency span

LO_1  - First LO frequency span

LO_2  - Second LO frequency span

Examples

CALC:MEAS:MIX:XAX INPUT
calculate2:measure1:mixer:xaxis output

See an example that creates, selects, and calibrates an SMC and VMC measurement using SCPI.

Query Syntax

CALCulate<ch>:MEASure<mnum>:MIXer:XAXis?

Return Type

Character

Default

INPut


CALCulate<cnum>:MEASure<mnum>:RDATA? <char>

Applicable Models: All

(Read-only) Returns receiver data for the selected measurement.

Parameters

 

<cnum>

Channel number of the measurement (optional).

<mnum>

Measurement number for each measurement.

<char>

Choose from any physical receiver in the VNA.

For example: "A"

Also, REF - returns data for either R1 or R2 data depending on the source port of the selected measurement.

See the block diagram showing the receivers in YOUR VNA.

Note: Logical receiver notation is NOT allowed with this command. Learn more.

Example

GPIB.Write "INITiate:CONTinuous OFF"
GPIB.Write "INITiate:IMMediate;*wai"
GPIB.Write "CALCulate:MEASure2:RDATA? A"

GPIB.Write "CALCulate:MEASure2:RDATA? REF"

Return Type

Depends on FORM:DATA - Two numbers per data point

Default

Not Applicable