Controls IM Spectrum measurement configuration.
SENSe:IMS: | INPut | OUTPut RESPonse | STARt | STOP | CENTer | SPAN STIMulus | FCENter | TOPWer | F1 | F2 SWEep: | TYPE | ORDer TPOWer | EQUal | LEV | SET TRACking | CHANnel | MSENable | SINDex | STATe
|
Click on a keyword to view the command details.
See Also
About IM Spectrum measurements
Applicable Models: N522xB, N524xB (Write-only) Sets the input port and output port of an IMS or IMSx channel. This setting is necessary only when using the limited port mapping feature. Learn more. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<input> |
VNA port connected to the DUT Input. Choose from 1 or 3. When input is 3, an external combiner must be used. |
<output> |
VNA port connected to the DUT Output. When input is 1, output must be 2. When input is 3, output must be 4. |
Examples |
SENS:IMS:PMAP 3,4 sense2:ims:pmap 3,4 |
Query Syntax |
Not Applicable |
Default |
1,2 |
Applicable Models: N522xB, N524xB (Read-only) Returns the VNA test port to be connected to the DUT input for an IMS or IMSx channel. Set the VNA port to DUT mapping using SENS:IMS:PMAP |
|
Parameters |
|
<cnum> |
IMS channel number. If unspecified, value is set to 1. |
Examples |
SENS:IMS:PMAP:INP? sense2:ims:pmap:input? |
Default |
1 |
Applicable Models: N522xB, N524xB (Read-only) Returns the VNA test port to be connected to the DUT output for an IMS or IMSx channel. Set the VNA port to DUT mapping using SENS:IMS:PMAP |
|
Parameters |
|
<cnum> |
IMS channel number. If unspecified, value is set to 1. |
Examples |
SENS:IMS:PMAP:OUTP? sense2:ims:pmap:output? |
Default |
2 |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the Resolution Bandwidth for the IM Spectrum measurement. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<num> |
Resolution BW in Hz. Choose from: 60k | 100k | 150k | 300k, 600k | 1.0M | 3.0M If an invalid number is specified, the VNA will round up to the closest valid number. |
Examples |
SENS:IMS:RBW 600e3 sense2:ims:rbw 1MHz |
Query Syntax |
SENSe<cnum>:IMS:RBW? |
Return Type |
Numeric |
Default |
600 kHz |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the receiver Start frequency for the IM Spectrum measurement. Valid ONLY when Tracking is NOT enabled and when Sweep Type = Linear. Otherwise, this setting is ignored. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<num> |
Start frequency in Hz. Choose a frequency within the range of the VNA. |
Examples |
SENS:IMS:RESP:STAR 1e9 sense2:ims:response:start 100e6 |
Query Syntax |
SENSe<cnum>:IMS:RESPonse:STARt? |
Return Type |
Numeric |
Default |
950 MHz |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the receiver Stop frequency for the IM Spectrum measurement. Valid ONLY when Tracking is NOT enabled and when Sweep Type = Linear. Otherwise, this setting is ignored. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<num> |
Stop frequency in Hz. Choose a frequency within the range of the VNA. |
Examples |
SENS:IMS:RESP:STOP 26e9 sense2:ims:response:stop 100e6 |
Query Syntax |
SENSe<cnum>:IMS:RESPonse:STOP? |
Return Type |
Numeric |
Default |
1.05 MHz |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the receiver Center frequency for the IM Spectrum measurement. Valid ONLY when Tracking is NOT enabled and when Sweep Type = Linear. Otherwise, this setting is ignored. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<num> |
Center frequency in Hz. Choose a frequency within the range of the VNA. |
Examples |
SENS:IMS:RESP:CENT 26e9 sense2:ims:response:center 100e6 |
Query Syntax |
SENSe<cnum>:IMS:RESPonse:CENTer? |
Return Type |
Numeric |
Default |
1.0 GHz |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the Span of receiver frequencies for the IM Spectrum measurement. Valid ONLY when Tracking is NOT enabled and when Sweep Type = Linear. Otherwise, this setting is ignored. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<num> |
Frequency span in Hz. All receiver frequencies should be within the range of the VNA. |
Examples |
SENS:IMS:RESP:SPAN 10e9 sense2:ims:response:span 100e6 |
Query Syntax |
SENSe<cnum>:IMS:RESPonse:SPAN? |
Return Type |
Numeric |
Default |
100 MHz |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the DeltaF (tone spacing) for the IM Spectrum measurement. Valid ONLY when Tracking is NOT enabled. Otherwise, this setting is ignored. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<num> |
Delta frequency in Hz. All stimulus settings MUST be within the frequency range of the VNA. |
Examples |
SENS:IMS:STIM:DFR 1e6 sense2:ims:stimulus:dfrequency 100e6 |
Query Syntax |
SENSe<cnum>:IMS:STIMulus:DFRequency? |
Return Type |
Numeric |
Default |
10 MHz |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the Center frequency for the IM Spectrum measurement. Valid ONLY when Tracking is NOT enabled. Otherwise, this setting is ignored. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<num> |
Center frequency in Hz. All stimulus settings MUST be within the frequency range of the VNA. |
Examples |
SENS:IMS:STIM:FCEN 1e6 sense2:ims:stimulus:fcenter 100e6 |
Query Syntax |
SENSe<cnum>:IMS:STIMulus:FCENter? |
Return Type |
Numeric |
Default |
1.0 GHz |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the F1 frequency for the IM Spectrum measurement. Valid ONLY when Tracking is NOT enabled. Otherwise, this setting is ignored. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<num> |
F1 frequency in Hz. All stimulus settings MUST be within the frequency range of the VNA. |
Examples |
SENS:IMS:STIM:F1FR 1e6 sense2:ims:stimulus:f1frequency 100e6 |
Query Syntax |
SENSe<cnum>:IMS:STIMulus:F1FRequency? |
Return Type |
Numeric |
Default |
995 MHz |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the F2 frequency for the IM Spectrum measurement. Valid ONLY when Tracking is NOT enabled. Otherwise, this setting is ignored. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<num> |
F2 frequency in Hz. All stimulus settings MUST be within the frequency range of the VNA. |
Examples |
SENS:IMS:STIM:F2FR 1e6 sense2:ims:stimulus:f2frequency 100e6 |
Query Syntax |
SENSe<cnum>:IMS:STIMulus:F2FRequency? |
Return Type |
Numeric |
Default |
1.005 MHz |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the power level of the F1 tone. When SENS:IMS:TPOW:COUP ON (tone power is coupled), setting either F1 or F2 power sets both. This setting is ignored if SENS:IMS:TRAC:STAT is enabled. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<value> |
F1 tone power level in dBm. Choose a value between +30 dBm and -30 dBm. |
Examples |
SENS:IMS:STIM:TPOW:F1 -10 sense2:ims:stimulus:tpower:f1 0 |
Query Syntax |
SENSe<cnum>:IMS:STIMulus:TPOWer:F1? |
Return Type |
Numeric |
Default |
-20 |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the power level of the F2 tone. When SENS:IMS:TPOW:COUP ON (tone power is coupled), setting either F1 or F2 power sets both. This setting is ignored if SENS:IMS:TRAC:STAT is enabled. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<value> |
F2 tone power level in dBm. Choose a value between +30 dBm and -30 dBm. |
Examples |
SENS:IMS:STIM:TPOW:F2 -10 sense2:ims:stimulus:tpower:f2 0 |
Query Syntax |
SENSe<cnum>:IMS:STIMulus:TPOWer:F2? |
Return Type |
Numeric |
Default |
-20 |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the method in which the spectrum of signals to view are specified. When Tracking is enabled the frequency of the main tones (f1 and f2) are always determined by the Swept IMD channel. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<char> |
IM Spectrum sweep type. Choose from:
|
Examples |
SENS:IMS:SWEep:TYPE LIN sense2:ims:sweep:type nth |
Query Syntax |
SENSe<cnum>:IMS:SWEep:TYPE? |
Return Type |
Character |
Default |
NTH |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the order number of signals to view when SENS:IMS:SWE:TYPE NTH is specified. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<num> |
Order number of IM products to view. The frequency range is set to N (this number) x DeltaF (set with SENS:IMS:STIM:DFR). |
Examples |
SENS:IMS:SWEep:ORD 5 sense2:ims:sweep:order 12 |
Query Syntax |
SENSe<cnum>:IMS:SWEep:ORDer? |
Return Type |
Numeric |
Default |
9 |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the state of power coupling for F1 and F2. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<bool> |
Tone power level coupling. Choose from: ON (or 1) - F1 and F2 power is coupled. OFF (or 0) - F1 and F2 power is NOT coupled. Set power levels individually. |
Examples |
SENS:IMS:TPOW:COUP 0 sense2:ims:tpower:couple:state ON |
Query Syntax |
SENSe<cnum>:IMS:TPOWer:COUPle[:STATe]? |
Return Type |
Boolean |
Default |
ON |
Applicable Models: N522xB, N524xB (Read-Write) This command is replaced with SENS:IMS:TPOW:LEV Sets and returns the state of Equal Tone Power setting. Learn more about tone power. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<bool> |
Equal Tone Power state. Choose from: ON (or 1) - Equalize f1 and f2 power. OFF (or 0) - Do NOT equalize f1 and f2 power. Use source power cal. |
Examples |
SENS:IMS:TPOW:EQU 0 sense2:ims:tpower:equalize:state ON |
Query Syntax |
SENSe<cnum>:IMS:TPOWer:EQUalize:STATe? |
Return Type |
Boolean |
Default |
OFF |
Applicable Models: N522xB, N524xB (Read-Write) This command replaces SENS:IMS:TPOW:EQU and SENS:IMS:TPOW:SET Sets and returns the tone power leveling mode. |
|
Parameters |
|
<cnum> |
Channel number of the IMD measurement. If unspecified, value is set to 1. |
<char> |
Choose from: NONE - (Set Input Power) The specified f1 and f2 power levels are set at the DUT input. INPUT - (Set Input Power, receiver leveling) The specified f1 and f2 power levels are set at the DUT input using receiver leveling at the input reference receiver. EQUAL - (Set Input Power, equal tones at output) The specified f1 and f2 power levels are set at the DUT input and a measurement is made at the output. OUTPUT - (Set Output Power, receiver leveling) The specified f1 and f2 power levels are set at the DUT output. |
Examples |
SENS:IMS:TPOW:LEV INPUT sense2:ims:tpower:level output |
Query Syntax |
SENSe<cnum>:IMS:TPOWer:LEV? |
Return Type |
Character |
Default |
NONE |
Applicable Models: N522xB, N524xB (Read-Write) This command is replaced with SENS:IMS:TPOW:LEV Sets and returns whether tone power is specified at the DUT input or output. |
|
Parameters |
|
<cnum> |
Channel number of the IMSpectrum measurement. If unspecified, value is set to 1. |
<char> |
Choose from: INPUT - Specified power level is set at the DUT input. OUTPUT - Specified power level is set at the DUT output. |
Examples |
SENS:IMS:TPOW:SET INPUT sense2:ims:tpower:set output |
Query Syntax |
SENSe<cnum>:IMS:TPOWer:SET? |
Return Type |
Character |
Default |
INPUT |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the IMD channel number to which the IM Spectrum channel is coupled. |
|
Parameters |
|
<cnum> |
IMS channel. If unspecified, value is set to 1. |
<num> |
Existing IMD channel to which frequency and power settings are coupled. |
Examples |
SENS:IMS:TRAC:CHAN 2 sense2:ims:tracking:channel 1 |
Query Syntax |
SENSe<cnum>:IMS:TRACking:CHANnel? |
Return Type |
Numeric |
Default |
First IMD channel |
Applicable Models: N522xB, N524xB (Read-Write) Sets and returns the step sweep mode for the IM Spectrum channel. |
|
Parameters |
|
<cnum> |
IMS channel. If unspecified, value is set to 1. |
<bool> |
Choose from: OFF (or 0) - Automatic Step ON (or 1) - Manual Step |
Examples |
SENS:IMS:TRAC:MSEN 1 sense2:ims:tracking:msenable 0 |
Query Syntax |
SENSe<cnum>:IMS:TRACking:MSENable? |
Return Type |
Boolean |
Default |
0 - Automatic |
Applicable Models: N522xB, N524xB (Read-Write) When SENS:IMS:TRAC:MSEN = Manual, sets and returns the data point number at which a sweep is performed. |
|
Parameters |
|
<cnum> |
IMS channel. If unspecified, value is set to 1. |
<num> |
Step index. Choose from 1 to the specified number of points. |
Examples |
SENS:IMS:TRAC:SINDex 201 sense2:ims:tracking:sindex 1 |
Query Syntax |
SENSe<cnum>:IMS:TRACking:SINDex? |
Return Type |
Numeric |
Default |
1 |
Applicable Models: N522xB, N524xB (Read-Write) When an IMD channel exists, allows the IM Spectrum frequency and power setting to track (couple with) the IMD channel settings. |
|
Parameters |
|
<cnum> |
IMS channel. If unspecified, value is set to 1. |
<bool> |
Tracking state. Choose from: ON (or 1) - IM Spectrum frequency and power settings track the IMD channel settings. OFF (or 0) - IM Spectrum frequency and power settings are specified in the IMS channel. |
Examples |
SENS:IMS:TRAC:STAT 0 sense2:ims:tracking:state ON |
Query Syntax |
SENSe<cnum>:IMS:TRACking:STATe? |
Return Type |
Boolean |
Default |
OFF |