Sense:Power Command - Superseded


This command is superseded by the SOURce:POWer:ATTenuation:RECeiver:TEST command.

 

Learn about Receiver Attenuation

SENSe<cnum>:POWer:ATTenuator <recvr>,<num>

Applicable Models: N522xB, N523xB, N524xB

(Read-Write) Sets the attenuation level for the specified receiver.

Note: Attenuation cannot be set with Sweep Type set to Power

Note: For M980xA/P50xxA/E5080B Receiver Gain, use :SENS:SOUR:REC:GAIN.

Parameters

 

<cnum>

Any existing channel number. If unspecified, value is set to 1

<recvr>

Receiver to get attenuation. Choose from:

  • ARECeiver - receiver A

  • BRECeiver - receiver B

  • CRECeiver - receiver C

  • DRECeiver - receiver D

Receiver attenuation can NOT be set using logical receiver notation.

<num>

Attenuation value in dB.  

If a number other than these is entered, the analyzer will select the next lower valid value. For example, if 19 is entered for the E8361A/C, then 10 dB attenuation will be selected.

Examples

SENS:POW:ATT AREC,10
sense2:power:attenuator breceiver,30

Query Syntax

SENSe<cnum>:POWer:ATTenuator? <rec>

Return Type

Numeric

Default

0