Simulator (S94050B, S94051B)

Beginning with firmware release A.14.80.xx, all the features of the standard class are enabled by the simulator license. Without the license, the firmware enters Viewer Mode in which many of the features are disabled.

To install the VNA simulator, user has to

  1. Download and install the IO library if it is not installed. https://www.keysight.com/find/iolibs

  2. Download Firmware from Keysight web (https://www.keysight.com/find/pxiusbvna-firmware). The firmware supports the simulator capability for all models including PNA and ENA.

  3. Install the firmware to the PC. Follow the instructions for the installation.

  4. Execute the Keysight License Manager from Start Menu in Windows to install the license. Click “What if I have a license file to install”, then follow the instruction to install the license file. Learn more on option enable.

  5. You can open the Simulator setup dialog thru VNA SFP Launcher.  

In this topic:

VNA Simulator Setup Dialog (for PC or PXIe/USB VNA only)

 

Model Type  Select the series for simulator mode.

Model Number  Pulldown menu to select the model for simulator mode. It will change depending on the selected Model Type.

Number of Ports  To change the number of ports with the Up/Down button or edit that value using keyboard. Acceptable number as the number of ports is even number from 2 to 66. The maximum number of ports will change depending on the selected model.

Run  Start the firmware as Simulator mode with the selected setup. The selected Model Type, Model Number and Number of ports will be saved as new default values and these new default values will be used when the dialog will open next time.

Cancel Does not apply any changes and close the simulator setup dialog.  

Help  Open Help.

VNA Simulator License

One of the licenses below is required to enable VNA Simulator.

When no simulator license exists, VNA Simulator starts with Data Viewer Mode.

Simulator Mode

There are three simulator modes as below:

 

1. Data Viewer

Data Viewer is a free version of VNA Simulator and supports STD Channel with restrictions. Advanced functions including applications and remote-control capability are disabled.

 

2. Standard Simulator

All the features of the standard class are enabled by the simulator base license. The required license for the standard simulator is S94050B.

Standard Simulator supports STD Channel and remote-control capability. Applications are not supported.

 

3. Advanced Simulator

The S94051B is needed to enable advanced simulator.

Advanced Simulator supports Standard Simulator features + Applications (SW options) listed below.

VNA Family

Product

Supported Software Options

 

N522xB

S93xxx: 008, 010,011,015,025,029,082,083,084,086,087,088,089,090,094,118,322,460

PNA

N523xB

S93xxx: 008, 010,011,015,082,090,322

 

N524xB

S93xxx: 008, 010,011,015,025,029,082,083,084,086,087,088,089,090,094,110,111,118,322,460

ENA

E5080A

S96xxx: 008, 010,082,086

E5080B

S96xxx: 008, 010,011,015,025,029,082,083,084,086,088,090,460,111

E5081A

S96xxx:008, 010,015,025,029,070,082,083,084,086,090,111

 

M983xA

S95xxx: 008, 010,015,025,029,070,082,083,084,086,090,111

PXI

M980xA

S95xxx: 008, 010,011,015,025,029,070,082,083,084,086,088,089,090,460,111

 

M937xA

M9372A-xxx: 009,010

Streamline

(USB VNA)

P50xxA/B

S97xxx: 008, 010,011,015,025,029,082,083,084,086,088,090,460,111

P937xA/B

P938xB

S97xxx: 010,082

 

The following options are not supported.

Hardware options:

The external devices such as source, power sensor are not supported. PXI internal devices such as the switch and M9341A/B Digital IO supports GUI only.

Dummy DUT

Dummy DUT capability provides measurement data manipulation for VNA simulator using the following format files.

The following data can be recalled from Dummy DUT dialog box. They can be stored under Save Recall > Save Others > Save Data...

The selection of GCA Sweep Data and GCX Sweep Data is shown only when the Gain Compression parameters are measured.

The data acquisition mode must be 2D (either Sweep Power per Frequency or Sweep Frequency per Power).

 

VNA Simulator automatically loads a “default” dummy DUT put under VNA installed folder (C:\Program Files\Keysight\Network Analyzer\simulations\DummyDUT.s6p)

Users can set their own default dummy DUT under user VNA document folder (C:\Users\Public\Documents\Network Analyzer\UserDummyDUT.s*p)

When there are multiple “UserDummyDUT.s*p” files, VNA simulator loads the first found one.

 

Dummy DUT Tool provides GUI for dummy DUT handling. The tool is Installed under VNA Macro softkey.

How to create Dummy DUT snp file

Use one of the following methods to make a dummy DUT snp file

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Macro > Macro1 > Dummy DUT tool

  1. Click Utility > Macro  > Dummy DUT tool [dummyduttool...]

Programming Commands

 

Current DUT  Show sNp file currently used as dummy DUT

Load...  Load user specific sNp file as current dummy DUT

Clear  Clear current dummy DUT

Noise  Set noise state ON/OFF

Save Current As User Default  Save current dummy DUT as user default

Calibration Simulation

Mechanical Calibration Kit Simulation

If you have an SnP file of the condition of open, short and load, the normal calibration can be simulated.

  1. Execute the dummy DUT dialog box

  2. Execute Smart Cal.

  3. Since Dummy DUT dialog box is hidden behind the GUI, make it visible by using Alt+Tab. Then, Load the SnP file of the open condition.

  4. Take a open calibration.

  5. Continue this for Short and Load.

ECal Simulation

The following two simulated ECal modules are available in the simulator.

Ecal Name

Model Number

Serial Number

Number of Ports

SimEcal4

129

SN00000000

4

SimEcal2

130

SN00000000

2

 

The simulated ECals do the followings: