Interface Control


The Interface Control feature allows you to send remote commands and data to the following VNA rear-panel Interfaces: GPIB, Material Handler I/O, and Auxiliary I/O.

Other System Configuration Topics

Overview

The Interface Control feature allows you to send data to control external equipment such as GPIB instruments, a material handler or other equipment, without needing to create a remote program. The VNA manages the timing and required interface setup. See Rear Panel Tour.

  1. GPIB Interface

  2. Material Handler Interface

  3. Dwell Time

How to access Interface Control settings

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Setup > Internal Hardware > Interface Control...

  1. Click Instrument

  2. Select Setup
  3. Select Internal Hardware

  4. Select Interface Control...

Programming Commands

Interface Control dialog box help

Dwell After Command  Specifies a wait time, in milliseconds, after all commands to all interfaces are sent. Any positive integer is allowed. This is used to allow all external devices to settle before beginning a measurement. An erratic trace could indicate that more settling time is necessary.

Reset All  Sets ALL fields on ALL channels to their default values.

Save and Recall  Saves and recalls the contents of this dialog box. If the Interface Control dialog box is populated with settings during an Instrument State Save, the settings are automatically recalled with the Instrument State settings.

Interface control uses an *.xml file type. An example file is stored on the VNA hard drive. You can recall it into the dialog, or you can open and edit it with a word processor, such as Word Pad.

OK  Applies the settings and closes the dialog box.

Cancel  Does not apply changes that were made, and closes the dialog box.