Setup Commands - Standard Measurement Class

Click here to view links to Setup commands for all Measurement Classes.

Main

Layout

System
Setup

Internal
Hardware

External
Hardware

 

Main Tab Commands
Softkey Sub-item SCPI

COM

Sweep Setup...   Sweep Type
Linear Frequency SENSe:SWEep:TYPE
Log Frequency SENSe:SWEep:TYPE
Power Sweep SENSe:SWEep:TYPE
CW Time SENSe:SWEep:TYPE
Segment Sweep SENSe:SWEep:TYPE
Phase Sweep SENSe:SWEep:TYPE
Sweep Properties
Start SENSe:FREQuency:STARt
Stop SENSe:FREQuency:STOP
Power SOURce:POWer[:LEVel][:IMMediate][:AMPLitude]
Points SENSe:SWEep:POINts
IF Bandwidth SENSe:BWIDth[:RESolution]
Start Power SOURce:POWer:STARt
Stop Power SOURce:POWer:STOP
CW Freq SENSe:FREQuency[:CW]
Segment Table
X-axis Point Spacing SENSe:SEGMent:X:SPACing
Allow arbitrary Segments SENSe:SEGMent:ARBitrary
Display Center/Span Freq SENSe:SEGMent:FREQuency:CENTer SENSe:SEGMent:FREQuency:SPAN
Timing
Sweep Time SENSe:SWEep:TIME
Dwell Time SENSe:SWEep:DWELl
Sweep Delay SENSe:SWEep:DWELl:SDELay
Auto Sweep Time SENSe:SWEep:TIME:AUTO
Fast Sweep - Reduce settling time SENSe:SWEep:SPEed
Sweep Mode SENSe:SWEep:GENeration
Sweep Sequence SENSe:SWEep:GENeration:POINtsweep

Meas Class...

  CALCulate:MEASure:DEFine
Quick Start... S-Param CALCulate:MEASure:PARameter
Balanced CALCulate:MEASure:PARameter
Other CALCulate:MEASure:PARameter
Layout Tab Commands
Softkey Sub-item SCPI

COM

New Trace   DISPlay:WINDow:TRACe[:STATe]
New Channel   None
New Window   DISPlay:WINDow[:STATe]
New Sheet   DISPlay:SHEet:STATe
Delete TrN DISPlay:WINDow:TRACe:DELete
ChN SYSTem:CHANnels:DELete
WinN DISPlay:WINDow[:STATe]
Select TrN DISPlay:WINDow:TRACe:SELect
ChN None
WinN DISPlay:WINDow:TRACe:SELect
Measure... S-Parameter CALCulate:MEASure:PARameter
Balanced CALCulate:MEASure:PARameter
Receivers CALCulate:MEASure:PARameter
Meas Class...   CALCulate:MEASure:DEFine
Internal Hardware Tab Commands
Softkey Sub-item SCPI

COM

Receiver Gain

 

SENSe:SOURce:RECeiver:GAIN

 
PXI Devices M9379A Amp Setup... SENS:AMPL:M9379:

 

M9341 I/O Control Setup... (Handler Tab) CONT:HAND (DUT Control Tab) SENSe:DUTControl:M9341 (Analog In Tab) SENS:DC:DC:VOLT:RANG                        SENS:DC:SAMP:TIME, SENS:DC:SAMP:POIN (Analog Out Tab) SENS:DC:DC:CURR:RANG                          SOUR:DC:PROT:RES                          SOUR:DC:VOLT:CAL:EXEC                          SOUR:DC:VOLT:CAL:DATE, TIME

 

M9111 SMU Setup... SOUR:DC

 

Reference...

Reference In

SENSe:ROSCillator:EXTernal:FREQuency

 

Internal/External

SENSe:ROSCillator:SOURce

SENSe:ROSCilator:SOURce:CATalog

 

Distrubuted VNA   SYSTem:PREFerences:DVNA:STATe  

External Hardware Tab Commands

Softkey

Sub-item

SCPI

COM

External Device...

New

SYSTem:CONFigure:EDEVice:ADD

Remove

SYSTem:CONFigure:EDEVice:REMove

Name

SYSTem:CONFigure:EDEVice:ADD

Device Type

SYSTem:CONFigure:EDEVice:DTYPe

Driver

SYSTem:CONFigure:EDEVice:DRIVer

Active - Show in UI

SYSTem:CONFigure:EDEVice:STATe

Device Properties...

DC Meter

Timeout

None

Dwell Before Sweep

SYSTem:CONFigure:EDEVice:DC:DSWeep

Dwell After Point Set

SYSTem:CONFigure:EDEVice:DC:DPOint

Type

SYSTem:CONFigure:EDEVice:DC:TYPE

Receiver Correction On

SYSTem:CONFigure:EDEVice:DC:CORRection

Offset

SYSTem:CONFigure:EDEVice:DC:OFFSet

Scaling

SYSTem:CONFigure:EDEVice:DC:SCALe

Edit Commands...

 

ID Query

SYSTem:CONFigure:EDEVice:DC:QUERy:ID

Error Query

SYSTem:CONFigure:EDEVice:DC:QUERy:ERRor

Enable I/O

SYSTem:CONFigure:EDEVice:DC:COMMand:INIT

Disable I/O

SYSTem:CONFigure:EDEVice:DC:COMMand:EXIT

Before Sweep

SYSTem:CONFigure:EDEVice:DC:COMMand:SWEep:BEFore

After Sweep

SYSTem:CONFigure:EDEVice:DC:COMMand:SWEep:AFTer

Abort Sweep

SYSTem:CONFigure:EDEVice:DC:COMMand:SWEep:ABORt

Point Set Commands

SYSTem:CONFigure:EDEVice:DC:COMMand:POINt:SET

DC Source

Timeout

None

Dwell Before Sweep

SYSTem:CONFigure:EDEVice:DC:DSWeep

Dwell After Point Set

SYSTem:CONFigure:EDEVice:DC:DPOint

Type

SYSTem:CONFigure:EDEVice:DC:TYPE

 

SYSTem:CONFigure:EDEVice:DC:LIMit:CURRent

 

SYSTem:CONFigure:EDEVice:DC:LIMit:VOLTage

Edit Commands...

 

ID Query

SYSTem:CONFigure:EDEVice:DC:QUERy:ID

Error Query

SYSTem:CONFigure:EDEVice:DC:QUERy:ERRor

Enable I/O

SYSTem:CONFigure:EDEVice:DC:COMMand:INIT

Disable I/O

SYSTem:CONFigure:EDEVice:DC:COMMand:EXIT

Read Max Using

SYSTem:CONFigure:EDEVice:DC:MAX:VALue

Define Max As

SYSTem:CONFigure:EDEVice:DC:MAX[:STATe]

SYSTem:CONFigure:EDEVice:DC:MAX:VALue

Read Min Using

SYSTem:CONFigure:EDEVice:DC:MIN:VALue

Define Min As

SYSTem:CONFigure:EDEVice:DC:MIN[:STATe]

SYSTem:CONFigure:EDEVice:DC:MIN:VALue

Before Sweep

SYSTem:CONFigure:EDEVice:DC:COMMand:SWEep:BEFore

After Sweep

SYSTem:CONFigure:EDEVice:DC:COMMand:SWEep:AFTer

Abort Sweep

SYSTem:CONFigure:EDEVice:DC:COMMand:SWEep:ABORt

Point Set Commands

SYSTem:CONFigure:EDEVice:DC:COMMand:POINt:SET

Hybrid Source

Input Source Carrier Frequency

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:FREQuency:CARRier

Input Multiplier

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:FREQuency:MULTiplier

Input Source Name

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:NAME

Input Source Power Limit

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:POWer:LIMit

Enable Pulse (Input)

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:INPut:PULSe:ENABle

LO Multiplier

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LO:FREQuency:MULTiplier

LO Source Name

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LO:NAME

LO Power

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LO:POWer

Enable Pulse (LO)

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LO:PULSe:ENABle

Lock Dependent Sources

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:LOCK:STATe

Freq Max (SSB Mixer)

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:OUTPut:FREQuency:MAX

Freq Min (SSB Mixer)

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:OUTPut:FREQuency:MIN

Gain (SSB Mixer)

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:OUTPut:GAIN

Equation (SSB Mixer)

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:OUTPut:MIXer:SIDeband

Hybrid Type

SYSTem:CONFigure:EDEVice:SOURce:HYBRid:TYPE

Power Meter

Sensor A/B

None

Tolerance

SOURce:POWer:CORRection:COLLect:AVERage:NTOLerance

Max Number of Readings

SOURce:POWer:CORRection:COLLect:AVERerage:COUNt

Use Loss Table

SOURce:POWer:CORRection:COLLect:TABLe:LOSS

SOURce:POWer:CORRection:COLLect:TABLe:SELect

Edit Table

SOURce:POWer:CORRection:COLLect:TABLe:POINts?

SOURce:POWer:CORRection:COLLect:TABLe:FREQuency

SOURce:POWer:CORRection:COLLect:TABLe:DATA

Uncertainty...

SYSTem:CONFigure:EDEVice:PMAR:UNCertainty:CATalog?

SYSTem:CONFigure:EDEVice:PMAR:UNCertainty:FILE

SYSTem:CONFigure:EDEVice:PMAR:UNCertainty:MODel

SYSTem:CONFigure:EDEVice:PMAR:UNCertainty:PLEVel?

SYSTem:CONFigure:EDEVice:PMAR:UNCertainty:READ?

Linearity

SYSTem:CONFigure:EDEVice:PMAR:LINearity

Pulse Generator

Time out

SYSTem:CONFigure:EDEVice:TOUT

Primary Mode

SYSTem:CONFigure:EDEVice:PULSe:PMODe

Output

SYSTem:CONFigure:EDEVice:PULSe:CHAN

High

SYSTem:CONFigure:EDEVice:PULSe:HAMP

Low

SYSTem:CONFigure:EDEVice:PULSe:LAMP

Source Imp

SYSTem:CONFigure:EDEVice:PULSe:SIMP

Load Imp

SYSTem:CONFigure:EDEVice:PULSe:LIMP

SMU

Setup

 

Chan N

SYSTem:CONFigure:EDEVice:ADD

Trigger Mode

SYSTem:CONFigure:EDEVice:SOURce:TMODe

SMU Trigger In

 

SMU Trigger Out

 

Source/Voltage Meter/Current Meter

 

SMU Chan

SYSTem:CONFigure:EDEVice:IOENable

SYSTem:CONFigure:EDEVice:SMU:CHANnel[1-4]:STATe

Source type

SYSTem:CONFigure:EDEVice:DC:TYPE

Timeout

SYSTem:CONFigure:EDEVice:TOUT

Dwell Before Sweep

SYSTem:CONFigure:EDEVice:DC:DSWeep

Dwell After Point Set

SYSTem:CONFigure:EDEVice:DC:DPOint

Current Limit

SYSTem:CONFigure:EDEVice:DC:LIMit:CURRent

Voltage Limit

SYSTem:CONFigure:EDEVice:DC:LIMit:VOLTage

Source Correction On

SYSTem:CONFigure:EDEVice:DC:CORRection

Offset

SYSTem:CONFigure:EDEVice:DC:OFFSet

Scaling

SYSTem:CONFigure:EDEVice:DC:SCALe

Receiver Correction On

SYSTem:CONFigure:EDEVice:DC:CORRection

Edit Commands - DC Source

 

Edit Commands - DC Meter

 

Source

Enable Output
(multi-channel sources)

SYSTem:CONFigure:EDEVice:CHANnel<cnum>:BASE

SYSTem:CONFigure:EDEVice:CHANnel<cnum>:COUNt

SYSTem:CONFigure:EDEVice:CHANnel<cnum>:NAME

SYSTem:CONFigure:EDEVice:CHANnel<cnum>:NUMBer

SYSTem:CONFigure:EDEVice:CHANnel<cnum>[:STATe]

SYSTem:CONFigure:EDEVice:CHANnel:SYNC

Timeout

SYSTem:CONFigure:EDEVice:TOUT

Dwell Per Point

SYSTem:CONFigure:EDEVice:SOURce:DPP

Enable Modulation Control

SYSTem:CONFigure:EDEVice:SOURce:MODulation:CONTrol[:STATe]

Trigger Mode

SYSTem:CONFigure:EDEVice:SOURce:TMODe

Trigger Port

SYSTem:CONFigure:EDEVice:SOURce:TPORt

Edit Commands...

 

Operation complete (*OPC)

None

Preset

None

Set CW Frequency

None

Set CW Sweep Mode

None

Set Power

None

Set Power State

None

Power Meter Setup...

Interface

SYSTem:COMMunicate:GPIB:PMETer:CATalog?

SYSTem:COMMunicate:USB:PMETer:CATalog?

Sensors

SYSTem:CONFigure:EDEVice:PMAR:SENSor

Tolerance

SYSTem:CONFigure:EDEVice:PMAR:READing:NTOLerance

Max Number of Readings

SYSTem:CONFigure:EDEVice:PMAR:READing:COUNt

Use Loss Table

SYSTem:CONFigure:EDEVice:PMAR:TABle:LOSS:DATA

Edit Table

SYSTem:CONFigure:EDEVice:PMAR:TABle:LOSS:DATA