Last updated: 2014-11-28
Before originating a call from the test set, you must set Channel Type to the appropriate setting.
The UE can be paged using either an IMSI (International Mobile Subscriber Identity) or TMSI (Temporary Mobile Subscriber Identity):
To page the UE using its IMSI, set Paging Identity Type to IMSI. If you know the UE's IMSI, you can enter it under Paging IMSI (CALL:PAGing:IMSI[:SELected]) and proceed directly to originating a call even if the UE has not registered. Otherwise, you must wait for the UE to report its IMSI upon registering with the test set.
To page the UE using a TMSI, the UE must first be assigned a TMSI during the Location Update procedure. You must then set Paging Identity Type to TMSI , then originate a call from the test set.
To originate a call from the test set, select Originate Call or send the CALL:ORIGinate command. Press the same button or send the CALL:END command to end the call, which will abort the current call processing operation and returns call status to "Idle".
|
|
|
GPIB Commands: CALL:ORIGinate, CALL:END