Last updated: 2010-03-10
For more information on the GPIB Command conventions, see GPIB Command conventions
See Out-of-Synchronization of Output Power (OOS) Measurement for the measurement description.
|
Function |
Sets/queries Segment Ta-b Interval. |
|
Setting |
Range: 40 to 5000 ms Resolution: 40 ms |
|
Query |
Same as setting |
|
*RST Setting |
5000 ms |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TOOSynch:INTerval:AB 5000 ms" |
|
Function |
Sets/queries Segment Tc-d Interval. |
|
Setting |
Range: 40 to 5000 ms Resolution: 40 ms |
|
Query |
Same as setting |
|
*RST Setting |
5000 ms |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TOOSynch:INTerval:CD 5000 ms" |
|
Function |
Sets/queries Segment Td-e Interval. |
|
Setting |
Range: 40 to 5000 ms Resolution: 40 ms |
|
Query |
Same as setting |
|
*RST Setting |
5000 ms |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TOOSynch:INTerval:DE 5000 ms" |
|
Function |
Sets/queries DPCH Quality Ratio A-B. |
|
Setting |
Range: -20 to 0 dB Resolution: 0.1 |
|
Query |
Same as setting |
|
*RST Setting |
-6 dB |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TOOSynch:RATio:AB -6" |
|
Function |
Sets/queries DPCH Quality Ratio B-D. |
|
Setting |
Range: -20 to 0 dB Resolution: 0.1 |
|
Query |
Same as setting |
|
*RST Setting |
-16 dB |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TOOSynch:RATio:BD -16" |
|
Function |
Sets/queries DPCH Quality Ratio D-E. |
|
Setting |
Range: -20 to 0 dB Resolution: 0.1 |
|
Query |
Same as setting |
|
*RST Setting |
-14 dB |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TOOSynch:RATio:DE -14" |
|
Function |
Sets/queries DPCH Quality Ratio E+. |
|
Setting |
Range: -20 to 0 dB Resolution: 0.1 |
|
Query |
Same as setting |
|
*RST Setting |
-3 dB |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TOOSynch:RATio:E -3" |
|
Function |
The setting form of this command performs two functions: (1) sets the measurement's timeout (see Measurement Timeout) value, and (2) sets the measurement's timeout STATe to 1 (on). The query form returns the measurement's timeout value. |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second |
|
Query |
Same as setting |
|
*RST Setting |
20 seconds, (off) |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TOOSynch:TIMeout 5" |
|
Function |
Sets/queries the measurement's timeout state (see Measurement Timeout) |
|
Setting |
Range: 1|ON|0|OFF |
|
Query |
Range: 1|0 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TOOSynch:TIMeout:STATe 0" |
|
Function |
Sets/queries the measurement's timeout setting to be used when the timeout state is set to ON (see Measurement Timeout). |
|
Setting |
Range: 0.1 to 999.9 seconds Resolution: 0.1 second |
|
Query |
Same as setting |
|
*RST Setting |
20 seconds |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TOOSynch:TIMeout:TIME 20" |
|
Function |
Sets/queries the link transmission mode (see Transmission Mode). |
|
Setting |
Range: Continue/Discontinue |
|
Query |
Same as setting |
|
*RST Setting |
Continue |
|
Requirements |
Test Application Revision: A.05.00 and above |
|
Programming Example |
"SETup:TOOSynch:TRANsmission:MODE Continue" |
|
Function |
Sets/queries the OOS trigger to be routed to the rear panel TRIG OUT. The test set provides two trigger modes:
This setting is GPIB only. |
|
Setting |
Range: ONE | MULTiple |
|
Query |
Range: ONE | MULT |
|
*RST Setting |
ONE |
|
Requirements |
Test Application Revision: A.04.00 and above |
|
Programming Example |
"SETup:TOOSynch:TRIGger:OUTPut:SUBFrames ONE" |