Last updated: November 11, 2010
This section is only applicable to the lab application or feature-licensed test application.
The
Recorded E-TFCI Information
screen displays the
E-TFCI Recording State
,
Current E-TFCI Boost
,
Recorded E-TFCI Values
and
Number of E-TFCI Results Recorded
. These results are set to their default values if you select
Measurement Reset
, when the
Operating Mode
changes, when a new HSPA connection is established in
Active Cell Operating Mode
, or when
Channel Type
changes to/from
12.2k RMC + HSPA
while in
FDD Test Operating Mode
. The results are also set to their default values if you select
Clear UE Info
when the test set is not recording.
This result indicates whether the test set is currently recording a sequence of E-TFCI values from the UE. Possible states include
Recording
and
Idle.
GPIB command: CALL:STATus:ETFCi:RECord[:STATe]?
GPIB command: CALL:STATus:ETFCi:BOOSt?
This result returns the sequence of E-TFCI values recorded when the Start Recording E-TFCI Values action was initiated.
GPIB command: CALL:STATus:ETFCi:RECord:ALL?
The number of E-TFCI results recorded is displayed at the bottom of the
Recorded E-TFCI Values
window (as shown circled above). When recording is active, this result is updated every 0.5 s. When recording is idle, this result indicates the number of E-TFCIs in the
Recorded E-TFCI Values
result.
GPIB command: CALL:STATus:ETFCi:RECord:COUNt?