How Do I Change Call Parameters?

How Do I Change Call Parameters?

Last updated: January 15, 2009

Setting Call Parameters

  1. Press the CALL SETUP key.
  2. Press the right More key to move between the Call Parms menus and set the call parameters as needed.

Setting Call Parameters that Can Only Be Changed in Cell Off Mode

  1. Press the CALL SETUP key.
  2. Set Operating Mode ( F1 ) to Cell Off .
  3. Press the right More key to move between the Call Parms menus and change the call parameters as needed.
  4. Set Operating Mode ( F1 ) to Active Cell .

Related Topics


Channel Type

Paging Service

How Do I Change HSUPA Parameters?

How Do I Change HSDPA Parameters?

Channel (UARFCN) Parameters

Signalling Radio Bearer (SRB) Parameters

Other Downlink Parameters

Uplink Closed Loop Power Control Parameters and UE Target Power