Last updated: January 15, 2009
This section is only applicable to the lab application.
Function |
Sets/queries Access Class Barred . This setting can only be changed when Call
Status is |
Setting |
Range: 16 characters from the set 0 and 1 |
Query |
Range: 16 characters from the set 0 and 1 |
*RST Setting |
1111111111111111 |
Requirements |
Lab Application Revision: J.01.00 and above |
Programming Example OUTPUT 714;"CALL:AREStriction:ACBarred 1111111111111111" ! Sets Access Class Barred List to 1111111111111111. |
|
Sets/queries Cell Barred State . This setting
can only be changed when call status is |
|
| 0 (Off) | |
OUTPUT 714;"CALL:AREStriction:BARRed:STATe 1" ! Sets Barred State to On. |
|
Sets/queries the Cell Barred Timer (Tbarred) . This setting
is only applicable when CALL[:CELL]:AREStriction:BARRed:STATe
is set to This setting
can only be changed when call status is |
|
| Same as setting | |
| 40 s | |
OUTPUT 714;"CALL:AREStriction:BARRed:TIMer 20s" ! Sets Barred Timer to 20 s. |
|
Sets/queries the Intra-frequency Cell Reselection Indicator . This setting
is only applicable when CALL[:CELL]:AREStriction:BARRed:STATe
is set to This setting
can only be changed when call status is |
|
| ALL | |
OUTPUT 714;"CALL:AREStriction:ITAFrequency:CRINdicator NALLowed" ! Sets the Intra-frequency Cell Reselection Indicator to Not Allowed. |
|