This section is only applicable to the lab application.
These settings
can only be changed when call status is
Idle . If BCCH Update Page
is set to Auto and
you change these settings while your UE is camped to the test
set, the test set performs a Broadcast Channel
(BCCH) Update Procedure (SIB Contents) . If
BCCH Update Page is set to
Inhibit (the default value) and you change these settings
while your UE is camped to the test set, you must force your UE
to re-read the BCCH to observe the change (see BCCH
Update Page for more details).
You can specify whether the S intersearch information element (see 3GPP TS 25.331 10.3.2.3 and 3GPP TS 25.304 5.2.6.1.5) is sent in SIB3 by the test set, and if included, what value is sent. S intersearch controls whether the UE must make measurements of inter-frequency cells while camped. If the quality of the serving cell is above S intersearch , then the UE will not measure other inter-frequency cells while camped. If S intersearch is not present, the UE must make inter-frequency measurements while camped. Note that if the UE does not make measurements on other cells, it will not reselect away from the current cell, even if there is another cell at a higher signal level. See 3GPP TS 25.304 5.2.6.1.1.
When Sintersearch is
On , it can be set to any even number value between
-32 dB and +20 dB, but any negative value will be interpreted
by the UE as 0 dB.
When Sintersearch is
Off , the S intersearch
information element is not included in SIB3.
Note, the Sintersearch parameter does
not affect measurements performed by the UE while on a connection
(see UE
Reported Measurements ).
GPIB command: CALL[:CELL]:BCCHannel:SERSearch[:SVALue] .
You can specify whether the S intrasearch information element (see 3GPP TS 25.331 10.3.2.3 and 3GPP TS 25.304 5.2.6.1.5) is sent in SIB3 by the test set, and if included, what value is sent. S intrasearch controls whether the UE must make measurements of intra-frequency cells while camped. If the quality of the serving cell is above S intrasearch , then the UE will not measure other intra-frequency cells while camped. If S intrasearch is not present, the UE must make intra-frequency measurements while camped. Note that if the UE does not make measurements on other cells, it will not reselect away from the current cell, even if there is another cell at a higher signal level. See 3GPP TS 25.304 5.2.6.1.1.
When Sintrasearch is
On , it can be set to any even number value between
-32 dB and +20 dB, but any negative value will be interpreted
by the UE as 0 dB.
When Sintrasearch is
Off , the S intrasearch
information element is not included in SIB3.
Note, the Sintrasearch parameter does
not affect measurements performed by the UE while on a connection
(see UE
Reported Measurements ).
GPIB commands: CALL[:CELL]:BCCHannel:SRASearch[:SVALue] .
This parameter sets the 3GPP TS 25.331 s10.3.2.3, "Cell selection and reselection quality measure" information element. This parameter specifies whether the UE should use CPICH Ec/N0 or CPICH RSCP as the quality measure for determining which cell to choose when performing a cell selection or mobile-initiated cell reselection.
Note, this
setting does not affect what measurements are reported to
the test set by the UE. When Report Measurement
Type is set to Intra-frequency
or All , the UE
will make both CPICH Ec/N0 and CPICH RSCP measurements, regardless
of the Quality Measure setting
(the Measurement Control message sent by the test set instructs
it to do so).
GPIB command: CALL[:CELL]:RESelection:QUALity:MEASure .
This parameter sets the 3GPP TS 25.331 s10.3.2.3 "Qhyst1" information element. Qhyst1 specifies the hysteresis value to be used by the UE if Quality Measure is CPICH RSCP.
GPIB command: CALL[:CELL]:RESelection:HYSTeresis[1] .
This parameter sets the 3GPP TS 25.331 s10.3.2.3 "Qhyst2" information element. Qhyst2 specifies the hysteresis value to be used by the UE if Quality Measure is CPICH Ec/N0.
GPIB command: CALL[:CELL]:RESelection:HYSTeresis2 .
This parameter sets 3GPP TS 25.331 s10.3.2.3 "Qqualmin" for FDD in the "Cell selection and re-selection info for SIB11/12" information element (see 25.331 s10.3.2.4). According to 3GPP TS 25.304 s5.2.6.1.4, Qqualmin is the "minimum required quality level in the cell (dB)". If Quality Measure is set to CPICH Ec/N0, the UE compares the CPICH Ec/N0 it measures for the cell with Qqualmin to determine if it may select/reselect to the cell.
GPIB command: CALL[:CELL]:RESelection:QUALity:LMINimum .
This parameter sets 3GPP TS 25.331 s10.3.2.3 "Qrxlevmin" for FDD in the "Cell selection and re-selection info for SIB11/12" information element (see 25.331 s10.3.2.4). According to 3GPP TS 25.304 s5.2.6.1.4, Qrxlevmin is the "minimum required RX level in the cell (dBm)". If Quality Measure is set to CPICH RSCP, the UE compares the CPICH RSCP it measures for the cell with Qrxlevmin to determine if it may select/reselect to the cell.
GPIB command: CALL[:CELL]:RESelection:RLMinimum .
This parameter sets the 3GPP TS 25.331 s10.3.2.3 "Treselection" information element. 3GPP TS 25.304 s5.2.6.1.4 states that the UE shall only reselect to a cell if it "is better ranked than the serving cell during a time interval Treselection".
GPIB command: CALL[:CELL]:RESelection:TIMer .
This section is only applicable to the lab application.
These settings
can only be changed when call status is
Idle . If BCCH Update Page
is set to Auto and
you change these settings while your UE is camped to the test
set, the test set performs a Broadcast Channel
(BCCH) Update Procedure (SIB Contents) . If
BCCH Update Page is set to
Inhibit (the default value) and you change these settings
while your UE is camped to the test set, you must force your UE
to re-read the BCCH to observe the change (see BCCH
Update Page for more details).
These parameters are sent in the Cell Access Restriction information element on SIB3. See 3GPP TS 25.331 s10.3.2.1.
According to 3GPP TS 25.304, a "Barred Cell" is "a cell a UE is not allowed to camp on." A UE is not allowed to camp on a barred cell, not even for emergency calls. If a cell on which a UE is currently camped becomes barred, a cell reselection is triggered.
This parameter controls whether the test set is a barred cell. It sets the 3GPP TS 25.331 s10.3.2.1 "Cell Barred" information element.
GPIB command: CALL[:CELL]:AREStriction:BARRed:STATe .
This parameter sets the 3GPP TS 25.331 s10.3.2.1 "T barred " information element. T barred specifies the time the UE must wait before considering a barred cell for reselection (see 3GPP TS 25.304 s5.3.1.1).
This setting
is only applicable when Cell Barred State
is set to On .
GPIB command: CALL[:CELL]:AREStriction:BARRed:TIMer .
This parameter set the 3GPP TS 25.331 s10.3.2.1 "Intra-frequency cell re-selection indicator" information element. According to 3GPP TS 25.304 s5.3.1.1, if a cell is barred, the UE must select another cell as follows:
This setting
is only applicable when Cell Barred State
is set to On .
GPIB command: CALL[:CELL]:AREStriction:ITAFrequency:CRINdicator .
This parameter sets the Access Class Barred List in IE Cell Access Restriction. Each bit represents one Access Class, the leftmost one represents Access Class 0, and the rightmost one represents Access Class 15. If one bit is set to 0, its corresponding Access Class is Barred.
This setting
can only be changed when Call Status is
Idle .
GPIB command: CALL[:CELL]:AREStriction:ACBarred.
The following
settings, with the exception of the T3312 Periodic
RA Update Timer and T3312 Periodic RA Update
Units settings, can only be changed when call status is Idle . If
BCCH Update Page is set to
Auto and you change these settings while your UE is camped
to the test set, the test set performs a Broadcast
Channel (BCCH) Update Procedure (SIB Contents) . If
BCCH Update Page is set to
Inhibit (the default value) and you change these settings
while your UE is camped to the test set, you must force your UE
to re-read the BCCH to observe the change (see BCCH
Update Page for more details).
This setting is only applicable to the lab application.
This setting determines how long the UE waits for the RRC Connection Setup after sending an RRC Connection Setup Request.
T300 can be set to one of the following values: 100, 200, 400, 600, 800, 1000, 1200, 1400, 1600, 1800, 2000, 3000, 4000, 6000, or 8000 ms.
GPIB command: CALL[:CELL]:BCCHannel:T300
This setting is only applicable to the lab application.
This setting specifies the maximum number of retransmissions of the RRC Connection Request message.
N300 can be set to any integer value from 0 to 7.
GPIB command: CALL[:CELL]:BCCHannel:N300
This setting is only applicable to the lab application.
This setting determines how long the UE waits for an N312 "in-sync" indication from layer 1 when establishing a dedicated channel and the connection status is idle. According to 3GPP TS 25.331 table 10.3.3.43, zero (0) can be signaled in the SIB1 message but has no meaning.
T312 can be set to any integer value from 1 to 15.
GPIB command: CALL[:CELL]:BCCHannel:T312[:IDLE]
This setting is only applicable to the lab application.
This setting specifies the number of " in-syncs" required when establishing a dedicated channel when the connection status is in Idle mode.
N312 can be set to one of the following values: 1, 2, 4, 10, 20, 50, 100, 200, 400, 600, 800, or 1000.
GPIB command: CALL[:CELL]:BCCHannel:N312[:IDLE]
This setting is only applicable to the lab application.
This setting specifies the amount of time between transmissions of the RRC Connection Release Complete message.
T308 can be set to one of the following values: 40, 80, 160, or 320 ms.
GPIB command: CALL[:CELL]:BCCHannel:T308
This setting is only applicable to the lab application.
This setting specifies the maximum number of times the RRC Connection Release Complete message is sent.
N308 can be set to any integer value from 1 to 8.
GPIB command: CALL[:CELL]:RRC:CRELease:N308
This setting is only applicable to the lab application.
This setting determines whether the test set keeps the uplink DPCH active until it has received all the RRC Connection Release Complete messages or whether it releases the DPCH and returns to Idle mode as soon as the first RRC Connection Release Complete message is received. Note: This parameter only controls the test set's behavior; it is not signaled to the UE.
You can choose from the following settings:
N308 ): The test set keeps the DPCH active until
all the RRC Connection Release Complete messages have
been received. RETRansmit1 ): The
test set releases the DPCH upon the reception of the first
RRC Connection Release Complete Message.GPIB command: CALL[:CELL]:RRC:CRELease:CWCount
T313 Out-Of-Sync Reception Timer
3GPP TS 25.331 8.5.6 states that after receiving N313 consecutive "out of sync" indications from layer 1 (see N313 Successive Out-Of-Sync Reception Max ), the UE shall start the T313 timer. Upon receiving N315 successive "in sync" indications from layer 1 ( N315 Successive In-Sync Reception Counter ), the UE shall stop and reset the T313 timer. If T313 expires, a "Radio Link failure" has occurred, and the UE shall drop the call. See 3GPP TS 25.214 4.3.1.2 for more details regarding "in sync" and "out of sync" indications.
T313 can be set to an integer value between 0 and 15 seconds.
GPIB command: CALL[:CELL]:BCCHannel:T313
N313 Successive Out-Of-Sync Reception
Max
N313 can be set to one of the following integer values: 1, 2, 4, 10, 20, 50, 100, 200.
GPIB command: CALL[:CELL]:BCCHannel:N313
N315 Successive In-Sync Reception
Counter
N315 can be set to one of the following integer values: 1, 2, 4, 10, 20, 50, 100, 200, 400, 600, 800, 1000.
GPIB command: CALL[:CELL]:BCCHannel:N315
T309 CCO From UTRAN to 2G Connect
Timer
This setting is only applicable to the lab application.
This setting determines the amount of time the UE waits to establish a connection on the 2G side after a Cell Change Order from UTRAN.
The T309 timer can be set to any integer from 0 to 8 seconds.
GPIB command: CALL[:CELL]:BCCHannel:T309
T3212 Periodic Location Update Timer
This setting is only applicable to the lab application.
T3212 controls how often the UE performs the periodic location update procedure (see Performing a Location Update (CS Domain Registration) ). It can be set between 0 and 255 decihours (1 decihour = 6 minutes). T3212 is signaled in SIB1 as part of the "CS domain specific system information" information element. If T3212 is set to zero, 3GPP TS 24.008 indicates that the UE shall interpret this as infinity (never perform a periodic location update).
GPIB command: CALL[:CELL]:BCCHannel:T3212
T3312 Periodic RA Update Timer
This setting is only applicable to the lab application.
This setting determines the value of the periodic Routing Area (RA) update timer. 3GPP TS 24.008 s4.7.2.2 states that "The value of timer T3312 is sent by the network to the MS in messages ATTACH ACCEPT and ROUTING AREA UPDATE ACCEPT."
The increment value of this parameter is set by the T3312 Periodic RA Update Units parameters.
The T309 timer can be set to any integer from 0 to 31.
GPIB command: CALL[:CELL]:BCCHannel:T3312[:VALue]
T3312 Periodic RA Update Units
This setting is only applicable to the lab application.
This setting specifies the unit that the T3312 Periodic RA Update Timer is incremented.
The following settings are available:
SEC2 ): The T3312 Periodic RA Update Timer is incremented
every 2 seconds. MINutes ): The T3312
Periodic RA Update Timer is incremented every minute. DHOurs ): The T3312
Periodic RA Update Timer is incremented every decihour
(1 decihour = 6 minutes). DEACtivated ): The
T3312 Periodic RA Update Timer is deactivated.GPIB command: CALL[:CELL]:BCCHannel:T3312:UNITs
T305 Periodic Cell Update Timer
This setting is only applicable to the lab application.
T305 specifies the length of the periodical cell update timer. T305 starts while the UE is in CELL_FACH state. When T305 expires, the UE initiates the cell update procedure.
GPIB command: CALL[:CELL]:BCCHannel:T305
T323
Fast Dormancy Timer
GPIB command: CALL[:CELL]:BCCHannel:T323[:VALue]
T314 CS Domain Re-Establishment Timer
This setting is only applicable to the lab application.
T314 specifies how long the UE waits till the completion of Cell Update procedure after the CS domain radio link fails.
This setting
can not be changed in Active
Cell Operating Mode or the Call/Data
Status is not Idle.
GPIB command: CALL[:CELL]:BCCHannel:T314
T315 PS Domain Re-Establishment Timer
This setting is only applicable to the lab application.
T315 specifies how long the UE waits till the completion of Cell Update procedure after the PS domain radio link fails.
This setting
can not be changed in Active
Cell Operating Mode or the Call/Data
Status is not Idle.
GPIB command: CALL[:CELL]:BCCHannel:T315