Last updated: October 19, 2012
|
Queries the connected/disconnected state of the call. A one is returned if the call is in the connected state. A zero is returned if the call is in the idle (disconnected) state. If the call is in any state other than connected or idle, the query will hang until the call state transitions to the connected or idle state. When used in conjunction with the CALL:CONNected:ARM and CALL:CONNected:TIMeout commands, the CALL:CONNected:STATe? command allows the control program to synchronize to call connection/disconnection. See Connected/Idle Query and Call State Change Detector . |
|
| Requirements | |
OUTPUT 714;"CALL:CONNECTED:STATE?" ! returns 1 if call is connected, 0 if call is idle. |
|
|
Sets (arms) the call-state-change detector. Arming this detector allows the control program to tell the test set that it is expecting a change in the state of a call, prior to initiating the state change. Once armed, the detector remains armed until there is a call state change to Idle or Connected from one of the transitory states, nor is it disarmed by any transitions from Idle to Idle or Connected to Connected. When used in conjunction with the CALL CONNected:STATe? and the CALL:CONNected: TIMeout commands, the CALL:CONNected:ARM command allows the control program to synchronize with call processing state changes. See Call State Change Detector . For an explanation of the :DONE?, :OPComplete?, :SEQuential, and :WAIT commands, s ee Call Processing Event Synchronization . |
|
| Requirements | |
OUTPUT 714;"CALL:CONNECTED:ARM:IMMEDIATE" ! Arms the call-state-change detector. |
|
|
Queries the arm state of the call-state-change detector. This command never hangs and immediately returns a one if the detector is armed, or a zero if the detector is not armed. See Call State Change Detector |
|
| Requirements | |
OUTPUT 714;"CALL:CONN:ARM:STATE?" ! Returns arm state of the call-state-change detector. |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -5.35 dB (on) | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary -7" ! Sets P-CCPCH connected power offset to -7 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -12 dB (on) | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:HSDPa -7" ! Sets HSDPA P-CCPCH connected power offset to -7 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -12 dB (on) | |
| Requirements |
Test Application Revision: A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:HSPA -7" ! Sets HSPA P-CCPCH connected power offset to -7 dB and turns its state on. |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -5.35 dB | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:LEVel -7" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -12 dB | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:LEVel:HSDPa -7" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -12 dB | |
| Requirements |
Test Application Revision A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:LEVel:HSPA -7" |
|
|
Sets/queries the
The |
|
| 1 (on) | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:STATe ON" |
|
|
Sets/queries the
The |
|
| 1 (on) | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:STATe:HSDPa ON" |
|
|
Sets/queries the
The |
|
| 1 (on) | |
| Requirements |
Test Application Revision A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -20.00 dB (off) | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary -10" ! Sets S-CCPCH connected power offset to -10 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -20.00 dB (off) | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:HSDPa -10" ! Sets HSDPA S-CCPCH connected power offset to -10 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -20.00 dB (off) | |
| Requirements |
Test Application Revision A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:HSPA -10" ! Sets HSPA S-CCPCH connected power offset to -10 dB and turns its state on. |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -20.00 dB | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:LEVel -5" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -20.00 dB | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:LEVel:HSDPa -5" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -20.00 dB | |
| Requirements |
Test Application Revision A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:LEVel:HSPA -5" |
|
|
Sets/queries the
The |
|
| 0 (off) | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:STATe OFF" |
|
|
Sets/queries the
The |
|
| 0 (off) | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:STATe:HSDPa OFF" |
|
|
Sets/queries the
The |
|
| 0 (off) | |
| Requirements |
Test Application Revision A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:STATe:HSPA OFF" |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -3.30 dB (on) | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:CPIChannel -7" ! Sets CPICH connected power offset to -7 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -10 dB (on) | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CPIChannel:HSDPa -7" ! Sets HSDPA CPICH connected power offset to -7 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -10 dB (on) | |
| Requirements |
Test Application Revision: A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CPIChannel:HSPA -7" ! Sets HSPA CPICH connected power offset to -7 dB and turns its state on. |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -3.30 dB | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:CPIChannel:LEVel -7" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -10 dB | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CPIChannel:LEVel:HSDPa -7" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -10 dB | |
| Requirements |
Test Application Revision: A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CPIChannel:LEVel:HSPA -7" |
|
|
Sets/queries the
The |
|
| 1 (ON) | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:CPIChannel:STATe ON" |
|
|
Sets/queries the
The |
|
| 1 (ON) | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CPIChannel:STATe:HSDPa ON" |
|
|
Sets/queries the
The |
|
| 1 (ON) | |
| Requirements |
Test Application Revision: A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:CPIChannel:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -10.30 dB (on) | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:DPCHannel -7" ! Sets DPCH connected power offset to -7 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -10 dB (on) | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:DPCHannel:HSDPa -7" ! Sets HSDPA DPCH connected power offset to -7 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -10 dB (on) | |
| Requirements |
Test Application Revision A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:DPCHannel:HSPA -7" ! Sets HSPA DPCH connected power offset to -7 dB and turns its state on. |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -10.30 dB | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:DPCHannel:LEVel -7" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -10 dB | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:DPCHannel:LEVel:HSDPa -7" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -10 dB | |
| Requirements |
Test Application Revision A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:DPCHannel:LEVel:HSPA -7" |
|
|
Sets/queries the
The |
|
| 1 (on) | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:DPCHannel:STATe ON" |
|
|
Sets/queries the
The |
|
| 1 (on) | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:DPCHannel:STATe:HSDPa ON" |
|
|
Sets/queries the
The |
|
| 1 (on) | |
| Requirements |
Test Application Revision A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:DPCHannel:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -20 dB (on) | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:EAGChannel -20"
! Sets the
|
|
|
Sets/queries the
The |
|
| Same as setting | |
| -20 dB | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:EAGChannel:LEVel -20" |
|
|
Sets/queries the
The |
|
| 1 (on) | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:EAGChannel:STATe ON" |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -20 dB (on) | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:EHIChannel -20"
! Sets the
|
|
|
Sets/queries the
The |
|
| Same as setting | |
| -20 dB | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:EHIChannel:LEVel -20" |
|
|
Sets/queries the
The |
|
| 1 (on) | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:EHIChannel:STATe ON" |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -20 dB (off) | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:ERGChannel -20"
! Sets the
|
|
|
Sets/queries the
The |
|
| Same as setting | |
| -20 dB | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:ERGChannel:LEVel -20" |
|
|
Sets/queries the
The |
|
| 0 (off) | |
|
Test Application Revision: A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:ERGChannel:STATe OFF" |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -3 dB (on) | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSPDschannel -4"
! Sets the
|
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -3 dB (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSPDschannel:HSPA -4"
! Sets the
|
|
|
Sets/queries the
The |
|
| Same as setting | |
| -3 dB | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSPDschannel:LEVel -4" |
|
|
Sets/queries the HSPA Cell 1 Connected HS-PDSCHs Level (Sum).
The |
|
| Same as setting | |
| -3 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSPDschannel:LEVel:HSPA -4" |
|
|
Sets/queries the
The |
|
| 1 (on) | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSPDschannel:STATe ON" |
|
|
Sets/queries the
The |
|
| 1 (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSPDschannel:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -10 dB (on) | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel -11"
! Sets the
|
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -10 dB (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel:HSPA -11"
! Sets the
|
|
|
Sets/queries the
The |
|
| Same as setting | |
| -10 dB | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel:LEVel -11" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -10 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel:LEVel:HSPA -11" |
|
|
Sets/queries the
The |
|
| 1 (on) | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel:STATe ON" |
|
|
Sets/queries the
The |
|
| 1 (on) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -15 dB (off) | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel2 -11"
! Sets the
|
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -15 dB (off) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel2:HSPA -11"
! Sets the
|
|
|
Sets/queries the
The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel2:LEVel -11" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel2:LEVel:HSPA -11" |
|
|
Sets/queries the
The |
|
| 0 (off) | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel2:STATe ON" |
|
|
Sets/queries the
The |
|
| 0 (off) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel2:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -15 dB (off) | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel3 -11"
! Sets the
|
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -15 dB (off) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel3:HSPA -11"
! Sets the
|
|
|
Sets/queries the
The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel3:LEVel -11" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel3:LEVel:HSPA -11" |
|
|
Sets/queries the
The |
|
| 0 (off) | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel3:STATe ON" |
|
|
Sets/queries the
The |
|
| 0 (off) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel3:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -15 dB (off) | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel4 -11"
! Sets the
|
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -15 dB (off) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel4:HSPA -11"
! Sets the
|
|
|
Sets/queries the
The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel4:LEVel -11" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -15 dB | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel4:LEVel:HSPA -11" |
|
|
Sets/queries the
The |
|
| 0 (off) | |
|
Test Application Revision: A.08.20 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel4:STATe ON" |
|
|
Sets/queries the
The |
|
| 0 (off) | |
|
Test Application Revision A.12 and above, with the required feature license. |
|
OUTPUT 714;"CALL:CONNected:HSSCchannel4:STATe:HSPA ON" |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -8.33 dB (on) | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:PICHannel -7" ! Sets PICH connected power offset to -7 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -15 dB (on) | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:PICHannel:HSDPa -7" ! Sets HSDPA PICH connected power offset to -7 dB and turns its state on. |
|
|
The setting form of this command performs two functions: (1) sets the
The query form of this command returns the |
|
| Same as setting | |
| -15 dB (on) | |
| Requirements |
Test Application Revision A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:PICHannel:HSPA -7" ! Sets HSDPA PICH connected power offset to -7 dB and turns its state on. |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -8.33 dB | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:PICHannel:LEVEL -7" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -15 dB | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:PICHannel:LEVEL:HSDPa -7" |
|
|
Sets/queries the
The |
|
| Same as setting | |
| -15 dB | |
| Requirements |
Test Application Revision A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:PICHannel:LEVEL:HSPA -7" |
|
|
Sets/queries the
The |
|
| 1 (ON) | |
| Requirements | |
OUTPUT 714;"CALL:CONNected:PICHannel:STATe OFF" |
|
|
Sets/queries the
The |
|
| 1 (ON) | |
| Requirements |
Test Application Revision: A.08.20 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:PICHannel:STATe:HSDPa OFF" |
|
|
Sets/queries the
The |
|
| 1 (ON) | |
| Requirements |
Test Application Revision A.12 and above, with the required feature license. |
OUTPUT 714;"CALL:CONNected:PICHannel:STATe:HSPA OFF" |
|
|
Sets/queries the maximum time the test set will wait for a hanging CALL:CONNected:STATe? query to complete. Default setting units are seconds. To set timeout time in units other than seconds, include an optional unit specifier in the command string. A timeout timer is started whenever the call-state-change detector becomes armed or gets rearmed when already armed. The duration of this timeout is set using the CALL:CONNected:TIMeout command and should be greater than the maximum amount of time the control program needs to wait between arming the call-state-change detector and the connect/disconnect operation starting. Once the process starts and the call state has moved to one of the transitory states, the W-CDMA defined protocol timers take over and prevent the call state from staying in a transitory state forever. See Call Processing State Synchronization . |
|
| Requirements | |
OUTPUT 714;"CALL:CONNECTED:TIMEOUT 3" ! Sets the CALL:CONNected:STATe? query timeout time to 3 seconds. OUTPUT 714;"CALL:CONNECTED:TIMEOUT 500 MS" ! Sets the Sets the CALL:CONNected:STATe? query timeout time to 500 milliseconds. |
|