Description
Using the call processing subsystem overlapped command synchronization commands, you can query the test set to find out when an overlapped command operation is done (:DONE?, :OPC?), force the test set to not execute any more commands until an overlapped command operation has completed (:WAIT), or simply force an overlapped command to behave as a sequential command (:SEQ).
Pending Operation Flags
Associated with each overlapped command, the test set maintains a binary indicator known as a pending operation flag. A pending operation flag is set true when the operation started by the overlapped command is executing, and is set false when the operation is no longer executing.
In addition to the call processing subsystem overlapped commands, the test set also provides the measurement-related INITiate <measurement> overlapped commands.
Call Processing Subsystem Overlapped Command Synchronization Commands
Overlapped Commands
|
Command |
Purpose Of Command |
Example
|
|
:DONE?
|
Returns a 0 if the associated command's pending operation flag is true, or a 1 if it is false.
|
10 OUTPUT 714;"CALL:TCH 65"
20 OUTPUT 714;"SETUP:TXP:CONT OFF"
30 OUTPUT 714;"SETUP:PFER:CONT OFF"
40 REPEAT
50 OUTPUT 714;"CALL:TCH:DONE?"
60 ENTER 714;Process_done
70 UNTIL Process_done
80 OUTPUT 714;INIT:TXP;PFER"
90 END
The example shown is from the E1960A GSM test application. Commands the test set to perform a traffic channel handover and execute two setup commands. After the two setup commands have finished, the :DONE? command is used to find out if the handover is finished
|
|
:SEQuential
|
Forces an overlapped command to execute in a sequential manner. No subsequent commands will be executed until the pending operation flag for this operation is false.
|
OUTPUT 714;"CALL:TCH:SEQ 65"
The example shown is from the E1960A GSM test application. Commands the test set to perform a traffic channel handover and to not execute any more commands until the pending operation flag associated with the CALL:TCH command is false.
|
|
:WAIT
|
Forces the test set to wait until the associated command's pending operation flag is false before executing any more commands.
|
10 OUTPUT 714;"CALL:TCH 65"
20 OUTPUT 714;"SETUP:TXP:CONT OFF"
30 OUTPUT 714;"SETUP:PFER:CONT OFF"
40 OUTPUT 714;"CALL:TCH:WAIT"
50 OUTPUT 714;"INIT:TXP;PFER"
60 END
The example shown is from the E1960A GSM test application. Commands the test set to perform a traffic channel handover and execute two setup commands. After the two setup commands have finished, the :WAIT command is sent to prevent the test set from executing the INITiate command until the handover is finished.
|
|
:OPComplete?
|
Places a 1 in the test set's output queue when the associated command's pending operation flag goes false. Controlling program hangs on this query until the 1 is retrieved.
|
10 OUTPUT 714;"CALL:TCH 65"
20 OUTPUT 714;"SETUP:TXP:CONT OFF"
30 OUTPUT 714;"SETUP:PFER:CONT OFF"
40 OUTPUT 714;"CALL:TCH:OPC?"
50 ENTER 714;Op_complete
60 OUTPUT 714;"INIT:TXP;PFER"
70 END
The example shown is from the E1960A GSM test application. Commands the test set to perform a traffic channel handover and execute two setup commands. After the two setup commands have finished, the :OPC? command is sent to hang program execution until a 1 is put in the test set's output queue, satisfying the ENTER statement and allowing program execution to continue with the INITiate command.
|
Operating Considerations
When using the call processing subsystem overlapped command synchronization commands, check the conditions that set the operation's pending operation flag (POF) false to avoid unexpected results.
Call Processing Subsystem Overlapped Commands
Overlapped Commands
|
Call Processing Command |
Purpose Of Command |
Pending Operation Flag (POF) is false when
|
|
CALL:ORIGinate
See
CALL:ORIGinate
.
|
Performs a base station call origination.
|
The call processing state leaves the Idle state (when the operating mode is active cell), or
The test set has noted this parameter change (when the operating mode is test mode).
|
|
CALL:CONNected:ARM[:IMMediate]
See
CALL:CONNected:ARM[:IMMediate]
.
|
Arms the call control status change detector.
|
The call control status change detector has been disarmed.
See
Connected/Idle Query
.
|