|
Queries the UE Reported Failure Cause . |
|
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:AUTHenticate:FAILcause?" !Queries the authentication fail cause. |
|
|
Queries the Configuration 1/2/3/4/5 Supported by UE . |
|
|
Range: 16 elements with each element raning from 0....1. Each element reflects a DB-DC-HSDPA configuration. 3GPP TS 25.331defines that there are 16 configurations at most. In 3GPP Release 9, there are three configurations defined in total, and there are two additional configurations added in 3GPP Release 10, thus only the first five elements make sense in these 16 elements. The X th element with the value 0 means the configuration on X is not supported by the UE, yet the value 1 means the configuration X is supported by the UE. |
|
| 0,0,0,0,0,0,0,0,0,0,0,0,0,0,0,0 | |
| Requirements |
Test Application Revision: A.20.00 and above, with the required feature licence |
OUTPUT 714;"CALL:MS:REPorted:CAPability:DCHSdpa:DBANd?" !Queries the DB-DC-HSDPA configuration(s) supported by the UE. |
|
|
Queries the UE (mobile station) reported measurement results after a successful Measurement Request (see CALL:MS:REPorted:MEASurement:REQuest ). The measurement results returned include CPICH Ec/No, Pathloss and CPICH RSCP (see UE Reported Measurements for more descriptions). After a successful Measurement Request, three comma separated results are returned in the order of CPICH Ec/No, Pathloss, and CPICH RSCP. See CALL:MS:REPorted[:CELL[1]]:CPICh:ECNO? , CALL:MS:REPorted[:CELL[1]]:PATHloss? , and CALL:MS:REPorted[:CELL[1]]:CPICh:RSCP? for more information. To obtain DTCH BLER results, see CALL:MS:REPorted[:CELL[1]]:DTCH:BLER? . |
|
| 9.91E +37 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:ALL?" |
|
|
Queries the UE (mobile station) reported CPICH Ec/No measurement result which is an index to a range of Ec/No values. See CPICH Ec/No for the mapping of this report value to actual Ec/No range. |
|
| 9.91E +37 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:CPICh:ECNO?" |
|
|
Queries the UE (mobile station) reported CPICH RSCP measurement result which is an index to a range of RSCP values. See CPICH RSCP (Received Signal Code Power) for the mapping of this report value to actual RSCP range. |
|
| 9.91E +37 | |
| Requirements |
Test Application Revision: A.03 and above. Lab Application Revision: A.01 and above. Lab Application Revision: I.01.00 and above, extended the range from 0 -- 91 to -5 -- 91. |
OUTPUT 714;"CALL:MS:REPorted:CPICh:RSCP?" |
|
|
Queries the UE (mobile station) reported Pathloss measurement result in the unit of dB. See Pathloss for more details. |
|
| 9.91E +37 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:PATHloss?" |
|
|
Queries the UE (mobile station) reported DTCH BLER measurement result which is an index to a range of BLER values. See DTCH BLER (Block Error Ratio) Report for the mapping of this report value to actual BLER range. |
|
| 9.91E +37 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:DTCH:BLER?" |
|
|
Queries the cell 2 UE (mobile station) reported measurement results after a successful Measurement Request (see CALL:MS:REPorted:MEASurement:REQuest ). The supported measurements include CPICH Ec/No, Pathloss and CPICH RSCP (see Cell 1/Cell 2 UE Reported Measurements for more information). After a successful Measurement Request, three comma separated results are returned in the order of CPICH Ec/No, Pathloss, and CPICH RSCP. See CALL:MS:REPorted[:CELL[1]]:CPICh:ECNO? , CALL:MS:REPorted[:CELL[1]]:PATHloss? , and CALL:MS:REPorted[:CELL[1]]:CPICh:RSCP? for more information. To obtain DTCH BLER results, see CALL:MS:REPorted[:CELL[1]]:DTCH:BLER? . |
|
| 9.91E +37 | |
| Requirements | Lab Application Revision: A.01 and above |
OUTPUT 714;"CALL:MS:REPorted:CELL2:ALL?" |
|
|
Queries the cell 2 UE (mobile station) reported CPICH Ec/No measurement result which is an index to a range of Ec/No values. See CPICH Ec/No for the mapping of this report value to actual Ec/No range. |
|
| 9.91E +37 | |
| Requirements | Lab Application Revision: A.01 and above |
OUTPUT 714;"CALL:MS:REPorted:CELL2:CPICh:ECNO?" |
|
|
Queries the cell 2 UE (mobile station) reported CPICH RSCP measurement result which is an index to a range of RSCP values. See CPICH RSCP (Received Signal Code Power) for the mapping of this report value to actual RSCP range. |
|
| 9.91E +37 | |
| Requirements |
Lab Application Revision: A.01 and above. Lab Application Revision: I.01.00 and above, extended the range from 0 -- 91 to -5 -- 91. |
OUTPUT 714;"CALL:MS:REPorted:CELL2:CPICh:RSCP?" |
|
|
Queries the UE reported SFN-SFN Observed Time Difference (OTD) measurement result. The type of OTD measurement performed by the UE can be queried using the CALL:MS:REPorted:CELL2:OTDifference:TYPE? command. |
|
| 9.91E +37 | |
| Requirements | Lab Application Revision: C.01 and above |
OUTPUT 714;"CALL:MS:REPorted:CELL2:OTDifference?" |
|
|
Queries the type of SFN-SFN Observed Time Difference (OTD) measurement performed by the UE. The UE reported OTD measurement result can be queried using the CALL:MS:REPorted:CELL2:OTDifference[:VALue]? command. |
|
| NONE | |
| Requirements | Lab Application Revision: C.01 and above |
OUTPUT 714;"CALL:MS:REPorted:CELL2:OTDifference:TYPE?" |
|
|
Queries the cell 2 UE reported Pathloss measurement result. |
|
| 9.91E +37 | |
| Requirements | Lab Application Revision: A.01 and above |
OUTPUT 714;"CALL:MS:REPorted:CELL2:PATHloss?" |
|
| Clears the UE (mobile) reported information. See Clear UE Info . | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:CLEar" |
|
|
Queries the International Mobile station Equipment Identity and Software Version number (IMEISV) reported by the UE. This result is not available when CALL[:CELL]:EIDentity:REQuest] is set to "IMEI". The IMEISV is composed of the following elements: - Type Allocation Code (TAC). Its length is 8 digits;- Serial Number (SNR) is an individual serial number uniquely identifying each equipment within each TAC. Its length is 6 digits;- Software Version Number (SVN) identifies the software version number of the mobile equipment. Its length is 2 digits. |
|
| Range: 0 to FFFFFFFFFFFFFFFF (16 chars, '0'-'9', 'A'-'F' in each char), No Results Available | |
| No Results Available | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:EISV?" |
|
|
Queries only the Software Version Number (SVN) element of the IMEISV reported by the UE. The SVN identifies the software version number of the mobile equipment. Its length is 2 digits. This result is not available when CALL[:CELL]:EIDentity:REQuest] is set to "IMEI". |
|
| Range: 0 to FF (2 chars, '0'-'9', 'A'-'F' in each char), No Results Available | |
| No Results Available | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:EISV:SVN?" |
|
Queries the
BCH ARFCN
result reported by the UE (for up to 8 GSM cells). Note that the cells are reported by the UE in order of RSSI strength. Use the
CALL:MS:REPorted:GSMSystem:CIDentity?
query to determine the
Inter-RAT Cell ID
for each of the reported cells. |
|
| 9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:GSMSystem:BCHannel?" |
|
Queries the
BSIC Value
corresponding to the
Inter-RAT Cell ID
reported by the UE (for up to 8 GSM cells). Note that the cells are reported by the UE in order of RSSI strength. Use the
CALL:MS:REPorted:GSMSystem:CIDentity?
query to determine the
Inter-RAT Cell ID
for each of the reported cells. |
|
| Range: 0 to 77, 9.91E+37 | |
| 9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37 | |
| Requirements | Lab Application Revision: D.00.04 and above. |
OUTPUT 714;"CALL:MS:REPorted:GSMSystem:BSIC:VALue?" |
|
Queries the
BSIC Verification
result reported by the UE (for up to 8 GSM cells). Note that the cells are reported by the UE in order of RSSI strength. Use the
CALL:MS:REPorted:GSMSystem:CIDentity?
query to determine the
Inter-RAT Cell ID
for each of the reported cells. |
|
| NREP,NREP,NREP,NREP,NREP,NREP,NREP,NREP | |
| Requirements | Lab Application Revision: D.00.04 and above. |
OUTPUT 714;"CALL:MS:REPorted:GSMSystem:BSIC:VERification?" |
|
| GSM neighbor cells are reported by the UE in order of RSSI strength. This query returns the Inter-RAT Cell ID for each of the cells reported by the UE, to allow you to map the UE reported results to the SIB11 GSM cell info list neighbor cells. | |
| 9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37 | |
| Requirements | Lab Application Revision: D.00.04 and above. |
OUTPUT 714;"CALL:MS:REPorted:GSMSystem:CIDentity?" |
|
| Queries the UE reported Total Number of GSM Cells . | |
| 0 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:GSMSystem:CELLs?" |
|
| Queries the RSSI (GSM Cells) result reported by the UE (for up to 8 GSM cells). Note that the cells are reported by the UE in order of RSSI strength. Use the CALL:MS:REPorted:GSMSystem:CIDentity? query to determine the cell ID for each of the reported cells. | |
| 9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:GSMSystem:RSSI?" |
|
|
Queries the mobile reported IMEI . |
|
|
Range: "0" to "FFFFFFFFFFFFFF" (0 to 15 characters from the set 0123456789ABCDEF) or "" (null string) |
|
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:IMEI?" |
|
|
Queries the mobile reported IMSI . |
|
|
Range: "0" to "FFFFFFFFFFFFFF" (0 to 15 characters from the set 0123456789ABCDEF) or "" (null string) |
|
| "" (null string) | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:IMSI?" |
|
| Queries the mobile reported total number of inter frequency cells (see Inter-Frequency Neighbor Cell Measurement Results ). | |
| 0 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:CELLs?" |
|
| Queries the mobile reported DL channel for inter frequency cells 1-8 (see Inter-Frequency Neighbor Cell Measurement Results ). | |
| 9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:DOWNlink:CHANnel?" |
|
| Queries the mobile reported Ec/No for inter frequency cells 1-8 (see Inter-Frequency Neighbor Cell Measurement Results ). | |
| 9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:ECNO?" |
|
| Queries the mobile reported pathloss for inter frequency cells 1-8 (see Inter-Frequency Neighbor Cell Measurement Results ). | |
| 9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:PATHloss?" |
|
| Queries the mobile reported RSCP for inter frequency cells 1-8 (see Inter-Frequency Neighbor Cell Measurement Results ). | |
| 9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37 | |
| Requirements |
Lab Application Revision: B.01 and above. Lab Application Revision: I.01.00 and above, extended the range from 0 -- 91 to -5 -- 91. |
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:RSCP?" |
|
| Queries the mobile reported RSSI for inter frequency cells 1-8 (see Inter-Frequency Neighbor Cell Measurement Results ). | |
| 9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:RSSI?" |
|
| Queries the mobile reported scrambling code for inter frequency cells 1-8 (see Inter-Frequency Neighbor Cell Measurement Results ). | |
| 9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37,9.91E+37 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:ITRFrequency:SCODe?" |
|
|
Sets/queries the SFN-SFN OTD Measurement Type performed by the UE when the CALL:MS:REPorted:MEASurement:REQuest command is sent. |
|
| Setting | Range: NONE|TYPE1|TYPE2 |
| Query | Same as setting. |
| *RST Setting | NONE |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:MEASurement:OTDifference:TYPE TYPE2" ! Sets SFN-SFN OTD Measurement Type to Type 2. |
|
|
Sends a Measurement Control message, which orders the UE to perform measurements on cell 1 (and cell 2 if you are using the lab application). Which measurements are performed by the UE is determined by the
CALL:MS:REPorted:MEASurement:TYPe
and
CALL:MS:REPorted:MEASurement:OTDifference:TYPE
commands. |
|
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:MEASurement:REQuest" |
|
| Sets/queries the Report Measurement Type , which determines which measurements are performed by the UE when the CALL:MS:REPorted:MEASurement:REQuest command is sent. | |
| Setting | |
| Same as setting. | |
| INTRAFREQ | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:MEASurement:TYPe ALL" |
|
|
Queries the Called Party Number . |
|
|
Range: 0 to 20 characters enclosed by double quotes, from the set 0123456789.*# or "Emergency Call" or "" (null string). |
|
| "" (null string) | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:ONUMber?" |
|
|
Queries the mobile reported Power Class . |
|
| 9.91E+37 | |
| Requirements | |
OUTPUT 714;"CALL:MS:REPorted:PCLass?" |
|
|
Queries the Detected PRACH Signature . |
|
| Requirements | Lab Application Revision: A.02 and above |
OUTPUT 714;"CALL:MS:REPorted:PRAChannel:SIGnature?" |
|