When there is an active link between the UE and the test set, the UE can perform measurements on the test set's (cell 1) downlink signal and report the measurement results. For non-HSDPA connections, you can view the UE measurement results from the front panel (see How Do I Order and Retrieve UE Reported Measurement Results? ) or retrieve them using the appropriate GPIB syntax queries (see CALL:MS:REPorted ).
With the lab application only, the UE can report measurement results for both cell 1 and cell 2.
With the lab application only, in addition to measuring cell 1 and cell 2 from the test set, if the UE supports compressed mode operation (see Compressed Mode ), the UE can perform measurements on inter frequency neighbor cells or GSM neighbor cells (see Inter-frequency Cells and GSM Cells ). To enable this, you must specify these neighbor cells in the test set's BCCH messaging (see SIB11 Cell Info List ), and then use an external source to provide these neighbor cells to the UE (you may also order the UE to measure these neighbor cells without actually providing them via an external source, but the UE will simply give results indicating that there was no usable signal at the specified neighbor cell). The test set can retrieve the UE's measurement results for up to 8 inter frequency neighbor cells and 8 GSM neighbor cells.
Once you have established a (non-HSDPA) connection between the test set and UE, you can order the UE to perform measurements on cell 1 (and cell 2 if you are using the lab application) by selecting
Send Measurement Request
(see
How Do I Order and Retrieve UE Reported Measurement Results?
and
CALL:MS:REPorted:MEASurement:REQuest
). When you select
Send Measurement Request
, the test set sends a Measurement Control Message to the UE indicating which measurements to perform, based on the following settings:
Report Measurement Type
Intra-frequency
: When
Report Measurement Type
is set to
Intra-frequency
, the UE will make
CPICH Ec/No
,
CPICH RSCP (Received Signal Code Power)
and
Pathloss
measurements and return the results.
Quality
: When
Report Measurement Type
is set to
Quality
, the UE will measure
DTCH BLER (Block Error Ratio) Report
and return the result.
All
: When
Report Measurement Type
is set to
All
, the UE will measure
CPICH Ec/No
,
CPICH RSCP (Received Signal Code Power)
,
Pathloss
and
DTCH BLER (Block Error Ratio) Report
and return the results.GPIB command: CALL:MS:REPorted:MEASurement:TYPe .
SFN-SFN OTD Measurement Type
This setting is applicable to the lab application only. See 3GPP TS 25.133 s9.1.8.
None
: When
SFN-SFN OTD Measurement Type
is set to
None
, the UE will not measure SFN-SFN OTD.
Type 1
: When
SFN-SFN OTD Measurement Type
is set to
Type 1
, the UE will perform a Type 1
SFN-SFN Observed Time Difference (OTD)
measurement and return the result.
Type 2
: When
SFN-SFN OTD Measurement Type
is set to
Type 2
, the UE will perform a Type 2
SFN-SFN Observed Time Difference (OTD)
measurement and return the result.GPIB command: CALL:MS:REPorted:MEASurement:OTDifference:TYPE .
CPICH Ec/No
CPICH Ec/No is the ratio of the received energy per PN chip for the CPICH to the total received power spectral density at the UE antenna connector. The reporting range for CPICH Ec/No is -24 dB to 0 dB (0 to 49). See 3GPP TS 25.133 s9.1.2.3. When the
Cell 1 Connected CPICH Level
setting is set to
-3.30 dB
, the UE should report a value of 42 (-3.5 </= CPICH Ec/No < -3).
| CPICH Ec/No Reported Value | Measured Quantity Value | Unit |
|---|---|---|
| 0 | CPICH Ec/No < -24 | dB |
| 1 | -24 </= CPICH Ec/No < -23.5 | dB |
| ... | ... | ... |
| 48 | -0.5 </= CPICH Ec/No < 0 | dB |
| 49 | 0 </= CPICH Ec/No | dB |
GPIB command: CALL:MS:REPorted[:CELL[1]]:CPICh:ECNO? and CALL:MS:REPorted:CELL2:CPICh:ECNO? .
CPICH RSCP (Received Signal Code Power)
This is the absolute power level of the CPICH as received by the UE. The reporting range for CPICH RSCP is from -120 dBm to -25 dBm (-5 to 91). See 3GPP TS 25.133 v10.2.0 s9.1.1.3. When the
Cell 1 Connected CPICH Level
setting is set to
-3.30 dB
and
Cell Power
is set to
-75.00 dBm
, the UE should report a value of 37 (-79 </= CPICH RSCP < -78).
| CPICH RSCP Reported Value | Measured Quantity Value | Unit |
|---|---|---|
| -5 | CPICH RSCP < -120 | dBm |
| 0 | CPICH RSCP < -115 | dBm |
| 1 | -115 </= CPICH RSCP < -114 | dBm |
| ... | ... | ... |
| 90 | -26 </= CPICH RSCP < -25 | dBm |
| 91 | -25 </= CPICH RSCP | dBm |
GPIB command: CALL:MS:REPorted[:CELL[1]]:CPICh:RSCP? and CALL:MS:REPorted:CELL2:CPICh:RSCP? .
This is the pathloss between the cell and UE. It is calculated by comparing the UE's measurement of CPICH RSCP and the value of Primary CPICH Tx Power (the power level of the CPICH at the cell, as reported by the cell).
Pathloss (dB) = Primary CPICH Tx Power (dBm) - CPICH RSCP (dBm)
The range of the Pathloss measurement result is 46 dB to 158 dB.
GPIB commands: CALL:MS:REPorted[:CELL[1]]:PATHloss? and CALL:MS:REPorted:CELL2:PATHloss? .
This is a measure of the UE's ability to receive the DTCH without errors. The reporting range for BLER is 0 to 1 (0 to 63). For the lab application, if you have enabled soft handover (see Soft Handover ), the DTCH BLER Report result includes both cell 1 and cell 2. See 3GPP TS 25.133 s9.1.5.
| DTCH BLER Reported Value | Measured Quantity Value | Unit |
|---|---|---|
| 0 | BLER = 0 | - |
| 1 | -infinity < Log10(BLER) < -4.03 | - |
| 2 | -4.03 </= Log10(BLER) < -3.965 | - |
| ... | ... | ... |
| 61 | -0.195 </= Log10(BLER) < -0.13 | |
| 62 | -0.13 </= Log10(BLER) < -0.065 | - |
| 63 | -0.065 </= Log10(BLER) < -0 | - |
GPIB command: CALL:MS:REPorted[:CELL[1]]:DTCH:BLER? .
To set the BLER reporting interval (the UE's observation period for determining BLER), see How Do I Order and Retrieve UE Reported Measurement Results? or CALL:DTCHannel:BLER:REPorting:INTerval .
This measurement result is available in the lab application only. As defined in 3GPP TS 25.215 5.1.9, the UE can measure the timing difference (in chips) between cell 1 and cell 2. There are two types of SFN-SFN OTD measurements:
You can change the time offset between cell 1 and cell 2 using the
Cell 2 Time Offset
setting. Note, while
Cell 2 Time Offset
can be set to a negative value, the OTD measurement result gives the absolute timing difference between cell 1 and cell 2.
GPIB commands: CALL:MS:REPorted:CELL2:OTDifference[:VALue]? and CALL:MS:REPorted:CELL2:OTDifference:TYPE? .
In the lab application only, you can enable compressed mode operation in the uplink and downlink, order the UE to perform measurements on Inter-frequency Cells , GSM Cells or SIB19 E-UTRA Info List , and then retrieve the UE's measurement results (see Compressed Mode ).
A single measurement report from the UE can return results for up to 8 GSM neighbor cells, 8 inter-frequency neighbor cells or 8 cells across four different EARFCNs (the standard allows the UE to measure up to 16 E-UTRAN cells (3GPP TS 25.331), but the test set only reports the first 8 E-UTRAN cells).
See How Do I Enable Compressed Mode and Obtain UE Measurement Results? .
Returns the total number of inter-frequency cells reported by the UE. Although the UE can measure up to 32 inter-frequency cells at two different frequencies (as per 3GPP TS 25.133 s8.1.2.1), the test set will only display on the front panel and return by GPIB query the results for the first 8 cells measured. As the test set can only specify up to 8 neighbor cells for the UE to measure, it is expected that the UE will not return results for more than 8 cells. However, the results for all measured cells are available in the Measurement Reports returned by the UE, which are viewable using the Wireless Protocol Advisor (see Protocol Logging ).
GPIB command: CALL:MS:REPorted:ITRFrequency:CELLs?
The scrambling code is returned for each inter-frequency cell measured by the UE (up to 8 measured cells).
GPIB command: CALL:MS:REPorted:ITRFrequency:SCODe?
The downlink channel is returned for each inter-frequency cell measured by the UE (up to 8 measured cells).
GPIB command: CALL:MS:REPorted:ITRFrequency:DOWNlink:CHANnel?
RSSI (Received Signal Strength Indicator) is returned for each inter-frequency cell measured by the UE (up to 8 measured cells). See 3GPP TS 25.133 table 9.12 for a mapping of returned value to actual value.
GPIB command: CALL:MS:REPorted:ITRFrequency:RSSI?
Ec/No is returned for each inter-frequency cell measured by the UE (up to 8 measured cells). See CPICH Ec/No .
GPIB command: CALL:MS:REPorted:ITRFrequency:ECNO?
RSCP is returned for each inter-frequency cell measured by the UE (up to 8 measured cells). See CPICH RSCP (Received Signal Code Power) .
GPIB command: CALL:MS:REPorted:ITRFrequency:RSCP?
Pathloss is returned for each inter-frequency cell measured by the UE (up to 8 measured cells). See Pathloss .
GPIB command: CALL:MS:REPorted:ITRFrequency:PATHloss?
Returns the number of GSM cell measurement results available from the front panel and over GPIB (up to 8). Per 3GPP TS 25.133 s8.1.2.1, the UE can measure as many as 32 GSM neighbor cells. As the test set can only specify up to 8 neighbor cells for the UE to measure, it is expected that the UE will not return results for more than 8 cells. However, the results for all measured cells are available in the Measurement Reports returned by the UE, which are viewable using the Wireless Protocol Advisor (see Protocol Logging ).
GPIB command: CALL:MS:REPorted:GSMSystem:CELLs?
The BCH ARFCN is returned for each GSM cell measured by the UE (up to 8 measured cells).
GPIB command: CALL:MS:REPorted:GSMSystem:BCHannel?
Because the cells are reported in order of RSSI strength rather than by cell ID, the cell ID for each cell (numbered 1 to 8) is returned to help you quickly determine which neighbor cell is being reported by the UE.
GPIB command: CALL:MS:REPorted:GSMSystem:CIDentity?
A result of
Verified
indicates that the UE decoded the BSIC of the measured cell, and it matched the BSIC it expected based on the NCC and BCC values in the SIB11 GSM cell info list for that cell. Note, you may need to set
GSM Meas BSIC Verification
to
verifiedBSIC
and include a TGPS with a
<num> TG Measurement Purpose (TGMP)
of
GSM Initial BSIC ID
or
GSM BSIC Reconfirmation
in order for the UE to attempt to verify the BSIC of the GSM cells.
GPIB command: CALL:MS:REPorted:GSMSystem:BSIC:VERification?
The
BSIC Value
result is not reported by the UE in the Measurement Reports. Rather, for your convenience, the test set calculates and posts the BSIC corresponding to the cell ID reported by the UE (the test set calculates the BSIC from the NCC and BCC values it signalled for that cell in the SIB11 GSM cell info list).
As per 3GPP TS 25.331 s10.3.8.2 and 23.003 s4.3.2, BSIC (Base Station Identity Code) is a 6-bit concatenation of NCC (Network Colour Code) and BCC (Base Station Colour Code). For example, if NCC = 2 and BCC = 1, BSIC = 21. As NCC and BCC range between 0 and 7, the range of BSIC is thus 0-7, 10-17, 20-27, 30-37, 40-47, 50-57, 60-67 and 70-77.
GPIB command: CALL:MS:REPorted:GSMSystem:BSIC:VALue?
The RSSI (Received Signal Strength Indicator) is returned for each GSM cell measured by the UE (up to 8 measured cells). See 3GPP TS 45.008 s8.1.4 for a mapping of returned value to actual value.
GPIB command: CALL:MS:REPorted:GSMSystem:RSSI?
This result indicates the EARFCN for the first 8 cells that are present in the measurement report.
GPIB command: CALL:MS:REPorted:EUTRa:EARFcn?
This result indicates the Cell ID for the first 8 cells that are present in the measurement report.
GPIB command: CALL:MS:REPorted:EUTRa:CID?
This result indicates the RSRP for the first 8 cells that are present in the measurement report.
GPIB command: CALL:MS:REPorted:EUTRa:RSRP?
This result indicates the RSRQ for the first 8 cells that are present in the measurement report.
GPIB command: CALL:MS:REPorted:EUTRa:RSRQ?
This result indicates the total number of E-UTRA cells that the UE included in its Measurement Result.
GPIB command: CALL:MS:REPorted:EUTRa:CELLs?
Manual Operation:
How Do I Order and Retrieve UE Reported Measurement Results?
and
How Do I Enable Compressed Mode and Obtain UE Measurement Results?
GPIB Syntax: CALL:MS:REPorted
UE Reported Measurements Ladder Diagrams
Troubleshooting UE Reported Measurements