Last updated: January 15, 2009
|
Generates a page attempt to the mobile station based on the Paging Service parameter setting. See Test Set-Originated Connection . If the call attempt fails, the test set will return to the idle call processing state. |
|
| Requirements |
Test Application Revision: A.02 and above. Lab Application Revision: A.01 and above. Lab Application Revision U.00.13 adds the optional AUTO mnemonic. |
OUTPUT 714;"CALL:ORIGinate" !pages the mobile station |
|
|
Generates a AMR voice page attempt to the mobile station regardless of the Paging Service parameter setting. See Test Set-Originated Connection . If the call attempt fails, the test set will return to the idle call processing state. |
|
| Requirements | |
OUTPUT 714;"CALL:ORIGinate:AMR" !sends an AMR voice page the mobile station |
|
| See Call Processing Event Synchronization | |
| Requirements | |
OUTPUT 714;"CALL:ORIGinate:DONE?" |
|
| See Call Processing Event Synchronization | |
| Requirements | |
OUTPUT 714;"CALL:ORIGinate:OPComplete?" |
|
|
Generates a PS Data page attempt to the mobile station regardless of the Paging Service parameter setting. See Test Set-Originated Connection . If the page attempt fails, the test set will return to the idle call processing state. |
|
| Requirements | |
OUTPUT 714;"CALL:ORIGinate:PSData" !sends an PS Data page the mobile station |
|
| Requirements | |
OUTPUT 714;"CALL:ORIGinate:SEQuential" |
|
| See Call Processing Event Synchronization | |
| Requirements | |
OUTPUT 714;"CALL:ORIGinate:WAIT" |
|