Last updated: January 16, 2009
This topic is only applicable to the lab application.
|
Sets/queries the RRC Connection Release Complete Wait Count .
This parameter can only be set when call status is |
|
| RETR1 | |
OUTPUT 714;"CALL:RRC:CRELease:CWCount RETRansmit1" ! Sets the RRC Connection Release Complete Wait Count to RETRansmit1 |
|
|
Sets/queries the N308 RRC Conn Release Comp Max Retransmits .
This parameter can only be set when call status is |
|
| Same as setting | |
| 2 | |
OUTPUT 714;"CALL:RRC:CRELease:N308 2" ! Sets the N308 constant to 2. |
|