Spectrum Emission Mask Troubleshooting

Spectrum Emission Mask Troubleshooting

Last updated: January 16, 2009

Possible Setup Issues

Interpreting Integrity Indicator Values

This measurement uses auto-ranging to automatically set the expected level into the test set.

If Over Range (5) is returned, the measured signal exceeds the expected input level or exceeds the maximum allowed input power for the test set.

If Under Range (6) is returned, the measured signal is below the expected input level.

If Uncalibrated Due to Temperature (19) is returned, the temperature in the test set has changed by ± 10° C or more since the last calibration and should be calibrated again. See Calibration Strategy

See Integrity Indicator .

Related Topics


Spectrum Emission Mask Measurement Description