This section is only applicable to the lab application.
You may configure the test set to ignore, reject or accept an Activate PDP Context Request from the UE. You can choose what value is sent in the SM Cause information element of the Activate PDP Context Reject message using the Activate PDP Context Reject SM Cause setting. Use this function in parallel with Protocol Logging to verify that the UE behaves in a manner conforming to the standards for this situation and for each associated SM Cause value.You can also specify the cause value that is sent in the SM Cause52 information element in the PDP Context Activation Accept Message using the Activate PDP Context Accept SM Cause 52 setting.
When
Activate PDP Context Reject State
is
On
, you may specify what value is sent in the SM Cause information element using the
Activate PDP Context Reject SM Cause
setting. From the front panel, you may choose from the valid causes specified in 3GPP TS 24.008 10.5.6.6.
If you select
Custom Value
from the front panel, a value of 0 is sent to the UE.
The
CALL:SERVice:GPRS:REJect:CAUSe
command allows you to send any value between 0 and 255 to the UE, even those not mapped to a cause in the standard. If you send a value other than those listed in the above table via the GPIB command, the front panel setting displays
CUSTOM
.
The setting specifies what value is sent in the SM Cause52 information element in the PDP Context Activation Accept Message. This setting is applicable when UE requested PDP Type is IPv4+IPv6 and DUT IP Version is set to IPv4 + IPv6, or when UE requested an additional primary PDP context's PDP Type is IPv4+IPv6 and DUT IP 2 Version is set to IPv4 + IPv6.
You can specify one of the following SM causes in the test set:
NONE
, SM Cause52 field is not included in the PDP Context Activation Accept Message, and the test set assigns an IPv4v6 address to the PDP context.
IPV4
, "SM Cause (52) - Single address bearers only allowed" is included in the PDP Context Activation Accept Message, and the test set overrides the PDP type requested by the UE to IPv4 for this PDP context.
IPV6
, "SM Cause (52) - Single address bearers only allowed" is included in the PDP Context Activation Accept Message, and the test set overrides the PDP type requested by the UE to IPv6 for this PDP context.See the following table for the detailed information:
| UE Requested PDP Type | SM Cause | ||||
|---|---|---|---|---|---|
| IPv4v6 | - | ||||
| IPv4v6 | 52 | ||||
| IPv4v6 | 52 |
GPIB command: CALL:SERVice:GPRS:ACCept:SMCause52
Ladder Diagram: UE Initiated GPRS Service, Activate PDP Context Reject