N1000A Regulatory Information and Instrument Markings
N1000A Regulatory Information
To find a current Declaration of Conformity for a specific Keysight product, go to:
http://www.keysight.com/go/conformity
SAFETY: Complies with the essential requirements of the European Low Voltage Directive as well as current editions of the following standards (dates and editions are cited in the Declaration of Conformity):
- IEC/EN 61010-1
- Canada: CSA C22.2 No. 61010-1
- USA UL std no. 61010-1
COMPLIANCE WITH CANADIAN EMC REQUIREMENTS
This ISM device complies with Canadian ICES-001.
Cet appareil ISM est conforme a la norme NMB du Canada.
EMC
Complies with the essential requirements of the European EMC Directive as well as current editions of the following standards (dates and editions are cited in the Declaration of Conformity):
- IEC/EN 61326-1
- CISPR Pub 11 Group 1, Class A
- AS/NZS CISPR 11
- ICES/NMB-001
This ISM device complies with Canadian ICES-001.
Cet appareil ISM est conforme a la norme NMB-001 du Canada.
South Korean Class A EMC Declaration:
This equipment is Class A suitable for professional use and is for use in electromagnetic environments outside of the home.
Acoustic statement: (European Machinery Directive)
Acoustic noise emission
LpA < 70 dB
Operator position
Normal operation mode per ISO 7779
Instrument Markings
The following table lists the definitions of markings that may be on the instrument.
Instrument Markings
| Marking |
Description |
|
The instruction documentation symbol. The product is marked with this symbol when it is necessary for the user to refer to the instruction in the documentation |
|
The ON/STANDBY symbol. The ON, OFF and STANDBY symbols are used to mark the positions of the instrument power line switch. |
|
The AC symbol is used to indicate the required nature of the line module input power. |
|
The chassis ground symbol. The chassis ground symbol is used to indicate a chassis connection. |
|
The CE marking is a registered trademark of the European Community (if accompanied by a year, it is the year when the design was proven). It indicates that the product complies with all relevant directives. |
|
The CSA mark is a registered trademark of the CSA International. |
|
The RCM mark is a registered trademark of the Australian Communications and Media Authority. |
|
ISM 1A
|
This is a symbol of an Industrial Scientific and Medical Group 1 Class A product (CISPR 11, Clause 5) |
|
ICES/NMB-001
|
This is a marking to indicate product compliance with the Canadian Interference-Causing Equipment Standard. Cet appareil ISM est conforme a la norme NMB du Canada. |
|
China Restricted Substance Product Label. The EPUP (environmental protection use period) number in the center indicates the time period during which no hazardous or toxic substances or elements are expected to leak or deteriorate during normal use and generally reflects the expected useful life of the product. |
|
South Korean Certification (KC) mark; includes the marking's identifier code which follows this format: MSIP-REM-YYY-ZZZZ. |
|
The crossed out wheeled bin symbol indicates that separate collection for waste electric and electronic equipment (WEEE) is required, as obligated by DIRECTIVE 2012/19/EU and other National legislation. Please refer to keysight.com/go/takeback to understand your Trade in options with Keysight in addition to product takeback instructions. |
|
Universal recycling symbol. This symbol indicates compliance with the China standard GB 18455-2001 as required by the China RoHS regulations for paper/fiberboard packaging. |
|
UK conformity mark is a UK government owned mark. Products showing this mark comply with all applicable UK regulations. |
|
The Keysight email address is required by EU directives applicable to our product. |