F-OTO (FlexOTO Basic Optimization)

L-OTO
L-OTO17
L-OTO48
L-OTO128
Flex Apps:
FlexDCA
FlexOTO

The FlexOTO feature activates the FlexOTO Optical Test Optimizer application. The feature is included in any of these licenses:

  • N1002000A (L-OTO), activates FlexOTO without support for an optical switch.
  • N1002014A (L-OTO17), activates 14 Port optical switch support for the FlexOTO.
  • N1002048A (L-OTO48), activates 48 Port optical switch support for the FlexOTO.
  • N1002128A (L-OTO128), activates 128 Port optical switch support for the FlexOTO.